/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2024 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ FDCAN_HandleTypeDef hfdcan2; /* USER CODE BEGIN PV */ FDCAN_RxHeaderTypeDef RxHeader; uint8_t RxData[8]; /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_FDCAN2_Init(void); /* USER CODE BEGIN PFP */ FDCAN_TxHeaderTypeDef TxHeader; uint8_t TxData[] = {0x10, 0x32, 0x54, 0x76, 0x98, 0x00, 0x11, 0x22, 0x33, 0x44, 0x55, 0x66, 0x77, 0x88, 0x99, 0x00}; /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_FDCAN2_Init(); /* USER CODE BEGIN 2 */ // FDCAN_TxHeaderTypeDef hdr = { // .Identifier = 0x700, // .IdType = FDCAN_STANDARD_ID, // .TxFrameType = FDCAN_DATA_FRAME, // .DataLength = FDCAN_DLC_BYTES_2, // // .ErrorStateIndicator = FDCAN_ESI_ACTIVE, // .BitRateSwitch = FDCAN_BRS_OFF, // .FDFormat = FDCAN_CLASSIC_CAN, // .TxEventFifoControl = FDCAN_STORE_TX_EVENTS, // .MessageMarker = 0x0 // // }; // uint16_t x = 0xff22; // HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan2, &hdr, &x); // */ TxHeader.Identifier = 0x321; TxHeader.IdType = FDCAN_STANDARD_ID; TxHeader.TxFrameType = FDCAN_DATA_FRAME; TxHeader.DataLength = FDCAN_DLC_BYTES_2; TxHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE; TxHeader.BitRateSwitch = FDCAN_BRS_OFF; TxHeader.FDFormat = FDCAN_CLASSIC_CAN; TxHeader.TxEventFifoControl = FDCAN_NO_TX_EVENTS; TxHeader.MessageMarker = 0; HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan2, &TxHeader, &TxData[0]); /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan2, &TxHeader, &TxData[0]); HAL_Delay(50); /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Supply configuration update enable */ HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY); /** Configure the main internal regulator output voltage */ __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3); while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {} /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_DIV1; RCC_OscInitStruct.HSICalibrationValue = 64; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI; RCC_OscInitStruct.PLL.PLLM = 4; RCC_OscInitStruct.PLL.PLLN = 12; RCC_OscInitStruct.PLL.PLLP = 2; RCC_OscInitStruct.PLL.PLLQ = 4; RCC_OscInitStruct.PLL.PLLR = 2; RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3; RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE; RCC_OscInitStruct.PLL.PLLFRACN = 0; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2 |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI; RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2; RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2; RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2; RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK) { Error_Handler(); } } /** * @brief FDCAN2 Initialization Function * @param None * @retval None */ static void MX_FDCAN2_Init(void) { /* USER CODE BEGIN FDCAN2_Init 0 */ FDCAN_FilterTypeDef sFilterConfig; /* USER CODE END FDCAN2_Init 0 */ /* USER CODE BEGIN FDCAN2_Init 1 */ /* USER CODE END FDCAN2_Init 1 */ hfdcan2.Instance = FDCAN2; hfdcan2.Init.FrameFormat = FDCAN_FRAME_CLASSIC; hfdcan2.Init.Mode = FDCAN_MODE_EXTERNAL_LOOPBACK; hfdcan2.Init.AutoRetransmission = ENABLE; hfdcan2.Init.TransmitPause = ENABLE; hfdcan2.Init.ProtocolException = DISABLE; hfdcan2.Init.NominalPrescaler = 12; hfdcan2.Init.NominalSyncJumpWidth = 1; hfdcan2.Init.NominalTimeSeg1 = 13; hfdcan2.Init.NominalTimeSeg2 = 2; hfdcan2.Init.DataPrescaler = 12; hfdcan2.Init.DataSyncJumpWidth = 1; hfdcan2.Init.DataTimeSeg1 = 13; hfdcan2.Init.DataTimeSeg2 = 2; hfdcan2.Init.MessageRAMOffset = 0; hfdcan2.Init.StdFiltersNbr = 4; hfdcan2.Init.ExtFiltersNbr = 4; hfdcan2.Init.RxFifo0ElmtsNbr = 3; hfdcan2.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_8; hfdcan2.Init.RxFifo1ElmtsNbr = 0; hfdcan2.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8; hfdcan2.Init.RxBuffersNbr = 0; hfdcan2.Init.RxBufferSize = FDCAN_DATA_BYTES_8; hfdcan2.Init.TxEventsNbr = 3; hfdcan2.Init.TxBuffersNbr = 0; hfdcan2.Init.TxFifoQueueElmtsNbr = 3; hfdcan2.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION; hfdcan2.Init.TxElmtSize = FDCAN_DATA_BYTES_8; if (HAL_FDCAN_Init(&hfdcan2) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN FDCAN2_Init 2 */ /* Configure Rx filter */ sFilterConfig.IdType = FDCAN_STANDARD_ID; sFilterConfig.FilterIndex = 0; sFilterConfig.FilterType = FDCAN_FILTER_MASK; sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0; sFilterConfig.FilterID1 = 0x321; sFilterConfig.FilterID2 = 0x7FF; if (HAL_FDCAN_ConfigFilter(&hfdcan2, &sFilterConfig) != HAL_OK) { /* Filter configuration Error */ Error_Handler(); } /* Start the FDCAN module */ if (HAL_FDCAN_Start(&hfdcan2) != HAL_OK) { /* Start Error */ Error_Handler(); } if (HAL_FDCAN_ActivateNotification(&hfdcan2, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0) != HAL_OK) { /* Notification Error */ Error_Handler(); } /* USER CODE END FDCAN2_Init 2 */ } /** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { /* USER CODE BEGIN MX_GPIO_Init_1 */ /* USER CODE END MX_GPIO_Init_1 */ /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOB_CLK_ENABLE(); /* USER CODE BEGIN MX_GPIO_Init_2 */ /* USER CODE END MX_GPIO_Init_2 */ } /* USER CODE BEGIN 4 */ void HAL_FDCAN_RxFifo0Callback(FDCAN_HandleTypeDef *hfdcan, uint32_t RxFifo0ITs) { if((RxFifo0ITs & FDCAN_IT_RX_FIFO0_NEW_MESSAGE) != RESET) { /* Retreive Rx messages from RX FIFO0 */ if (HAL_FDCAN_GetRxMessage(hfdcan, FDCAN_RX_FIFO0, &RxHeader, RxData) != HAL_OK) { /* Reception Error */ Error_Handler(); } /* Display LEDx */ if ((RxHeader.Identifier == 0x321) && (RxHeader.IdType == FDCAN_STANDARD_ID) && (RxHeader.DataLength == FDCAN_DLC_BYTES_2)) { volatile int x = 0; } if (HAL_FDCAN_ActivateNotification(hfdcan, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0) != HAL_OK) { /* Notification Error */ Error_Handler(); } } } /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */