/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2024 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ #include /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ CAN_HandleTypeDef hcan1; /* USER CODE BEGIN PV */ /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_CAN1_Init(void); /* USER CODE BEGIN PFP */ static void led1_on(void); static void led1_off(void); static void led2_on(void); static void led2_off(void); /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_CAN1_Init(); /* USER CODE BEGIN 2 */ CAN_TxHeaderTypeDef TxHeader; CAN_RxHeaderTypeDef RxHeader; uint8_t TxData[8]; uint8_t RxData[8]; uint32_t TxMailbox; TxHeader.StdId = 0x11; TxHeader.RTR = CAN_RTR_DATA; TxHeader.IDE = CAN_ID_STD; TxHeader.DLC = 2; TxHeader.TransmitGlobalTime = DISABLE; TxData[0] = 0xCA; TxData[1] = 0xFE; if (HAL_CAN_AddTxMessage(&hcan1, &TxHeader, TxData, &TxMailbox) != HAL_OK) { Error_Handler(); } while(HAL_CAN_IsTxMessagePending(&hcan1, TxMailbox)); while(HAL_CAN_GetTxMailboxesFreeLevel(&hcan1) != 3); HAL_Delay(20); if (HAL_CAN_GetRxFifoFillLevel(&hcan1, CAN_RX_FIFO0) != 1) { /** * I always get into this if-statement in the debugger, because * nothing was received respectively the sending process causes an error */ Error_Handler(); } if (HAL_CAN_GetRxMessage(&hcan1, CAN_RX_FIFO0, &RxHeader, RxData) != HAL_OK) { Error_Handler(); } if ((RxHeader.StdId != 0x11) || (RxHeader.RTR != CAN_RTR_DATA) || (RxHeader.IDE != CAN_ID_STD) || (RxHeader.DLC != 2) || ((RxData[0]<<8 | RxData[1]) != 0xCAFE)) { /* Rx message Error */ while (1) { led1_on(); HAL_Delay(150); led1_off(); HAL_Delay(150); } } /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Configure the main internal regulator output voltage */ __HAL_RCC_PWR_CLK_ENABLE(); __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3); /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK) { Error_Handler(); } } /** * @brief CAN1 Initialization Function * @param None * @retval None */ static void MX_CAN1_Init(void) { /* USER CODE BEGIN CAN1_Init 0 */ /* USER CODE END CAN1_Init 0 */ /* USER CODE BEGIN CAN1_Init 1 */ /* USER CODE END CAN1_Init 1 */ hcan1.Instance = CAN1; hcan1.Init.Prescaler = 16; hcan1.Init.Mode = CAN_MODE_LOOPBACK; hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ; hcan1.Init.TimeSeg1 = CAN_BS1_1TQ; hcan1.Init.TimeSeg2 = CAN_BS2_2TQ; hcan1.Init.TimeTriggeredMode = DISABLE; hcan1.Init.AutoBusOff = DISABLE; hcan1.Init.AutoWakeUp = DISABLE; hcan1.Init.AutoRetransmission = DISABLE; hcan1.Init.ReceiveFifoLocked = DISABLE; hcan1.Init.TransmitFifoPriority = DISABLE; if (HAL_CAN_Init(&hcan1) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN CAN1_Init 2 */ CAN_FilterTypeDef CAN1_Filter; CAN1_Filter.FilterBank = 0; CAN1_Filter.FilterMode = CAN_FILTERMODE_IDMASK; CAN1_Filter.FilterScale = CAN_FILTERSCALE_32BIT; CAN1_Filter.FilterIdHigh = 0x0000; CAN1_Filter.FilterIdLow = 0x0000; CAN1_Filter.FilterMaskIdHigh = 0x0000; CAN1_Filter.FilterMaskIdLow = 0x0000; CAN1_Filter.FilterFIFOAssignment = CAN_RX_FIFO0; CAN1_Filter.FilterActivation = ENABLE; CAN1_Filter.SlaveStartFilterBank = 14; if (HAL_CAN_ConfigFilter(&hcan1, &CAN1_Filter) != HAL_OK) { Error_Handler(); } if (HAL_CAN_ActivateNotification( &hcan1, CAN_IT_RX_FIFO0_MSG_PENDING | CAN_IT_TX_MAILBOX_EMPTY | CAN_IT_ERROR ) != HAL_OK) { Error_Handler(); } if (HAL_CAN_Start(&hcan1) != HAL_OK) { Error_Handler(); } /* USER CODE END CAN1_Init 2 */ } /** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOB_CLK_ENABLE(); __HAL_RCC_GPIOD_CLK_ENABLE(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOB, LED1_Pin|LED2_Pin, GPIO_PIN_RESET); /*Configure GPIO pins : LED1_Pin LED2_Pin */ GPIO_InitStruct.Pin = LED1_Pin|LED2_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_PULLDOWN; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); } /* USER CODE BEGIN 4 */ /** * @brief Rx Fifo 0 message pending callback * @param hcan: pointer to a CAN_HandleTypeDef structure that contains * the configuration information for the specified CAN. * @retval None */ void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan) { // currently not used as we use polling for test purposes led1_on(); } static void led1_on(void) { HAL_GPIO_WritePin(GPIOB, LED1_Pin, GPIO_PIN_SET); } static void led1_off(void) { HAL_GPIO_WritePin(GPIOB, LED1_Pin, GPIO_PIN_RESET); } static void led2_on(void) { HAL_GPIO_WritePin(GPIOB, LED2_Pin, GPIO_PIN_SET); } static void led2_off(void) { HAL_GPIO_WritePin(GPIOB, LED2_Pin, GPIO_PIN_RESET); } /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { led2_on(); } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */