/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2024 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ uint8_t mode1 = 0; uint8_t mode2 = 0; uint8_t mode3 = 0; uint8_t mode4 = 0; /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ I2C_HandleTypeDef hi2c1; /* USER CODE BEGIN PV */ /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_I2C1_Init(void); /* USER CODE BEGIN PFP */ uint8_t val = 0; /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ uint8_t dataWrite[4]; uint8_t dataRead[4]; uint8_t dataR[4]; /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_I2C1_Init(); /* USER CODE BEGIN 2 */ dataWrite[0] = 1; dataWrite[1] = 0; dataWrite[2] = 0; dataWrite[3] = 1; // write_ext_eeprom((3<<6), temp); // val_ = read_ext_eeprom((3<<6)); HAL_Delay(20); uint8_t output = HAL_I2C_Mem_Write(&hi2c1, 0xA0, (3 << 6), 4, dataWrite, 4, 1000); if (output == HAL_ERROR) { output = 10; } HAL_Delay(20); output = HAL_I2C_Mem_Read(&hi2c1, 0xA0, (3 << 6), 4, dataRead, 4, 1000); if (output == HAL_ERROR) { output = 10; } /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ mode1 = 1; dataWrite[0] = mode1; HAL_I2C_Mem_Write(&hi2c1, 0xA0, (3 << 6), 4, dataWrite, 4, 20); HAL_Delay(10); HAL_I2C_Mem_Read(&hi2c1, 0xA0, (3 << 6), 4, dataRead, 4, 20); HAL_Delay(10); dataR[0] = dataRead[0]; dataR[1] = dataRead[1]; dataR[2] = dataRead[2]; dataR[3] = dataRead[3]; HAL_Delay(1000); mode2 = 1; dataWrite[1] = mode2; HAL_I2C_Mem_Write(&hi2c1, 0xA0, (3 << 6), 4, dataWrite, 4, 20); HAL_Delay(10); HAL_I2C_Mem_Read(&hi2c1, 0xA0, (3 << 6), 4, dataRead, 4, 20); HAL_Delay(10); dataR[0] = dataRead[0]; dataR[1] = dataRead[1]; dataR[2] = dataRead[2]; dataR[3] = dataRead[3]; HAL_Delay(1000); mode3 = 1; dataWrite[2] = mode3; HAL_I2C_Mem_Write(&hi2c1, 0xA0, (3 << 6), 4, dataWrite, 4, 20); HAL_Delay(10); HAL_I2C_Mem_Read(&hi2c1, 0xA0, (3 << 6), 4, dataRead, 4, 20); HAL_Delay(10); dataR[0] = dataRead[0]; dataR[1] = dataRead[1]; dataR[2] = dataRead[2]; dataR[3] = dataRead[3]; HAL_Delay(1000); mode4 = 1; dataWrite[3] = mode4; HAL_I2C_Mem_Write(&hi2c1, 0xA0, (3 << 6), 4, dataWrite, 4, 20); HAL_Delay(10); HAL_I2C_Mem_Read(&hi2c1, 0xA0, (3 << 6), 4, dataRead, 4, 20); HAL_Delay(10); dataR[0] = dataRead[0]; dataR[1] = dataRead[1]; dataR[2] = dataRead[2]; dataR[3] = dataRead[3]; HAL_Delay(1000); mode1 = 0; dataWrite[0] = mode1; HAL_I2C_Mem_Write(&hi2c1, 0xA0, (3 << 6), 4, dataWrite, 4, 20); HAL_Delay(10); HAL_I2C_Mem_Read(&hi2c1, 0xA0, (3 << 6), 4, dataRead, 4, 20); HAL_Delay(10); dataR[0] = dataRead[0]; dataR[1] = dataRead[1]; dataR[2] = dataRead[2]; dataR[3] = dataRead[3]; HAL_Delay(1000); mode2 = 0; dataWrite[1] = mode2; HAL_I2C_Mem_Write(&hi2c1, 0xA0, (3 << 6), 4, dataWrite, 4, 20); HAL_Delay(10); HAL_I2C_Mem_Read(&hi2c1, 0xA0, (3 << 6), 4, dataRead, 4, 20); HAL_Delay(10); dataR[0] = dataRead[0]; dataR[1] = dataRead[1]; dataR[2] = dataRead[2]; dataR[3] = dataRead[3]; HAL_Delay(1000); mode3 = 0; dataWrite[2] = mode3; HAL_I2C_Mem_Write(&hi2c1, 0xA0, (3 << 6), 4, dataWrite, 4, 20); HAL_Delay(10); HAL_I2C_Mem_Read(&hi2c1, 0xA0, (3 << 6), 4, dataRead, 4, 20); HAL_Delay(10); dataR[0] = dataRead[0]; dataR[1] = dataRead[1]; dataR[2] = dataRead[2]; dataR[3] = dataRead[3]; HAL_Delay(1000); mode4 = 0; dataWrite[3] = mode4; HAL_I2C_Mem_Write(&hi2c1, 0xA0, (3 << 6), 4, dataWrite, 4, 20); HAL_Delay(10); HAL_I2C_Mem_Read(&hi2c1, 0xA0, (3 << 6), 4, dataRead, 4, 20); HAL_Delay(10); dataR[0] = dataRead[0]; dataR[1] = dataRead[1]; dataR[2] = dataRead[2]; dataR[3] = dataRead[3]; HAL_Delay(1000); } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV4; RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI; RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK) { Error_Handler(); } } /** * @brief I2C1 Initialization Function * @param None * @retval None */ static void MX_I2C1_Init(void) { /* USER CODE BEGIN I2C1_Init 0 */ /* USER CODE END I2C1_Init 0 */ /* USER CODE BEGIN I2C1_Init 1 */ /* USER CODE END I2C1_Init 1 */ hi2c1.Instance = I2C1; hi2c1.Init.Timing = 0x40000A0B; hi2c1.Init.OwnAddress1 = 0; hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT; hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE; hi2c1.Init.OwnAddress2 = 0; hi2c1.Init.OwnAddress2Masks = I2C_OA2_NOMASK; hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE; hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE; if (HAL_I2C_Init(&hi2c1) != HAL_OK) { Error_Handler(); } /** Configure Analogue filter */ if (HAL_I2CEx_ConfigAnalogFilter(&hi2c1, I2C_ANALOGFILTER_ENABLE) != HAL_OK) { Error_Handler(); } /** Configure Digital filter */ if (HAL_I2CEx_ConfigDigitalFilter(&hi2c1, 0) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN I2C1_Init 2 */ /* USER CODE END I2C1_Init 2 */ } /** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { /* USER CODE BEGIN MX_GPIO_Init_1 */ /* USER CODE END MX_GPIO_Init_1 */ /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOB_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); /* USER CODE BEGIN MX_GPIO_Init_2 */ /* USER CODE END MX_GPIO_Init_2 */ } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */