/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2023 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ /* USER CODE BEGIN PV */ /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ void LCD_ToggleEnable(){ /* Write the Data */ HAL_GPIO_WritePin(GPIOA, E_Pin, GPIO_PIN_SET); HAL_GPIO_WritePin(GPIOA, LED_PA4_Pin, GPIO_PIN_SET); HAL_Delay(3); /* 3ms delay should be enough for any instruction to execute, longest instruction is Clear Display (1.52ms) */ HAL_GPIO_WritePin(GPIOA, E_Pin, GPIO_PIN_RESET); HAL_GPIO_WritePin(GPIOA, LED_PA4_Pin, GPIO_PIN_RESET); HAL_Delay(3); } void Nibble(uint8_t cmd) { //0x#0 ===> the second nibble with always be ignored /* Set Data Pins (UPPER NIBBLE) * Written like this so can easily make compatible with 8-bit in future*/ HAL_GPIO_WritePin(GPIOA, DB7_Pin, 0x80&cmd); //extracts 1000 0000 HAL_GPIO_WritePin(GPIOA, DB6_Pin, 0x40&cmd); //extracts 0100 0000 HAL_GPIO_WritePin(GPIOA, DB5_Pin, 0x20&cmd); //extracts 0010 0000 HAL_GPIO_WritePin(GPIOA, DB4_Pin, 0x10&cmd); //extracts 0001 0000 /* Set Registry Pins */ LCD_ToggleEnable(); } /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); /* USER CODE BEGIN 2 */ //Will put these into a function later, for a start we will send commands //These details were taken from the ST7066U manual page 25 HAL_Delay(500); // HAL_GPIO_WritePin(GPIOA, RW_Pin, GPIO_PIN_RESET); //Write to registers HAL_GPIO_WritePin(GPIOA, RS_Pin, GPIO_PIN_RESET); //command registry //Function Set Nibble(0x30); //4-bit mode //Function set again 0x28 will be for a 2-line display and 5x8 character Nibble(0x28); //Write the upper nibble //Write the lower nibble after a bit shift left by 4 Nibble(0x28<<4); //Function set again 0x28 will be for a 2-line display and 5x8 character Nibble(0x28); //Write the upper nibble //Write the lower nibble after a bit shift left by 4 Nibble(0x28<<4); //Display ON, Cursor ON, Blinking ON Nibble(0x0F); //Write the upper nibble //Write the lower nibble after a bit shift left by 4 Nibble(0x0F<<4); //Clear Display Nibble(0x01); //Write the upper nibble //Write the lower nibble after a bit shift left by 4 Nibble(0x01<<4); //Increment cursor but don't shift display Nibble(0x06); //Write the upper nibble //Write the lower nibble after a bit shift left by 4 Nibble(0x06<<4); //SETUP IS NOW COMPLETE ACCORDING TO MANUAL //Now write to data registers HAL_GPIO_WritePin(GPIOA, RS_Pin, GPIO_PIN_SET); //command registry //Write an A Nibble(0x41); //Write the upper nibble //Write the lower nibble after a bit shift left by 4 Nibble(0x41<<4); /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK) { Error_Handler(); } } /** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* USER CODE BEGIN MX_GPIO_Init_1 */ /* USER CODE END MX_GPIO_Init_1 */ /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOA, DB4_Pin|E_Pin|RW_Pin|RS_Pin |LED_PA4_Pin|DB5_Pin|DB6_Pin|DB7_Pin, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(LED_GPIO_Port, LED_Pin, GPIO_PIN_RESET); /*Configure GPIO pins : DB4_Pin E_Pin RW_Pin RS_Pin LED_PA4_Pin DB5_Pin DB6_Pin DB7_Pin */ GPIO_InitStruct.Pin = DB4_Pin|E_Pin|RW_Pin|RS_Pin |LED_PA4_Pin|DB5_Pin|DB6_Pin|DB7_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /*Configure GPIO pin : LED_Pin */ GPIO_InitStruct.Pin = LED_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(LED_GPIO_Port, &GPIO_InitStruct); /* USER CODE BEGIN MX_GPIO_Init_2 */ /* USER CODE END MX_GPIO_Init_2 */ } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */