/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file dma.c * @brief This file provides code for the configuration * of all the requested memory to memory DMA transfers. ****************************************************************************** * @attention * * Copyright (c) 2024 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "dma.h" /* USER CODE BEGIN 0 */ /* USER CODE END 0 */ /*----------------------------------------------------------------------------*/ /* Configure DMA */ /*----------------------------------------------------------------------------*/ /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /** * Enable DMA controller clock */ void MX_DMA_Init(void) { /* DMA controller clock enable */ __HAL_RCC_DMA1_CLK_ENABLE(); /* DMA interrupt init */ /* DMA1_Channel1_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn); } /* USER CODE BEGIN 2 */ /* USER CODE END 2 */