/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2024 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" #include /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ FDCAN_HandleTypeDef hfdcan1; UART_HandleTypeDef huart1; /* USER CODE BEGIN PV */ static GPIO_InitTypeDef GPIO_InitStruct; /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_USART1_UART_Init(void); static void MX_FDCAN1_Init(void); /* USER CODE BEGIN PFP */ FDCAN_TxHeaderTypeDef TxHeader; uint8_t TxData0[] = { 1, 2, 3, 4, 5, 6, 7, 8 }; /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ static void dump_msg(const char* msg) { HAL_UART_Transmit( &huart1, (const uint8_t*)msg, strlen( msg ), 1000 ); } static void CAN_TX( void ) { TxHeader.Identifier = 0x444; TxHeader.IdType = FDCAN_STANDARD_ID; TxHeader.TxFrameType = FDCAN_DATA_FRAME; TxHeader.DataLength = FDCAN_DLC_BYTES_12; TxHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE; TxHeader.BitRateSwitch = FDCAN_BRS_ON; TxHeader.FDFormat = FDCAN_FD_CAN; TxHeader.TxEventFifoControl = FDCAN_STORE_TX_EVENTS; TxHeader.MessageMarker = 0x52; if (HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &TxHeader, TxData0) != HAL_OK) { dump_msg( "error from HAL_FDCAN_AddMessageToTxFifoQ\r\n" ); //Error_Handler(); } else { dump_msg( "CAN_TX: successful add to FIF0\n" ); } } /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_USART1_UART_Init(); MX_FDCAN1_Init(); /* USER CODE BEGIN 2 */ HAL_FDCAN_Start(&hfdcan1); /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ dump_msg( "hello!\r\n" ); CAN_TX(); HAL_Delay( 1000 ); } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Configure the main internal regulator output voltage */ if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE3) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI; RCC_OscInitStruct.MSIState = RCC_MSI_ON; RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT; RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_0; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI; RCC_OscInitStruct.PLL.PLLMBOOST = RCC_PLLMBOOST_DIV4; RCC_OscInitStruct.PLL.PLLM = 3; RCC_OscInitStruct.PLL.PLLN = 8; RCC_OscInitStruct.PLL.PLLP = 2; RCC_OscInitStruct.PLL.PLLQ = 1; RCC_OscInitStruct.PLL.PLLR = 2; RCC_OscInitStruct.PLL.PLLRGE = RCC_PLLVCIRANGE_1; RCC_OscInitStruct.PLL.PLLFRACN = 0; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2 |RCC_CLOCKTYPE_PCLK3; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK) { Error_Handler(); } } /** * @brief FDCAN1 Initialization Function * @param None * @retval None */ static void MX_FDCAN1_Init(void) { /* USER CODE BEGIN FDCAN1_Init 0 */ /* USER CODE END FDCAN1_Init 0 */ /* USER CODE BEGIN FDCAN1_Init 1 */ /* USER CODE END FDCAN1_Init 1 */ hfdcan1.Instance = FDCAN1; hfdcan1.Init.ClockDivider = FDCAN_CLOCK_DIV1; hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC; hfdcan1.Init.Mode = FDCAN_MODE_NORMAL; hfdcan1.Init.AutoRetransmission = DISABLE; hfdcan1.Init.TransmitPause = DISABLE; hfdcan1.Init.ProtocolException = DISABLE; hfdcan1.Init.NominalPrescaler = 16; hfdcan1.Init.NominalSyncJumpWidth = 1; // 24? hfdcan1.Init.NominalTimeSeg1 = 2; // 135? hfdcan1.Init.NominalTimeSeg2 = 2; // 24? hfdcan1.Init.DataPrescaler = 1; hfdcan1.Init.DataSyncJumpWidth = 1; hfdcan1.Init.DataTimeSeg1 = 1; hfdcan1.Init.DataTimeSeg2 = 1; hfdcan1.Init.StdFiltersNbr = 0; hfdcan1.Init.ExtFiltersNbr = 0; hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION; #if 0 hfdcan1.Init.MessageRAMOffset = 0; hfdcan1.Init.StdFiltersNbr = 10; hfdcan1.Init.ExtFiltersNbr = 0; hfdcan1.Init.RxFifo0ElmtsNbr = 10; hfdcan1.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_8; hfdcan1.Init.RxFifo1ElmtsNbr = 0; hfdcan1.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8; hfdcan1.Init.RxBuffersNbr = 10; hfdcan1.Init.RxBufferSize = FDCAN_DATA_BYTES_8; hfdcan1.Init.TxEventsNbr = 0; hfdcan1.Init.TxBuffersNbr = 10; hfdcan1.Init.TxFifoQueueElmtsNbr = 10; hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION; hfdcan1.Init.TxElmtSize = FDCAN_DATA_BYTES_8; #endif if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN FDCAN1_Init 2 */ /* USER CODE END FDCAN1_Init 2 */ } /** * @brief USART1 Initialization Function * @param None * @retval None */ static void MX_USART1_UART_Init(void) { /* USER CODE BEGIN USART1_Init 0 */ /* USER CODE END USART1_Init 0 */ /* USER CODE BEGIN USART1_Init 1 */ /* USER CODE END USART1_Init 1 */ huart1.Instance = USART1; huart1.Init.BaudRate = 115200; huart1.Init.WordLength = UART_WORDLENGTH_8B; huart1.Init.StopBits = UART_STOPBITS_1; huart1.Init.Parity = UART_PARITY_NONE; huart1.Init.Mode = UART_MODE_TX_RX; huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart1.Init.OverSampling = UART_OVERSAMPLING_16; huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; huart1.Init.ClockPrescaler = UART_PRESCALER_DIV1; huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; if (HAL_UART_Init(&huart1) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_SetTxFifoThreshold(&huart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_SetRxFifoThreshold(&huart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_DisableFifoMode(&huart1) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN USART1_Init 2 */ /* USER CODE END USART1_Init 2 */ } /** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { /* USER CODE BEGIN MX_GPIO_Init_1 */ /* USER CODE END MX_GPIO_Init_1 */ /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOA_CLK_ENABLE(); /* USER CODE BEGIN MX_GPIO_Init_2 */ GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; GPIO_InitStruct.Pin = GPIO_PIN_0; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0, GPIO_PIN_SET ); /* USER CODE END MX_GPIO_Init_2 */ } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */