/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2023 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ #include #include #include #include "ov5640.h" //#include "modified_resized_image_data.h" /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ DCMI_HandleTypeDef hdcmi; DMA_HandleTypeDef hdma_dcmi; UART_HandleTypeDef hlpuart1; DMA_HandleTypeDef hdma_lpuart_tx; /* USER CODE BEGIN PV */ #define RES160X120 //#define RES320X240 //#define RES640X480 //#define RES800x600 //#define RES1024x768 //#define RES1280x960 #ifdef RES160X120 enum imageResolution imgRes=RES_160X120; uint8_t frameBuffer[RES_160X120] = { 0 }; #endif #ifdef RES320X240 enum imageResolution imgRes=RES_320X240; uint8_t frameBuffer[RES_320X240] = { 0 }; #endif #ifdef RES640X480 enum imageResolution imgRes=RES_640X480; uint8_t frameBuffer[RES_640X480] = { 0 }; #endif #ifdef RES800x600 enum imageResolution imgRes=RES_800x600; uint8_t frameBuffer[RES_800x600] = { 0 }; #endif #ifdef RES1024x768 enum imageResolution imgRes=RES_1024x768; uint8_t frameBuffer[RES_1024x768] = { 0 }; #endif #ifdef RES1280x960 enum imageResolution imgRes = RES_1280x960; uint8_t frameBuffer[RES_1280x960] = { 0 }; #endif short mutex = 0; uint16_t bufferPointer = 0; short headerFound = 0; uint8_t rx_buffer[64]; /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_DMA_Init(void); static void MX_DCMI_Init(void); static void MX_LPUART1_UART_Init(void); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ void send_hex_array_over_uart(const uint8_t* data, size_t size) { for (size_t i = 0; i < size; ++i) { char hex_string[3]; // 2 Zeichen für das Byte und 1 für '\0' snprintf(hex_string, sizeof(hex_string), "%02X", data[i]); HAL_UART_Transmit(&hlpuart1, (uint8_t*)hex_string, sizeof(hex_string) - 1, HAL_MAX_DELAY); // Senden Sie den Hex-String ohne das Null-Terminierungszeichen } } void vprint(const char *fmt, va_list argp) { char string[200]; if (0 < vsprintf(string, fmt, argp)) // build string { HAL_UART_Transmit(&hlpuart1, (uint8_t*) string, strlen(string), 0xffffff); // send message via UART } } void my_printf(const char *fmt, ...) // custom printf() function { va_list argp; va_start(argp, fmt); vprint(fmt, argp); va_end(argp); } void validateJpegInFramebuffer() { int startFound = 0; int endFound = 0; int jpegSize = 0; int startInt = 0; int endInt = 0; // Überprüfen, ob das Ende des JPEG-Bildes vorhanden ist for (int i = 0; i < 65536 - 1; i++) { if (frameBuffer[i] == 0xFF && frameBuffer[i + 1] == 0xD8) { startInt = i; startFound = 1; break; } if (frameBuffer[i] == 0xFF && frameBuffer[i + 1] == 0xD9) { endInt = i; endFound = 1; jpegSize = i + 2; break; } } if (startFound && endFound) { printf("\nJPEG validiert, Grösse: %d Bytes\n", jpegSize); } else { printf("\nJPEG nicht validiert\n"); if(startFound == 0){ printf("Header nicht gefunden\n"); } else { printf("End nicht gefunden\n"); } } printf("Start: %d\n", startInt); printf("Ende: %d\n", endInt); printf("Start gefunden: %d\n", startFound); printf("Ende gefunden: %d\n", endFound); } #ifdef __GNUC__ #define PUTCHAR_PROTOTYPE int __io_putchar(int ch) #else #define PUTCHAR_PROTOTYPE int fputc(int ch, FILE *f) #endif PUTCHAR_PROTOTYPE { HAL_UART_Transmit(&hlpuart1, (uint8_t *)&ch, 1, HAL_MAX_DELAY); return ch; } /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ #ifdef DEBUG my_printf("Start configuration \r\n"); #endif /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_DMA_Init(); MX_DCMI_Init(); MX_LPUART1_UART_Init(); /* USER CODE BEGIN 2 */ /* OV2640_Init(&hi2c1, &hdcmi); HAL_Delay(10); OV2640_ResolutionOptions(imgRes); HAL_Delay(10); */ HAL_Delay(10); printf("Initializing, please wait ...\r\n"); while(OV5640_Init()) { HAL_Delay(500); printf("OV5640 Initialization error, please check !\r\n"); } /** * Extra options */ OV5640_Light_Mode(0); //set auto OV5640_Color_Saturation(3); //default OV5640_Brightness(4); //default OV5640_Contrast(3); //default OV5640_Sharpness(33); //set auto #ifdef DEBUG my_printf("Finishing configuration \r\n"); #endif printf("Waveshare OV5640 Test \r\n"); printf("press Button to send JPEG to UART port \r\n"); int takePhoto = 1; /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { if (HAL_GPIO_ReadPin(USER_Btn_GPIO_Port, USER_Btn_Pin)) { printf("Lets go\r\n"); HAL_Delay(2000); int headerInt = 0; int endInt = 0; if (mutex == 1) { memset(frameBuffer, 0, sizeof frameBuffer); //OV2640_CaptureSnapshot((uint32_t) frameBuffer, imgRes); jpeg_test((uint32_t) frameBuffer, QVGA_320_240); while (1) { if (headerFound == 0 && frameBuffer[bufferPointer] == 0xFF && frameBuffer[bufferPointer + 1] == 0xD8) { headerFound = 1; headerInt = bufferPointer; #ifdef DEBUG my_printf("Found header of JPEG file \r\n"); #endif } if (headerFound == 1 && frameBuffer[bufferPointer] == 0xFF && frameBuffer[bufferPointer + 1] == 0xD9) { bufferPointer = bufferPointer + 2; #ifdef DEBUG my_printf("Found end of JPEG file \r\n"); #endif headerFound = 0; endInt = bufferPointer; break; } if (bufferPointer >= 65535) { printf("Error: Image size too large \r\n"); break; } bufferPointer++; } #ifdef DEBUG my_printf("Image size: %d bytes \r\n",bufferPointer); #endif HAL_Delay(2000); HAL_UART_Transmit(&hlpuart1, frameBuffer, bufferPointer, HAL_MAX_DELAY); //HAL_UART_Transmit_DMA(&hlpuart1, frameBuffer, bufferPointer); //Use of DMA may be necessary for larger data streams. HAL_Delay(2000); bufferPointer = 0; mutex = 0; validateJpegInFramebuffer(); printf("Databurst, Header: %d\n", headerInt); printf("Databurst, End: %d\n", headerInt); printf("Abgeschlossen \r\n"); } takePhoto = 0; } else { mutex = 1; } /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Configure the main internal regulator output voltage */ if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK) { Error_Handler(); } /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI; RCC_OscInitStruct.MSIState = RCC_MSI_ON; RCC_OscInitStruct.MSICalibrationValue = 0; RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI; RCC_OscInitStruct.PLL.PLLM = 1; RCC_OscInitStruct.PLL.PLLN = 24; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2; RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK) { Error_Handler(); } HAL_RCC_MCOConfig(RCC_MCO1, RCC_MCO1SOURCE_PLLCLK, RCC_MCODIV_2); } /** * @brief DCMI Initialization Function * @param None * @retval None */ static void MX_DCMI_Init(void) { /* USER CODE BEGIN DCMI_Init 0 */ /* USER CODE END DCMI_Init 0 */ /* USER CODE BEGIN DCMI_Init 1 */ /* USER CODE END DCMI_Init 1 */ hdcmi.Instance = DCMI; hdcmi.Init.SynchroMode = DCMI_SYNCHRO_HARDWARE; hdcmi.Init.PCKPolarity = DCMI_PCKPOLARITY_RISING; hdcmi.Init.VSPolarity = DCMI_VSPOLARITY_LOW; hdcmi.Init.HSPolarity = DCMI_HSPOLARITY_LOW; hdcmi.Init.CaptureRate = DCMI_CR_ALL_FRAME; hdcmi.Init.ExtendedDataMode = DCMI_EXTEND_DATA_8B; hdcmi.Init.JPEGMode = DCMI_JPEG_ENABLE; hdcmi.Init.ByteSelectMode = DCMI_BSM_ALL; hdcmi.Init.ByteSelectStart = DCMI_OEBS_ODD; hdcmi.Init.LineSelectMode = DCMI_LSM_ALL; hdcmi.Init.LineSelectStart = DCMI_OELS_ODD; if (HAL_DCMI_Init(&hdcmi) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN DCMI_Init 2 */ /* USER CODE END DCMI_Init 2 */ } /** * @brief LPUART1 Initialization Function * @param None * @retval None */ static void MX_LPUART1_UART_Init(void) { /* USER CODE BEGIN LPUART1_Init 0 */ /* USER CODE END LPUART1_Init 0 */ /* USER CODE BEGIN LPUART1_Init 1 */ /* USER CODE END LPUART1_Init 1 */ hlpuart1.Instance = LPUART1; hlpuart1.Init.BaudRate = 115200; hlpuart1.Init.WordLength = UART_WORDLENGTH_8B; hlpuart1.Init.StopBits = UART_STOPBITS_1; hlpuart1.Init.Parity = UART_PARITY_NONE; hlpuart1.Init.Mode = UART_MODE_TX_RX; hlpuart1.Init.HwFlowCtl = UART_HWCONTROL_NONE; hlpuart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; hlpuart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; if (HAL_UART_Init(&hlpuart1) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN LPUART1_Init 2 */ /* USER CODE END LPUART1_Init 2 */ } /** * Enable DMA controller clock */ static void MX_DMA_Init(void) { /* DMA controller clock enable */ __HAL_RCC_DMA2_CLK_ENABLE(); /* DMA interrupt init */ /* DMA2_Channel5_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA2_Channel5_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA2_Channel5_IRQn); /* DMA2_Channel6_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA2_Channel6_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA2_Channel6_IRQn); } /** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* USER CODE BEGIN MX_GPIO_Init_1 */ /* USER CODE END MX_GPIO_Init_1 */ /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOE_CLK_ENABLE(); __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOH_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); __HAL_RCC_GPIOG_CLK_ENABLE(); HAL_PWREx_EnableVddIO2(); __HAL_RCC_GPIOD_CLK_ENABLE(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOB, LED1_Pin|LED3_Pin|LED2_Pin, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(OV5640_PWDN_GPIO_Port, OV5640_PWDN_Pin, GPIO_PIN_SET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(USB_PowerSwitchOn_GPIO_Port, USB_PowerSwitchOn_Pin, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOB, OV5640_SIOC_Pin|OV5640_SIOD_Pin, GPIO_PIN_SET); /*Configure GPIO pin : USER_Btn_Pin */ GPIO_InitStruct.Pin = USER_Btn_Pin; GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(USER_Btn_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pins : LED1_Pin LED3_Pin LED2_Pin */ GPIO_InitStruct.Pin = LED1_Pin|LED3_Pin|LED2_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); /*Configure GPIO pin : WAKE_UP_KEY_Pin */ GPIO_InitStruct.Pin = WAKE_UP_KEY_Pin; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_PULLUP; HAL_GPIO_Init(WAKE_UP_KEY_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pins : OV5640_PWDN_Pin USB_PowerSwitchOn_Pin */ GPIO_InitStruct.Pin = OV5640_PWDN_Pin|USB_PowerSwitchOn_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOG, &GPIO_InitStruct); /*Configure GPIO pin : DCMI_XCLK_Pin */ GPIO_InitStruct.Pin = DCMI_XCLK_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; GPIO_InitStruct.Alternate = GPIO_AF0_MCO; HAL_GPIO_Init(DCMI_XCLK_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pins : OV5640_SIOC_Pin OV5640_SIOD_Pin */ GPIO_InitStruct.Pin = OV5640_SIOC_Pin|OV5640_SIOD_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_OD; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); /* USER CODE BEGIN MX_GPIO_Init_2 */ /* USER CODE END MX_GPIO_Init_2 */ } /* USER CODE BEGIN 4 */ void debugPrint(UART_HandleTypeDef *huart, char _out[]){ //HAL_StatusTypeDef HAL_RESULT; HAL_UART_Transmit(huart, (uint8_t *) _out, strlen(_out), 10); asm("nop"); //HAL_UART_Transmit_IT(&huart2,(uint8_t *) _out, strlen(_out)); } //ProteusIII Funktion delay auf HAL_Delay umleiten void delay(unsigned int sleepFor) { HAL_Delay(sleepFor); } /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */