#include "main.h" #include "linked_list.h" ADC_HandleTypeDef hadc1; DMA_HandleTypeDef handle_GPDMA1_Channel5; extern DMA_QListTypeDef Queue; /* USER CODE BEGIN PV */ extern uint32_t aSRC_Buffer1; extern uint32_t aDST_Buffer1[4]; /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_GPDMA1_Init(void); static void MX_ADC1_Init(void); static void MX_ICACHE_Init(void); static void TransferComplete(DMA_HandleTypeDef *hdma); static void TransferError(DMA_HandleTypeDef *hdma); /* USER CODE BEGIN PFP */ __IO uint32_t TransferCompleteDetected = 0U, TransferErrorDetected = 0U; /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_GPDMA1_Init(); MX_ADC1_Init(); MX_ICACHE_Init(); /* USER CODE BEGIN 2 */ MX_Queue_Config(); if (HAL_DMAEx_List_LinkQ(&handle_GPDMA1_Channel5, &Queue) != HAL_OK) { Error_Handler(); } HAL_DMA_RegisterCallback(&handle_GPDMA1_Channel5, HAL_DMA_XFER_CPLT_CB_ID, TransferComplete); HAL_DMA_RegisterCallback(&handle_GPDMA1_Channel5, HAL_DMA_XFER_ERROR_CB_ID, TransferError); /* Enable All the DMA interrupts */ /*if (HAL_DMAEx_List_Start_IT(&handle_GPDMA1_Channel5) != HAL_OK) { Error_Handler(); }*/ HAL_ADC_Start_DMA(&hadc1, &aDST_Buffer1, 4); /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { aSRC_Buffer1++; HAL_Delay(500); /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Configure the main internal regulator output voltage */ __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0); while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {} /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS_DIGITAL; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLL1_SOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = 4; RCC_OscInitStruct.PLL.PLLN = 250; RCC_OscInitStruct.PLL.PLLP = 2; RCC_OscInitStruct.PLL.PLLQ = 2; RCC_OscInitStruct.PLL.PLLR = 2; RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1_VCIRANGE_1; RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1_VCORANGE_WIDE; RCC_OscInitStruct.PLL.PLLFRACN = 0; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2 |RCC_CLOCKTYPE_PCLK3; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK) { Error_Handler(); } } /** * @brief ADC1 Initialization Function * @param None * @retval None */ static void MX_ADC1_Init(void) { ADC_ChannelConfTypeDef sConfig = {0}; /** Common config */ hadc1.Instance = ADC1; hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV2; hadc1.Init.Resolution = ADC_RESOLUTION_12B; hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE; hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV; hadc1.Init.LowPowerAutoWait = DISABLE; hadc1.Init.ContinuousConvMode = ENABLE; hadc1.Init.NbrOfConversion = 2; hadc1.Init.DiscontinuousConvMode = DISABLE; hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START; hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; hadc1.Init.DMAContinuousRequests = ENABLE; hadc1.Init.SamplingMode = ADC_SAMPLING_MODE_NORMAL; hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED; hadc1.Init.OversamplingMode = DISABLE; hadc1.DMA_Handle = &handle_GPDMA1_Channel5; if (HAL_ADC_Init(&hadc1) != HAL_OK) { Error_Handler(); } /** Configure Regular Channel */ sConfig.Channel = ADC_CHANNEL_3; sConfig.Rank = ADC_REGULAR_RANK_1; sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5; sConfig.SingleDiff = ADC_SINGLE_ENDED; sConfig.OffsetNumber = ADC_OFFSET_NONE; sConfig.Offset = 0; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } /** Configure Regular Channel */ sConfig.Channel = ADC_CHANNEL_10; sConfig.Rank = ADC_REGULAR_RANK_2; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } } /** * @brief GPDMA1 Initialization Function * @param None * @retval None */ static void MX_GPDMA1_Init(void) { /* USER CODE BEGIN GPDMA1_Init 0 */ /* USER CODE END GPDMA1_Init 0 */ /* Peripheral clock enable */ __HAL_RCC_GPDMA1_CLK_ENABLE(); /* USER CODE BEGIN GPDMA1_Init 1 */ /* USER CODE END GPDMA1_Init 1 */ handle_GPDMA1_Channel5.Instance = GPDMA1_Channel5; handle_GPDMA1_Channel5.InitLinkedList.Priority = DMA_HIGH_PRIORITY; handle_GPDMA1_Channel5.InitLinkedList.LinkStepMode = DMA_LSM_FULL_EXECUTION; handle_GPDMA1_Channel5.InitLinkedList.LinkAllocatedPort = DMA_LINK_ALLOCATED_PORT0; handle_GPDMA1_Channel5.InitLinkedList.TransferEventMode = DMA_TCEM_EACH_LL_ITEM_TRANSFER; handle_GPDMA1_Channel5.InitLinkedList.LinkedListMode = DMA_LINKEDLIST_CIRCULAR; if (HAL_DMAEx_List_Init(&handle_GPDMA1_Channel5) != HAL_OK) { Error_Handler(); } if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel5, DMA_CHANNEL_NPRIV) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN GPDMA1_Init 2 */ /* USER CODE END GPDMA1_Init 2 */ } /** * @brief ICACHE Initialization Function * @param None * @retval None */ static void MX_ICACHE_Init(void) { /* USER CODE BEGIN ICACHE_Init 0 */ /* USER CODE END ICACHE_Init 0 */ /* USER CODE BEGIN ICACHE_Init 1 */ /* USER CODE END ICACHE_Init 1 */ /** Enable instruction cache (default 2-ways set associative cache) */ if (HAL_ICACHE_Enable() != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN ICACHE_Init 2 */ /* USER CODE END ICACHE_Init 2 */ } /** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* USER CODE BEGIN MX_GPIO_Init_1 */ /* USER CODE END MX_GPIO_Init_1 */ /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOE_CLK_ENABLE(); __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOF_CLK_ENABLE(); __HAL_RCC_GPIOH_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); __HAL_RCC_GPIOD_CLK_ENABLE(); __HAL_RCC_GPIOG_CLK_ENABLE(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(LED2_YELLOW_GPIO_Port, LED2_YELLOW_Pin, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(LED1_GREEN_GPIO_Port, LED1_GREEN_Pin, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(LED3_RED_GPIO_Port, LED3_RED_Pin, GPIO_PIN_RESET); /*Configure GPIO pin : USER_BUTTON_Pin */ GPIO_InitStruct.Pin = USER_BUTTON_Pin; GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(USER_BUTTON_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pin : LED2_YELLOW_Pin */ GPIO_InitStruct.Pin = LED2_YELLOW_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(LED2_YELLOW_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pins : RMII_MDC_Pin RMII_RXD0_Pin RMII_RXD1_Pin */ GPIO_InitStruct.Pin = RMII_MDC_Pin|RMII_RXD0_Pin|RMII_RXD1_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; GPIO_InitStruct.Alternate = GPIO_AF11_ETH; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); /*Configure GPIO pins : RMII_REF_CLK_Pin RMII_MDIO_Pin RMII_CRS_DV_Pin */ GPIO_InitStruct.Pin = RMII_REF_CLK_Pin|RMII_MDIO_Pin|RMII_CRS_DV_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; GPIO_InitStruct.Alternate = GPIO_AF11_ETH; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /*Configure GPIO pin : LED1_GREEN_Pin */ GPIO_InitStruct.Pin = LED1_GREEN_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(LED1_GREEN_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pins : UCPD_CC1_Pin UCPD_CC2_Pin */ GPIO_InitStruct.Pin = UCPD_CC1_Pin|UCPD_CC2_Pin; GPIO_InitStruct.Mode = GPIO_MODE_ANALOG; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); /*Configure GPIO pin : RMII_TXD1_Pin */ GPIO_InitStruct.Pin = RMII_TXD1_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; GPIO_InitStruct.Alternate = GPIO_AF11_ETH; HAL_GPIO_Init(RMII_TXD1_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pins : T_VCP_TX_Pin T_VCP_RX_Pin */ GPIO_InitStruct.Pin = T_VCP_TX_Pin|T_VCP_RX_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; GPIO_InitStruct.Alternate = GPIO_AF7_USART3; HAL_GPIO_Init(GPIOD, &GPIO_InitStruct); /*Configure GPIO pin : LED3_RED_Pin */ GPIO_InitStruct.Pin = LED3_RED_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(LED3_RED_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pin : UCPD_FLT_Pin */ GPIO_InitStruct.Pin = UCPD_FLT_Pin; GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(UCPD_FLT_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pins : USB_FS_N_Pin USB_FS_P_Pin */ GPIO_InitStruct.Pin = USB_FS_N_Pin|USB_FS_P_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; GPIO_InitStruct.Alternate = GPIO_AF10_USB; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /*Configure GPIO pins : RMII_TXT_EN_Pin RMI_TXD0_Pin */ GPIO_InitStruct.Pin = RMII_TXT_EN_Pin|RMI_TXD0_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; GPIO_InitStruct.Alternate = GPIO_AF11_ETH; HAL_GPIO_Init(GPIOG, &GPIO_InitStruct); /*Configure GPIO pins : ARD_D1_TX_Pin ARD_D0_RX_Pin */ GPIO_InitStruct.Pin = ARD_D1_TX_Pin|ARD_D0_RX_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; GPIO_InitStruct.Alternate = GPIO_AF8_LPUART1; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); /* USER CODE BEGIN MX_GPIO_Init_2 */ /* USER CODE END MX_GPIO_Init_2 */ } /* USER CODE BEGIN 4 */ static void TransferComplete(DMA_HandleTypeDef *hdma) { TransferCompleteDetected = 1U; } /** * @brief DMA transfer error callback * @note This function is executed when the transfer error interrupt * is generated during DMA transfer * @retval None */ static void TransferError(DMA_HandleTypeDef *hdma) { TransferErrorDetected = 1U; } /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */