/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2023 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ #include "stdio.h" #include "string.h" /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ FDCAN_HandleTypeDef hfdcan1; UART_HandleTypeDef huart2; /* USER CODE BEGIN PV */ /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_USART2_UART_Init(void); static void MX_FDCAN1_Init(void); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ FDCAN_TxHeaderTypeDef TxHeader1; FDCAN_RxHeaderTypeDef RxHeader; uint8_t TxData[12]; uint8_t RxData[12]; uint8_t msg[25]; int datacheck; int indx = 0; void HAL_FDCAN_RxFifo0Callback(FDCAN_HandleTypeDef *hfdcan, uint32_t RxFifo0ITs) { if((RxFifo0ITs & FDCAN_IT_RX_FIFO0_NEW_MESSAGE) != RESET) { /* Retreive Rx messages from RX FIFO0 */ if (HAL_FDCAN_GetRxMessage(hfdcan, FDCAN_RX_FIFO0, &RxHeader, RxData) != HAL_OK) { /* Reception Error */ Error_Handler(); } if (HAL_FDCAN_ActivateNotification(hfdcan, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0) != HAL_OK) { /* Notification Error */ Error_Handler(); } } datacheck = 1; } /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_USART2_UART_Init(); MX_FDCAN1_Init(); /* USER CODE BEGIN 2 */ if(HAL_FDCAN_Start(&hfdcan1)!= HAL_OK) { Error_Handler(); } if (HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0) != HAL_OK) { /* Notification Error */ Error_Handler(); } TxHeader1.Identifier = 0x123; TxHeader1.IdType = FDCAN_STANDARD_ID; TxHeader1.TxFrameType = FDCAN_DATA_FRAME; TxHeader1.DataLength = FDCAN_DLC_BYTES_2; TxHeader1.ErrorStateIndicator = FDCAN_ESI_ACTIVE; TxHeader1.BitRateSwitch = FDCAN_BRS_OFF; TxHeader1.FDFormat = FDCAN_FD_CAN; TxHeader1.TxEventFifoControl = FDCAN_NO_TX_EVENTS; TxHeader1.MessageMarker = 0; /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ HAL_Delay (1000); if (datacheck) { TxData[0] =150; TxData[1] = 30; HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &TxHeader1, TxData); if (HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &TxHeader1, TxData)!= HAL_OK) { Error_Handler(); } for (int i=0; i