#include "main.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ #define SRC_BUF_SIZE 65472 //ADC buffer where ADC data is transfered by the DMA. #define XFR_SIZE 32736 //Size of each transmission from SRC_Buf to DST_Buf. #define DST_BUF_SIZE XFR_SIZE //3 x Size of SRC_Buf. Enough samples for a transaction of ~50 ms /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ ADC_HandleTypeDef hadc3; DMA_HandleTypeDef hdma_adc3; MDMA_HandleTypeDef hmdma_mdma_channel0_sw_0; MDMA_LinkNodeTypeDef node_mdma_channel0_sw_1; MDMA_LinkNodeTypeDef node_mdma_channel0_sw_2; MDMA_LinkNodeTypeDef node_mdma_channel0_sw_3; MDMA_LinkNodeTypeDef node_mdma_channel0_sw_4; MDMA_LinkNodeTypeDef node_mdma_channel0_sw_5; /* USER CODE BEGIN PV */ uint8_t SRC_Buf0[SRC_BUF_SIZE]; uint8_t DST_Buf0[DST_BUF_SIZE]; uint8_t DST_Buf1[DST_BUF_SIZE]; uint8_t DST_Buf2[DST_BUF_SIZE]; uint8_t DST_Buf3[DST_BUF_SIZE]; uint8_t DST_Buf4[DST_BUF_SIZE]; uint8_t DST_Buf5[DST_BUF_SIZE]; /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MPU_Initialize(void); static void MPU_Config(void); static void MX_MDMA_Init(void); static void MX_GPIO_Init(void); static void MX_DMA_Init(void); static void MX_ADC3_Init(void); /* USER CODE BEGIN PFP */ static void MDMA_TransferCompleteCallback(MDMA_HandleTypeDef *hmdma); static void MDMA_TransferErrorCallback(MDMA_HandleTypeDef *hmdma); static void MDMA_TransferBlockCompleteCallback(MDMA_HandleTypeDef *hmdma); /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ unsigned int j = 0; for(unsigned int i = 0; i < SRC_BUF_SIZE; i++){ SRC_Buf0[i] = j; j++; if(j >= 256){ j = 0; } } for(unsigned int i = 0; i < DST_BUF_SIZE; i++){ DST_Buf0[i] = 0; DST_Buf1[i] = 0; DST_Buf2[i] = 0; DST_Buf3[i] = 0; DST_Buf4[i] = 0; DST_Buf5[i] = 0; } __NOP(); /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* MPU Configuration--------------------------------------------------------*/ MPU_Config(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_MDMA_Init(); MX_GPIO_Init(); MX_DMA_Init(); MX_ADC3_Init(); /* USER CODE BEGIN 2 */ if (HAL_MDMA_Start_IT(&hmdma_mdma_channel0_sw_0, (uint32_t)&SRC_Buf0[XFR_SIZE], (uint32_t)&DST_Buf0, XFR_SIZE, 1) != HAL_OK) { __NOP(); } HAL_ADC_Start_DMA(&hadc3, (uint32_t*)SRC_Buf0, SRC_BUF_SIZE); /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Supply configuration update enable */ HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY); /** Configure the main internal regulator output voltage */ __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0); while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {} /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_DIV1; RCC_OscInitStruct.HSICalibrationValue = 64; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI; RCC_OscInitStruct.PLL.PLLM = 4; RCC_OscInitStruct.PLL.PLLN = 34; RCC_OscInitStruct.PLL.PLLP = 1; RCC_OscInitStruct.PLL.PLLQ = 2; RCC_OscInitStruct.PLL.PLLR = 2; RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3; RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE; RCC_OscInitStruct.PLL.PLLFRACN = 3072; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2 |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2; RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2; RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2; RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2; RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK) { Error_Handler(); } } /** * @brief ADC3 Initialization Function * @param None * @retval None */ static void MX_ADC3_Init(void) { /* USER CODE BEGIN ADC3_Init 0 */ /* USER CODE END ADC3_Init 0 */ ADC_ChannelConfTypeDef sConfig = {0}; /* USER CODE BEGIN ADC3_Init 1 */ /* USER CODE END ADC3_Init 1 */ /** Common config */ hadc3.Instance = ADC3; hadc3.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1; hadc3.Init.Resolution = ADC_RESOLUTION_8B; hadc3.Init.DataAlign = ADC3_DATAALIGN_RIGHT; hadc3.Init.ScanConvMode = ADC_SCAN_DISABLE; hadc3.Init.EOCSelection = ADC_EOC_SINGLE_CONV; hadc3.Init.LowPowerAutoWait = DISABLE; hadc3.Init.ContinuousConvMode = ENABLE; hadc3.Init.NbrOfConversion = 1; hadc3.Init.DiscontinuousConvMode = DISABLE; hadc3.Init.ExternalTrigConv = ADC_SOFTWARE_START; hadc3.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; hadc3.Init.DMAContinuousRequests = ENABLE; hadc3.Init.SamplingMode = ADC_SAMPLING_MODE_NORMAL; hadc3.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DR; hadc3.Init.Overrun = ADC_OVR_DATA_PRESERVED; hadc3.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE; hadc3.Init.OversamplingMode = DISABLE; if (HAL_ADC_Init(&hadc3) != HAL_OK) { Error_Handler(); } /** Configure Regular Channel */ sConfig.Channel = ADC_CHANNEL_4; sConfig.Rank = ADC_REGULAR_RANK_1; sConfig.SamplingTime = ADC3_SAMPLETIME_2CYCLES_5; sConfig.SingleDiff = ADC_SINGLE_ENDED; sConfig.OffsetNumber = ADC_OFFSET_NONE; sConfig.Offset = 0; sConfig.OffsetSignedSaturation = DISABLE; sConfig.OffsetSign = ADC3_OFFSET_SIGN_NEGATIVE; if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN ADC3_Init 2 */ /* USER CODE END ADC3_Init 2 */ } /** * Enable DMA controller clock */ static void MX_DMA_Init(void) { /* DMA controller clock enable */ __HAL_RCC_DMA1_CLK_ENABLE(); /* DMA interrupt init */ /* DMA1_Stream0_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA1_Stream0_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Stream0_IRQn); } /** * Enable MDMA controller clock * Configure MDMA for global transfers * hmdma_mdma_channel0_sw_0 * node_mdma_channel0_sw_1 * node_mdma_channel0_sw_2 * node_mdma_channel0_sw_3 * node_mdma_channel0_sw_4 * node_mdma_channel0_sw_5 */ static void MX_MDMA_Init(void) { /* MDMA controller clock enable */ __HAL_RCC_MDMA_CLK_ENABLE(); /* Local variables */ MDMA_LinkNodeConfTypeDef nodeConfig; /* Configure MDMA channel MDMA_Channel0 */ /* Configure MDMA request hmdma_mdma_channel0_sw_0 on MDMA_Channel0 */ hmdma_mdma_channel0_sw_0.Instance = MDMA_Channel0; hmdma_mdma_channel0_sw_0.Init.Request = MDMA_REQUEST_SW; hmdma_mdma_channel0_sw_0.Init.TransferTriggerMode = MDMA_BLOCK_TRANSFER; hmdma_mdma_channel0_sw_0.Init.Priority = MDMA_PRIORITY_VERY_HIGH; hmdma_mdma_channel0_sw_0.Init.Endianness = MDMA_LITTLE_ENDIANNESS_PRESERVE; hmdma_mdma_channel0_sw_0.Init.SourceInc = MDMA_SRC_INC_BYTE; hmdma_mdma_channel0_sw_0.Init.DestinationInc = MDMA_DEST_INC_BYTE; hmdma_mdma_channel0_sw_0.Init.SourceDataSize = MDMA_SRC_DATASIZE_BYTE; hmdma_mdma_channel0_sw_0.Init.DestDataSize = MDMA_DEST_DATASIZE_BYTE; hmdma_mdma_channel0_sw_0.Init.DataAlignment = MDMA_DATAALIGN_PACKENABLE; hmdma_mdma_channel0_sw_0.Init.BufferTransferLength = 1; hmdma_mdma_channel0_sw_0.Init.SourceBurst = MDMA_SOURCE_BURST_SINGLE; hmdma_mdma_channel0_sw_0.Init.DestBurst = MDMA_DEST_BURST_SINGLE; hmdma_mdma_channel0_sw_0.Init.SourceBlockAddressOffset = 0; hmdma_mdma_channel0_sw_0.Init.DestBlockAddressOffset = 0; if (HAL_MDMA_Init(&hmdma_mdma_channel0_sw_0) != HAL_OK) { Error_Handler(); } /* Initialize MDMA link node according to specified parameters */ nodeConfig.Init.Request = MDMA_REQUEST_SW; nodeConfig.Init.TransferTriggerMode = MDMA_BLOCK_TRANSFER; nodeConfig.Init.Priority = MDMA_PRIORITY_VERY_HIGH; nodeConfig.Init.Endianness = MDMA_LITTLE_ENDIANNESS_PRESERVE; nodeConfig.Init.SourceInc = MDMA_SRC_INC_BYTE; nodeConfig.Init.DestinationInc = MDMA_DEST_INC_BYTE; nodeConfig.Init.SourceDataSize = MDMA_SRC_DATASIZE_BYTE; nodeConfig.Init.DestDataSize = MDMA_DEST_DATASIZE_BYTE; nodeConfig.Init.DataAlignment = MDMA_DATAALIGN_PACKENABLE; nodeConfig.Init.BufferTransferLength = 1; nodeConfig.Init.SourceBurst = MDMA_SOURCE_BURST_SINGLE; nodeConfig.Init.DestBurst = MDMA_DEST_BURST_SINGLE; nodeConfig.Init.SourceBlockAddressOffset = 0; nodeConfig.Init.DestBlockAddressOffset = 0; nodeConfig.PostRequestMaskAddress = 0; nodeConfig.PostRequestMaskData = 0; nodeConfig.SrcAddress = (uint32_t)&SRC_Buf0[0]; nodeConfig.DstAddress = (uint32_t)DST_Buf1; nodeConfig.BlockDataLength = XFR_SIZE; nodeConfig.BlockCount = 1; if (HAL_MDMA_LinkedList_CreateNode(&node_mdma_channel0_sw_1, &nodeConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN mdma_channel0_sw_1 */ /* USER CODE END mdma_channel0_sw_1 */ /* Connect a node to the linked list */ if (HAL_MDMA_LinkedList_AddNode(&hmdma_mdma_channel0_sw_0, &node_mdma_channel0_sw_1, 0) != HAL_OK) { Error_Handler(); } /* Initialize MDMA link node according to specified parameters */ nodeConfig.Init.Request = MDMA_REQUEST_SW; nodeConfig.Init.TransferTriggerMode = MDMA_BLOCK_TRANSFER; nodeConfig.Init.Priority = MDMA_PRIORITY_VERY_HIGH; nodeConfig.Init.Endianness = MDMA_LITTLE_ENDIANNESS_PRESERVE; nodeConfig.Init.SourceInc = MDMA_SRC_INC_BYTE; nodeConfig.Init.DestinationInc = MDMA_DEST_INC_BYTE; nodeConfig.Init.SourceDataSize = MDMA_SRC_DATASIZE_BYTE; nodeConfig.Init.DestDataSize = MDMA_DEST_DATASIZE_BYTE; nodeConfig.Init.DataAlignment = MDMA_DATAALIGN_PACKENABLE; nodeConfig.Init.BufferTransferLength = 1; nodeConfig.Init.SourceBurst = MDMA_SOURCE_BURST_SINGLE; nodeConfig.Init.DestBurst = MDMA_DEST_BURST_SINGLE; nodeConfig.Init.SourceBlockAddressOffset = 0; nodeConfig.Init.DestBlockAddressOffset = 0; nodeConfig.PostRequestMaskAddress = 0; nodeConfig.PostRequestMaskData = 0; nodeConfig.SrcAddress = (uint32_t)&SRC_Buf0[XFR_SIZE]; nodeConfig.DstAddress = (uint32_t)DST_Buf2; nodeConfig.BlockDataLength = XFR_SIZE; nodeConfig.BlockCount = 1; if (HAL_MDMA_LinkedList_CreateNode(&node_mdma_channel0_sw_2, &nodeConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN mdma_channel0_sw_2 */ /* USER CODE END mdma_channel0_sw_2 */ /* Connect a node to the linked list */ if (HAL_MDMA_LinkedList_AddNode(&hmdma_mdma_channel0_sw_0, &node_mdma_channel0_sw_2, 0) != HAL_OK) { Error_Handler(); } /* Initialize MDMA link node according to specified parameters */ nodeConfig.Init.Request = MDMA_REQUEST_SW; nodeConfig.Init.TransferTriggerMode = MDMA_BLOCK_TRANSFER; nodeConfig.Init.Priority = MDMA_PRIORITY_VERY_HIGH; nodeConfig.Init.Endianness = MDMA_LITTLE_ENDIANNESS_PRESERVE; nodeConfig.Init.SourceInc = MDMA_SRC_INC_BYTE; nodeConfig.Init.DestinationInc = MDMA_DEST_INC_BYTE; nodeConfig.Init.SourceDataSize = MDMA_SRC_DATASIZE_BYTE; nodeConfig.Init.DestDataSize = MDMA_DEST_DATASIZE_BYTE; nodeConfig.Init.DataAlignment = MDMA_DATAALIGN_PACKENABLE; nodeConfig.Init.BufferTransferLength = 1; nodeConfig.Init.SourceBurst = MDMA_SOURCE_BURST_SINGLE; nodeConfig.Init.DestBurst = MDMA_DEST_BURST_SINGLE; nodeConfig.Init.SourceBlockAddressOffset = 0; nodeConfig.Init.DestBlockAddressOffset = 0; nodeConfig.PostRequestMaskAddress = 0; nodeConfig.PostRequestMaskData = 0; nodeConfig.SrcAddress = (uint32_t)&SRC_Buf0[0]; nodeConfig.DstAddress = (uint32_t)DST_Buf3; nodeConfig.BlockDataLength = XFR_SIZE; nodeConfig.BlockCount = 1; if (HAL_MDMA_LinkedList_CreateNode(&node_mdma_channel0_sw_3, &nodeConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN mdma_channel0_sw_3 */ /* USER CODE END mdma_channel0_sw_3 */ /* Connect a node to the linked list */ if (HAL_MDMA_LinkedList_AddNode(&hmdma_mdma_channel0_sw_0, &node_mdma_channel0_sw_3, 0) != HAL_OK) { Error_Handler(); } /* Initialize MDMA link node according to specified parameters */ nodeConfig.Init.Request = MDMA_REQUEST_SW; nodeConfig.Init.TransferTriggerMode = MDMA_BLOCK_TRANSFER; nodeConfig.Init.Priority = MDMA_PRIORITY_VERY_HIGH; nodeConfig.Init.Endianness = MDMA_LITTLE_ENDIANNESS_PRESERVE; nodeConfig.Init.SourceInc = MDMA_SRC_INC_BYTE; nodeConfig.Init.DestinationInc = MDMA_DEST_INC_BYTE; nodeConfig.Init.SourceDataSize = MDMA_SRC_DATASIZE_BYTE; nodeConfig.Init.DestDataSize = MDMA_DEST_DATASIZE_BYTE; nodeConfig.Init.DataAlignment = MDMA_DATAALIGN_PACKENABLE; nodeConfig.Init.BufferTransferLength = 1; nodeConfig.Init.SourceBurst = MDMA_SOURCE_BURST_SINGLE; nodeConfig.Init.DestBurst = MDMA_DEST_BURST_SINGLE; nodeConfig.Init.SourceBlockAddressOffset = 0; nodeConfig.Init.DestBlockAddressOffset = 0; nodeConfig.PostRequestMaskAddress = 0; nodeConfig.PostRequestMaskData = 0; nodeConfig.SrcAddress = (uint32_t)&SRC_Buf0[XFR_SIZE]; nodeConfig.DstAddress = (uint32_t)DST_Buf4; nodeConfig.BlockDataLength = XFR_SIZE; nodeConfig.BlockCount = 1; if (HAL_MDMA_LinkedList_CreateNode(&node_mdma_channel0_sw_4, &nodeConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN mdma_channel0_sw_4 */ /* USER CODE END mdma_channel0_sw_4 */ /* Connect a node to the linked list */ if (HAL_MDMA_LinkedList_AddNode(&hmdma_mdma_channel0_sw_0, &node_mdma_channel0_sw_4, 0) != HAL_OK) { Error_Handler(); } /* Initialize MDMA link node according to specified parameters */ nodeConfig.Init.Request = MDMA_REQUEST_SW; nodeConfig.Init.TransferTriggerMode = MDMA_BLOCK_TRANSFER; nodeConfig.Init.Priority = MDMA_PRIORITY_VERY_HIGH; nodeConfig.Init.Endianness = MDMA_LITTLE_ENDIANNESS_PRESERVE; nodeConfig.Init.SourceInc = MDMA_SRC_INC_BYTE; nodeConfig.Init.DestinationInc = MDMA_DEST_INC_BYTE; nodeConfig.Init.SourceDataSize = MDMA_SRC_DATASIZE_BYTE; nodeConfig.Init.DestDataSize = MDMA_DEST_DATASIZE_BYTE; nodeConfig.Init.DataAlignment = MDMA_DATAALIGN_PACKENABLE; nodeConfig.Init.BufferTransferLength = 1; nodeConfig.Init.SourceBurst = MDMA_SOURCE_BURST_SINGLE; nodeConfig.Init.DestBurst = MDMA_DEST_BURST_SINGLE; nodeConfig.Init.SourceBlockAddressOffset = 0; nodeConfig.Init.DestBlockAddressOffset = 0; nodeConfig.PostRequestMaskAddress = 0; nodeConfig.PostRequestMaskData = 0; nodeConfig.SrcAddress = (uint32_t)&SRC_Buf0[0]; nodeConfig.DstAddress = (uint32_t)DST_Buf5; nodeConfig.BlockDataLength = XFR_SIZE; nodeConfig.BlockCount = 1; if (HAL_MDMA_LinkedList_CreateNode(&node_mdma_channel0_sw_5, &nodeConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN mdma_channel0_sw_5 */ HAL_MDMA_RegisterCallback(&hmdma_mdma_channel0_sw_0, HAL_MDMA_XFER_CPLT_CB_ID, MDMA_TransferCompleteCallback); HAL_MDMA_RegisterCallback(&hmdma_mdma_channel0_sw_0, HAL_MDMA_XFER_ERROR_CB_ID, MDMA_TransferErrorCallback); HAL_MDMA_RegisterCallback(&hmdma_mdma_channel0_sw_0, HAL_MDMA_XFER_BLOCKCPLT_CB_ID, MDMA_TransferBlockCompleteCallback); /* USER CODE END mdma_channel0_sw_5 */ /* Connect a node to the linked list */ if (HAL_MDMA_LinkedList_AddNode(&hmdma_mdma_channel0_sw_0, &node_mdma_channel0_sw_5, 0) != HAL_OK) { Error_Handler(); } /* Make the linked list circular by connecting the last node to the first */ if (HAL_MDMA_LinkedList_EnableCircularMode(&hmdma_mdma_channel0_sw_0) != HAL_OK) { Error_Handler(); } /* MDMA interrupt initialization */ /* MDMA_IRQn interrupt configuration */ HAL_NVIC_SetPriority(MDMA_IRQn, 0, 0); HAL_NVIC_EnableIRQ(MDMA_IRQn); } /** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { /* USER CODE BEGIN MX_GPIO_Init_1 */ /* USER CODE END MX_GPIO_Init_1 */ /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOF_CLK_ENABLE(); /* USER CODE BEGIN MX_GPIO_Init_2 */ /* USER CODE END MX_GPIO_Init_2 */ } /* USER CODE BEGIN 4 */ static void MDMA_TransferCompleteCallback(MDMA_HandleTypeDef *hmdma) { __NOP(); } static void MDMA_TransferErrorCallback(MDMA_HandleTypeDef *hmdma) { __NOP(); } static void MDMA_TransferBlockCompleteCallback(MDMA_HandleTypeDef *hmdma) { __NOP(); //HAL_MDMA_GenerateSWRequest(&hmdma_mdma_channel0_sw_0); } void HAL_ADC_ConvHalfCpltCallback(ADC_HandleTypeDef* hadc){ HAL_MDMA_GenerateSWRequest(&hmdma_mdma_channel0_sw_0); } //Called when buffer is completely filled void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc){ HAL_MDMA_GenerateSWRequest(&hmdma_mdma_channel0_sw_0); } /* USER CODE END 4 */ /* MPU Configuration */ void MPU_Config(void) { MPU_Region_InitTypeDef MPU_InitStruct = {0}; /* Disables the MPU */ HAL_MPU_Disable(); /** Initializes and configures the Region and the memory to be protected */ MPU_InitStruct.Enable = MPU_REGION_ENABLE; MPU_InitStruct.Number = MPU_REGION_NUMBER0; MPU_InitStruct.BaseAddress = 0x0; MPU_InitStruct.Size = MPU_REGION_SIZE_4GB; MPU_InitStruct.SubRegionDisable = 0x87; MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0; MPU_InitStruct.AccessPermission = MPU_REGION_NO_ACCESS; MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE; MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE; MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE; MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE; HAL_MPU_ConfigRegion(&MPU_InitStruct); /* Enables the MPU */ HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT); } /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */