/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file stm32f1xx_hal_msp.c * @brief This file provides code for the MSP Initialization * and de-Initialization codes. ****************************************************************************** * @attention * * Copyright (c) 2023 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" /* USER CODE BEGIN Includes */ /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN TD */ /* USER CODE END TD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN Define */ /* USER CODE END Define */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN Macro */ /* USER CODE END Macro */ /* Private variables ---------------------------------------------------------*/ /* USER CODE BEGIN PV */ /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* External functions --------------------------------------------------------*/ /* USER CODE BEGIN ExternalFunctions */ /* USER CODE END ExternalFunctions */ /* USER CODE BEGIN 0 */ /* USER CODE END 0 */ /** * Initializes the Global MSP. */ void HAL_MspInit(void) { /* USER CODE BEGIN MspInit 0 */ /* USER CODE END MspInit 0 */ __HAL_RCC_AFIO_CLK_ENABLE(); __HAL_RCC_PWR_CLK_ENABLE(); /* System interrupt init*/ /* USER CODE BEGIN MspInit 1 */ /* USER CODE END MspInit 1 */ } /** * @brief ADC MSP Initialization * This function configures the hardware resources used in this example * @param hadc: ADC handle pointer * @retval None */ void HAL_ADC_MspInit(ADC_HandleTypeDef* hadc) { GPIO_InitTypeDef GPIO_InitStruct = {0}; if(hadc->Instance==ADC1) { /* USER CODE BEGIN ADC1_MspInit 0 */ /* USER CODE END ADC1_MspInit 0 */ /* Peripheral clock enable */ __HAL_RCC_ADC1_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); /**ADC1 GPIO Configuration PA2 ------> ADC1_IN2 */ GPIO_InitStruct.Pin = GPIO_PIN_2; GPIO_InitStruct.Mode = GPIO_MODE_ANALOG; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /* USER CODE BEGIN ADC1_MspInit 1 */ /* USER CODE END ADC1_MspInit 1 */ } } /** * @brief ADC MSP De-Initialization * This function freeze the hardware resources used in this example * @param hadc: ADC handle pointer * @retval None */ void HAL_ADC_MspDeInit(ADC_HandleTypeDef* hadc) { if(hadc->Instance==ADC1) { /* USER CODE BEGIN ADC1_MspDeInit 0 */ /* USER CODE END ADC1_MspDeInit 0 */ /* Peripheral clock disable */ __HAL_RCC_ADC1_CLK_DISABLE(); /**ADC1 GPIO Configuration PA2 ------> ADC1_IN2 */ HAL_GPIO_DeInit(GPIOA, GPIO_PIN_2); /* USER CODE BEGIN ADC1_MspDeInit 1 */ /* USER CODE END ADC1_MspDeInit 1 */ } } /** * @brief TIM_IC MSP Initialization * This function configures the hardware resources used in this example * @param htim_ic: TIM_IC handle pointer * @retval None */ void HAL_TIM_IC_MspInit(TIM_HandleTypeDef* htim_ic) { GPIO_InitTypeDef GPIO_InitStruct = {0}; if(htim_ic->Instance==TIM2) { /* USER CODE BEGIN TIM2_MspInit 0 */ /* USER CODE END TIM2_MspInit 0 */ /* Peripheral clock enable */ __HAL_RCC_TIM2_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); /**TIM2 GPIO Configuration PA0-WKUP ------> TIM2_CH1 */ GPIO_InitStruct.Pin = GPIO_PIN_0; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /* TIM2 interrupt Init */ HAL_NVIC_SetPriority(TIM2_IRQn, 0, 0); HAL_NVIC_EnableIRQ(TIM2_IRQn); /* USER CODE BEGIN TIM2_MspInit 1 */ /* USER CODE END TIM2_MspInit 1 */ } } /** * @brief TIM_IC MSP De-Initialization * This function freeze the hardware resources used in this example * @param htim_ic: TIM_IC handle pointer * @retval None */ void HAL_TIM_IC_MspDeInit(TIM_HandleTypeDef* htim_ic) { if(htim_ic->Instance==TIM2) { /* USER CODE BEGIN TIM2_MspDeInit 0 */ /* USER CODE END TIM2_MspDeInit 0 */ /* Peripheral clock disable */ __HAL_RCC_TIM2_CLK_DISABLE(); /**TIM2 GPIO Configuration PA0-WKUP ------> TIM2_CH1 */ HAL_GPIO_DeInit(GPIOA, GPIO_PIN_0); /* TIM2 interrupt DeInit */ HAL_NVIC_DisableIRQ(TIM2_IRQn); /* USER CODE BEGIN TIM2_MspDeInit 1 */ /* USER CODE END TIM2_MspDeInit 1 */ } } /** * @brief UART MSP Initialization * This function configures the hardware resources used in this example * @param huart: UART handle pointer * @retval None */ void HAL_UART_MspInit(UART_HandleTypeDef* huart) { GPIO_InitTypeDef GPIO_InitStruct = {0}; if(huart->Instance==USART1) { /* USER CODE BEGIN USART1_MspInit 0 */ /* USER CODE END USART1_MspInit 0 */ /* Peripheral clock enable */ __HAL_RCC_USART1_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); /**USART1 GPIO Configuration PA9 ------> USART1_TX PA10 ------> USART1_RX */ GPIO_InitStruct.Pin = GPIO_PIN_9; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); GPIO_InitStruct.Pin = GPIO_PIN_10; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /* USER CODE BEGIN USART1_MspInit 1 */ /* USER CODE END USART1_MspInit 1 */ } } /** * @brief UART MSP De-Initialization * This function freeze the hardware resources used in this example * @param huart: UART handle pointer * @retval None */ void HAL_UART_MspDeInit(UART_HandleTypeDef* huart) { if(huart->Instance==USART1) { /* USER CODE BEGIN USART1_MspDeInit 0 */ /* USER CODE END USART1_MspDeInit 0 */ /* Peripheral clock disable */ __HAL_RCC_USART1_CLK_DISABLE(); /**USART1 GPIO Configuration PA9 ------> USART1_TX PA10 ------> USART1_RX */ HAL_GPIO_DeInit(GPIOA, GPIO_PIN_9|GPIO_PIN_10); /* USER CODE BEGIN USART1_MspDeInit 1 */ /* USER CODE END USART1_MspDeInit 1 */ } } /* USER CODE BEGIN 1 */ /* USER CODE END 1 */