#include "octospi.h" #include "main.h" #include "alt_main.h" #include "gpio.h" #include "quadspi.h" //bijgevoegd #define LOADER_OK 0x1 #define LOADER_FAIL 0x0 extern void SystemClock_Config(void); //extern void MX_OCTOSPI2_Init(void); extern void MX_GPIO_Init(void); /** * @brief System initialization. * @param None * @retval LOADER_OK = 1 : Operation succeeded * @retval LOADER_FAIL = 0 : Operation failed */ int Init(void) { *(uint32_t*)0xE000EDF0 = 0xA05F0000; //enable interrupts in debug SystemInit(); /* ADAPTATION TO THE DEVICE * * change VTOR setting for H7 device * SCB->VTOR = 0x24000000 | 0x200; * * change VTOR setting for other devices * SCB->VTOR = 0x20000000 | 0x200; * * */ SCB->VTOR = 0x20000000 | 0x200; __set_PRIMASK(0); //enable interrupts HAL_Init(); SystemClock_Config(); MX_GPIO_Init(); __HAL_RCC_OSPI2_FORCE_RESET(); //completely reset peripheral __HAL_RCC_OSPI2_RELEASE_RESET(); if (CSP_QUADSPI_Init() != HAL_OK) { __set_PRIMASK(1); //disable interrupts return LOADER_FAIL; } if (CSP_QSPI_EnableMemoryMappedMode() != HAL_OK) { __set_PRIMASK(1); //disable interrupts return LOADER_FAIL; } __set_PRIMASK(1); //disable interrupts return LOADER_OK; } /** * @brief Program memory. * @param Address: page address * @param Size : size of data * @param buffer : pointer to data buffer * @retval LOADER_OK = 1 : Operation succeeded * @retval LOADER_FAIL = 0 : Operation failed */ int Write(uint32_t Address, uint32_t Size, uint8_t* buffer) { __set_PRIMASK(0); //enable interrupts if (HAL_OSPI_Abort(&hospi2) != HAL_OK) { __set_PRIMASK(1); //disable interrupts return LOADER_FAIL; } if (CSP_QSPI_WriteMemory((uint8_t*) buffer, (Address & (0x0fffffff)), Size) != HAL_OK) //nakijken { __set_PRIMASK(1); //disable interrupts return LOADER_FAIL; } __set_PRIMASK(1); //disable interrupts return LOADER_OK; } /** * @brief Sector erase. * @param EraseStartAddress : erase start address * @param EraseEndAddress : erase end address * @retval LOADER_OK = 1 : Operation succeeded * @retval LOADER_FAIL = 0 : Operation failed */ int SectorErase(uint32_t EraseStartAddress, uint32_t EraseEndAddress) { __set_PRIMASK(0); //enable interrupts if (HAL_OSPI_Abort(&hospi2) != HAL_OK) { __set_PRIMASK(1); //disable interrupts return LOADER_FAIL; } if (CSP_QSPI_EraseSector(EraseStartAddress, EraseEndAddress) != HAL_OK) { __set_PRIMASK(1); //disable interrupts return LOADER_FAIL; } __set_PRIMASK(1); //disable interrupts return LOADER_OK; } /** * Description : * Mass erase of external flash area * Optional command - delete in case usage of mass erase is not planed * Inputs : * none * outputs : * none * Note: Optional for all types of device */ int MassErase(void) { __set_PRIMASK(0); //enable interrupts if (HAL_OSPI_Abort(&hospi2) != HAL_OK) { __set_PRIMASK(1); //disable interrupts return LOADER_FAIL; } if (CSP_QSPI_Erase_Chip() != HAL_OK) { __set_PRIMASK(1); //disable interrupts return LOADER_FAIL; } __set_PRIMASK(1); //disable interrupts return LOADER_OK; } /** * Description : * Calculates checksum value of the memory zone * Inputs : * StartAddress : Flash start address * Size : Size (in WORD) * InitVal : Initial CRC value * outputs : * R0 : Checksum value * Note: Optional for all types of device */ uint32_t CheckSum(uint32_t StartAddress, uint32_t Size, uint32_t InitVal) { uint8_t missalignementAddress = StartAddress % 4; uint8_t missalignementSize = Size; int cnt; uint32_t Val; StartAddress -= StartAddress % 4; Size += (Size % 4 == 0) ? 0 : 4 - (Size % 4); for (cnt = 0; cnt < Size; cnt += 4) { Val = *(uint32_t*) StartAddress; if (missalignementAddress) { switch (missalignementAddress) { case 1: InitVal += (uint8_t) (Val >> 8 & 0xff); InitVal += (uint8_t) (Val >> 16 & 0xff); InitVal += (uint8_t) (Val >> 24 & 0xff); missalignementAddress -= 1; break; case 2: InitVal += (uint8_t) (Val >> 16 & 0xff); InitVal += (uint8_t) (Val >> 24 & 0xff); missalignementAddress -= 2; break; case 3: InitVal += (uint8_t) (Val >> 24 & 0xff); missalignementAddress -= 3; break; } } else if ((Size - missalignementSize) % 4 && (Size - cnt) <= 4) { switch (Size - missalignementSize) { case 1: InitVal += (uint8_t) Val; InitVal += (uint8_t) (Val >> 8 & 0xff); InitVal += (uint8_t) (Val >> 16 & 0xff); missalignementSize -= 1; break; case 2: InitVal += (uint8_t) Val; InitVal += (uint8_t) (Val >> 8 & 0xff); missalignementSize -= 2; break; case 3: InitVal += (uint8_t) Val; missalignementSize -= 3; break; } } else { InitVal += (uint8_t) Val; InitVal += (uint8_t) (Val >> 8 & 0xff); InitVal += (uint8_t) (Val >> 16 & 0xff); InitVal += (uint8_t) (Val >> 24 & 0xff); } StartAddress += 4; } return (InitVal); } /** * Description : * Verify flash memory with RAM buffer and calculates checksum value of * the programmed memory * Inputs : * FlashAddr : Flash address * RAMBufferAddr : RAM buffer address * Size : Size (in WORD) * InitVal : Initial CRC value * outputs : * R0 : Operation failed (address of failure) * R1 : Checksum value * Note: Optional for all types of device */ uint64_t Verify(uint32_t MemoryAddr, uint32_t RAMBufferAddr, uint32_t Size, uint32_t missalignement) { __set_PRIMASK(0); //enable interrupts uint32_t VerifiedData = 0, InitVal = 0; uint64_t checksum; Size *= 4; if (CSP_QSPI_EnableMemoryMappedMode() != HAL_OK) { __set_PRIMASK(1); //disable interrupts return LOADER_FAIL; } checksum = CheckSum((uint32_t) MemoryAddr + (missalignement & 0xf), Size - ((missalignement >> 16) & 0xF), InitVal); while (Size > VerifiedData) { if (*(uint8_t*) MemoryAddr++ != *((uint8_t*) RAMBufferAddr + VerifiedData)) { __set_PRIMASK(1); //disable interrupts return ((checksum << 32) + (MemoryAddr + VerifiedData)); } VerifiedData++; } __set_PRIMASK(1); //disable interrupts return (checksum << 32); }