/**
******************************************************************************
* @file Audio_playback_and_record/src/main.c
* @author MCD Application Team
* @version V1.0.0
* @date 28-October-2011
* @brief Main program body
******************************************************************************
* @attention
*
* THE PRESENT FIRMWARE WHICH IS FOR GUIDANCE ONLY AIMS AT PROVIDING CUSTOMERS
* WITH CODING INFORMATION REGARDING THEIR PRODUCTS IN ORDER FOR THEM TO SAVE
* TIME. AS A RESULT, STMICROELECTRONICS SHALL NOT BE HELD LIABLE FOR ANY
* DIRECT, INDIRECT OR CONSEQUENTIAL DAMAGES WITH RESPECT TO ANY CLAIMS ARISING
* FROM THE CONTENT OF SUCH FIRMWARE AND/OR THE USE MADE BY CUSTOMERS OF THE
* CODING INFORMATION CONTAINED HEREIN IN CONNECTION WITH THEIR PRODUCTS.
*
*
© COPYRIGHT 2011 STMicroelectronics
*/
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "spi_3201.h"
#include
/* Exported macro ------------------------------------------------------------*/
/* Select 3201: Chip Select pin low */
//#define 3201_CS_LOW() GPIO_ResetBits(GPIOB, GPIO_Pin_12)
/* Deselect 3201: Chip Select pin high */
//#define 3201_CS_HIGH() GPIO_SetBits(GPIOB, GPIO_Pin_12)
/* Private typedef -----------------------------------------------------------*/
/* Private define ------------------------------------------------------------*/
#define ADC3_DR_ADDRESS ((uint32_t)0x4001224C)
/* Private variables ---------------------------------------------------------*/
static __IO uint32_t TimingDelay;
extern uint8_t NbrOfDataToTransfer;
extern uint8_t NbrOfDataToRead;
extern __IO uint8_t TxCounter;
extern __IO uint16_t RxCounter;
extern uint8_t RxBuffer[];
char *command;
char *command_AT1 = "AT+CGATT?\r\n";
//char *command_AT2 = "AT+UPSD=0,1,"AIRTELGPRS.COM"\r\n";
//char command[]="vv, "as" ";
unsigned char *Buffer;
unsigned char ab[64];
unsigned char bc[64];
unsigned char cd[64];
unsigned char de[64];
unsigned char ef[64];
unsigned char gh[64];
unsigned char hi[64];
unsigned char ij[64];
unsigned char jk[64];
unsigned int i;
unsigned char d;
__IO uint16_t ADC3ConvertedValue = 0;
__IO uint32_t ADC3ConvertedVoltage = 0;
RCC_ClocksTypeDef RCC_Clocks;
__IO uint8_t RepeatState = 0;
__IO uint8_t RepeatState1 = 0;
__IO uint8_t RepeatState2 = 0;
__IO uint8_t RepeatState3 = 0;
__IO uint8_t RepeatState4 = 0;
__IO uint8_t RepeatState5 = 0;
__IO uint8_t RepeatState6 = 0;
__IO uint8_t RepeatState7 = 0;
__IO uint8_t RepeatState8 = 0;
__IO uint8_t RepeatState9 = 0;
__IO uint8_t RepeatState10 = 0;
__IO uint16_t CCR_Val = 16826;
extern __IO uint8_t LED_Toggle;
/* Private function prototypes -----------------------------------------------*/
static void TIM_LED_Config(void);
void RCC_Configuration(void);
void NVIC_Config(void);
void GPIO_Configuration(void);
void ADC3_CH12_DMA_Config(void);
void itoa(int,char *,int);
/* Private functions ---------------------------------------------------------*/
void RCC_Configuration(void)
{
/* --------------------------- System Clocks Configuration -----------------*/
/* GPIOC clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
/* USART4 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_UART4, ENABLE);
/* GPIOC clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);
/* USART5 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_UART5, ENABLE);
}
void NVIC_Config(void)
{
NVIC_InitTypeDef NVIC_InitStructure;
/* Enable the USARTx Interrupt */
NVIC_InitStructure.NVIC_IRQChannel = UART4_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
}
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_UART4);/* UART4_TX */
GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_UART4);/* UART4_RX */
GPIO_PinAFConfig(GPIOC, GPIO_PinSource12, GPIO_AF_UART5);/* UART4_TX */
GPIO_PinAFConfig(GPIOD, GPIO_PinSource2, GPIO_AF_UART5);/* UART4_RX */
/*-------------------------- GPIO Configuration ----------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOC, &GPIO_InitStructure);
/*-------------------------- GPIO Configuration ----------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12 ;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOC, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 ;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOD, &GPIO_InitStructure);
}
void USART4_Configuration(void)
{
USART_InitTypeDef USART_InitStructure;
// USART_ClockInitTypeDef USART_ClockInitStruct;
/* USARTx configuration ------------------------------------------------------*/
/* USARTx configured as follow:
- BaudRate = 9600 baud
- Word Length = 8 Bits
- Two Stop Bit
- Odd parity
- Hardware flow control disabled (RTS and CTS signals)
- Receive and transmit enabled
*/
USART_InitStructure.USART_BaudRate = 9600; //115200;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(UART4,&USART_InitStructure); //uart
USART_Cmd(UART4, ENABLE);
}
void USART5_Configuration(void)
{
USART_InitTypeDef USART_InitStructure;
// USART_ClockInitTypeDef USART_ClockInitStruct;
/* USARTx configuration ------------------------------------------------------*/
/* USARTx configured as follow:
- BaudRate = 9600 baud
- Word Length = 8 Bits
- Two Stop Bit
- Odd parity
- Hardware flow control disabled (RTS and CTS signals)
- Receive and transmit enabled
*/
USART_InitStructure.USART_BaudRate = 9600; //115200;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(UART5,&USART_InitStructure); //uart
USART_Cmd(UART5, ENABLE);
}
void relay_config(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/* GPIOD Periph clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);
/* Configure PD11 in output pushpull mode */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOD, &GPIO_InitStructure);
}
void SendChar(char ch)
{
/* Wait till holding buffer empty */
while(USART_GetFlagStatus(UART4, USART_FLAG_TXE) == RESET);
USART_SendData(UART4, (unsigned int) ch);
}
void SendInt(uint16_t num)
{
while(USART_GetFlagStatus(UART4, USART_FLAG_TXE) == RESET);
USART_SendData(UART4, (uint16_t) num);
}
void SendInt2(char num)
{
while(USART_GetFlagStatus(UART4, USART_FLAG_TXE) == RESET);
USART_SendData(UART4, (unsigned int) num);
}
void SendString(char *s)
{
while(*s)
{
while(USART_GetFlagStatus(UART4, USART_FLAG_TXE) == RESET);
USART_SendData(UART4, (unsigned int) *s++);
}
}
void SendStringadc(uint32_t *s)
{
while(*s)
{
while(USART_GetFlagStatus(UART4, USART_FLAG_TXE) == RESET);
USART_SendData(UART4, (unsigned int) *s++);
}
}
void SendChar5(unsigned char ch)
{
/* Wait till holding buffer empty */
while(USART_GetFlagStatus(UART5, USART_FLAG_TXE) == RESET);
USART_SendData(UART5, (unsigned int) ch);
}
void SendString5(unsigned char *s)
{
while(*s)
{
while(USART_GetFlagStatus(UART5, USART_FLAG_TXE) == RESET);
USART_SendData(UART5, (unsigned int) *s++);
}
}
unsigned int RecvChar(void)
{
unsigned int aa;
/* Wait till holding buffer empty */
while(USART_GetFlagStatus(UART4, USART_FLAG_RXNE) == RESET);
aa = (unsigned int) (USART_ReceiveData(UART4) & 0x7F);
return aa;
}
void RecvString(unsigned char *buffer)
{
unsigned char data;
do
{
while(USART_GetFlagStatus(UART4, USART_FLAG_RXNE) == RESET); // Wait for data to be received
data = (unsigned char) (USART_ReceiveData(UART4) & 0x7F);
*buffer = data;
buffer++; // Increment the string pointer
}
while(data!='K');
*buffer='\0';
}
void RecvStringg(void)
{
unsigned char data;
int i=0;
do
{
while(USART_GetFlagStatus(UART4, USART_FLAG_RXNE) == RESET); // Wait for data to be received
data = (unsigned char) (USART_ReceiveData(UART4) & 0x7F);
ab[i] = data;
i++; // Increment the string pointer
}
while(data!='K');
}
/**
* @brief Delay Function.
* @param nCount:specifies the Delay time length.
* @retval None
*/
void Delay(__IO uint32_t nCount)
{
while(nCount--)
{
}
}
void Response(void)
{
i=0;
do
{
while(USART_GetFlagStatus(UART4, USART_FLAG_RXNE) == RESET);
d = (USART_ReceiveData(UART4) & 0x7F);
ab[i]=d;
i++;
}while(d!='K');
}
void Response1(void)
{
i=0;
do
{
while(USART_GetFlagStatus(UART4, USART_FLAG_RXNE) == RESET);
d = (USART_ReceiveData(UART4) & 0x7F);
bc[i]=d;
i++;
}while(d!='K');
}
void Response2(void)
{
i=0;
do
{
while(USART_GetFlagStatus(UART4, USART_FLAG_RXNE) == RESET);
d = (USART_ReceiveData(UART4) & 0x7F);
cd[i]=d;
i++;
}while(d!='K');
}
void ResponseSt(void)
{
i=0;
do
{
while(USART_GetFlagStatus(UART4, USART_FLAG_RXNE) == RESET);
d = (USART_ReceiveData(UART4) & 0x7F);
ab[i]=d;
i++;
}while(ab[1]!='K');
}
void Gprs(void)
{
SendString("AT+UPSDA=0,4\r\n"); //GPRS DEACTIVATE
Response();
SendString5(ab);
SendString("AT+UPSD=0,1,\"AIRTELGPRS.COM\"\r\n");
Response();
SendString5(ab);
SendString("AT+UPSD=0,7,\"0.0.0.0\"\r\n");
Response();
SendString5(ab);;
SendString("AT+UPSDA=0,3\r\n"); //GPRS ACTIVATE
Response();
SendString5(ab);
}
void Http(void)
{
SendString("AT+UHTTP=0\r\n"); //RESET
Response();
SendString5(ab);
SendString("AT+UHTTP=0,2,\"marudham\"\r\n"); //USERNAME
Response();
SendString5(ab);
SendString("AT+UHTTP=0,3,\"marudham\"\r\n"); //PASSWORD
Response();
SendString5(ab);
SendString("AT+UHTTP=0,1,\"www.marudham.co.in\"\r\n"); //gate way
Response();
SendString5(ab);
//SendString("AT+UHTTPC=0,1,\"/datacapture.php?imeiid=357464034993805&latitude=13.0218N&longitude=80.2056E&date=23062012&time=092652.000&speed=0.61\",\"get.ffs\"\r\n");
//Response();
}
/**
* @brief Main program.
* @param None
* @retval None
void AdcConfig(void)
{
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN;
GPIO_Init(GPIOC, &GPIO_InitStructure);
// ADC1 configuration ------------------------------------------------------
ADC_InitStructure.ADC_Mode = ADC_Mode_Independent;
ADC_InitStructure.ADC_ScanConvMode = ENABLE;
ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfChannel = 1;
ADC_Init(ADC1, &ADC_InitStructure);
} */
void SpiConfig(void)
{
SPI_InitTypeDef SPI_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
RCC_APB2PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE);
/*!< Enable GPIO clocks */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);
/*!< SPI pins configuration *************************************************/
/*!< Connect SPI pins to AF5 */
GPIO_PinAFConfig(GPIOB, GPIO_PinSource13, GPIO_AF_SPI2 );
GPIO_PinAFConfig(GPIOB, GPIO_PinSource14, GPIO_AF_SPI2 );
GPIO_PinAFConfig(GPIOB, GPIO_PinSource15, GPIO_AF_SPI2 );
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;
/*!< SPI SCK pin configuration */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13;
GPIO_Init(GPIOB, &GPIO_InitStructure);
/*!< SPI MOSI pin configuration */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_15;
GPIO_Init(GPIOB, &GPIO_InitStructure);
/*!< SPI MISO pin configuration */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_14;
GPIO_Init(GPIOB, &GPIO_InitStructure);
/*!< Configure sFLASH Card CS pin in output pushpull mode ********************/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOB, &GPIO_InitStructure);
/*!< Deselect the FLASH: Chip Select high */
c3201_CS_HIGH();
/*!< SPI configuration */
SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
SPI_InitStructure.SPI_Mode = SPI_Mode_Master;
SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;
SPI_InitStructure.SPI_CPOL = SPI_CPOL_High;
SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge;
SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;
SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_4;
SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;
SPI_InitStructure.SPI_CRCPolynomial = 7;
SPI_Init(SPI2, &SPI_InitStructure);
/*!< Enable the sFLASH_SPI */
SPI_Cmd(SPI2, ENABLE);
}
/*
char *itoa(int n, char *s, int b) {
static char digits[] = "0123456789abcdefghijklmnopqrstuvwxyz";
int i=0, sign;
if ((sign = n) < 0)
n = -n;
do {
s[i++] = digits[n % b];
} while ((n /= b) > 0);
if (sign < 0)
s[i++] = '-';
s[i] = '\0';
return strrev(s);
}
*/
char * utoa(unsigned int n)
{
char * res, buf[30]; // long enough for largest number
unsigned int i, counter = 0;
if (n == 0)
buf[counter++] = '0';
for ( ; n; n /= 10)
buf[counter++] = "0123456789"[n%10];
res = malloc(counter);
for (i = 0; i < counter; ++i)
res[i] = buf[counter - i - 1];
return res;
}
int main(void)
{
char read;
char value;
int num = 123;
char buf[5];
//SystemCoreClockUpdate();
/* Initialize LEDS */
STM_EVAL_LEDInit(LED3);
STM_EVAL_LEDInit(LED4);
STM_EVAL_LEDInit(LED5);
STM_EVAL_LEDInit(LED6);
/* Green Led On: start of application */
STM_EVAL_LEDOn(LED4);
/* SysTick end of count event each 10ms */
RCC_GetClocksFreq(&RCC_Clocks);
SysTick_Config(RCC_Clocks.HCLK_Frequency / 100);
/* Configure TIM4 Peripheral to manage LEDs lighting */
//TIM_LED_Config();
//relay_config();
NVIC_Config(); //***
RCC_Configuration(); //***
GPIO_Configuration(); //****
USART4_Configuration(); //***
USART5_Configuration();
/* Enable the uart receive interrupt: this interrupt is generated when the
transmit data register is empty */
//USART_ITConfig(UART4, USART_IT_RXNE, ENABLE); //***
//AdcConfig();
SpiConfig();
/* ADC3 configuration *******************************************************/
/* - Enable peripheral clocks */
/* - DMA2_Stream0 channel2 configuration */
/* - Configure ADC Channel12 pin as analog input */
/* - Configure ADC3 Channel12 */
//ADC3_CH12_DMA_Config();
/* Start ADC3 Software Conversion */
//ADC_SoftwareStartConv(ADC3);
value=4;
while (1)
{
STM_EVAL_LEDOn(LED6);
//Gprs();
//Http();
//ADC3ConvertedVoltage = ADC3ConvertedValue *3300/0xFFF;
SendChar('a');
c3201_CS_LOW();
SendChar('b');
while (SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_RXNE) == RESET);
read=SPI_I2S_ReceiveData(SPI2);
SendChar('d');
c3201_CS_HIGH();
SendChar('e');
SendChar(read);
STM_EVAL_LEDOn(LED5);
//atoi ("456");
//atol (Convert string to long integer)
//atof (Convert string to double)
//strtol (Convert string to long integer)
//SendInt2(value);
//SendChar('a');
/*
SendChar('a');
ADC3ConvertedVoltage = ADC3ConvertedValue *3300/0xFFF;
command=utoa(ADC3ConvertedVoltage);
SendString(command);
SendChar('b');
*/
}
}
/**
* @brief ADC3 channel12 with DMA configuration
* @param None
* @retval None
*/
void ADC3_CH12_DMA_Config(void)
{
ADC_InitTypeDef ADC_InitStructure;
ADC_CommonInitTypeDef ADC_CommonInitStructure;
DMA_InitTypeDef DMA_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
/* Enable ADC3, DMA2 and GPIO clocks ****************************************/
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2 | RCC_AHB1Periph_GPIOC, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC3, ENABLE);
/* DMA2 Stream0 channel0 configuration **************************************/
DMA_InitStructure.DMA_Channel = DMA_Channel_2;
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)ADC3_DR_ADDRESS;
DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&ADC3ConvertedValue;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;
DMA_InitStructure.DMA_BufferSize = 1;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Disable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;
DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;
DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
DMA_Init(DMA2_Stream0, &DMA_InitStructure);
DMA_Cmd(DMA2_Stream0, ENABLE);
/* Configure ADC3 Channel12 pin as analog input ******************************/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_Init(GPIOC, &GPIO_InitStructure);
/* ADC Common Init **********************************************************/
ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;
ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;
ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;
ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;
ADC_CommonInit(&ADC_CommonInitStructure);
/* ADC3 Init ****************************************************************/
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ScanConvMode = DISABLE;
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfConversion = 1;
ADC_Init(ADC3, &ADC_InitStructure);
/* ADC3 regular channel12 configuration *************************************/
ADC_RegularChannelConfig(ADC3, ADC_Channel_12, 1, ADC_SampleTime_3Cycles);
/* Enable DMA request after last transfer (Single-ADC mode) */
ADC_DMARequestAfterLastTransferCmd(ADC3, ENABLE);
/* Enable ADC3 DMA */
ADC_DMACmd(ADC3, ENABLE);
/* Enable ADC3 */
ADC_Cmd(ADC3, ENABLE);
}
/**
* @brief Configures the TIM Peripheral for Led toggling.
* @param None
* @retval None
*/
static void TIM_LED_Config(void)
{
TIM_OCInitTypeDef TIM_OCInitStructure;
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
NVIC_InitTypeDef NVIC_InitStructure;
uint16_t prescalervalue = 0;
/* TIM4 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE);
NVIC_PriorityGroupConfig(NVIC_PriorityGroup_2);
/* Enable the TIM3 gloabal Interrupt */
NVIC_InitStructure.NVIC_IRQChannel = TIM4_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
/* Initialize Leds mounted on STM324F4-EVAL board */
STM_EVAL_LEDInit(LED3);
STM_EVAL_LEDInit(LED4);
STM_EVAL_LEDInit(LED6);
/* Compute the prescaler value */
prescalervalue = (uint16_t) ((SystemCoreClock ) / 550000) - 1;
/* Time base configuration */
TIM_TimeBaseStructure.TIM_Period = 65535;
TIM_TimeBaseStructure.TIM_Prescaler = prescalervalue;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure);
/* Enable TIM4 Preload register on ARR */
TIM_ARRPreloadConfig(TIM4, ENABLE);
/* TIM PWM1 Mode configuration: Channel */
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Timing;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = CCR_Val;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
/* Output Compare PWM1 Mode configuration: Channel2 */
TIM_OC1Init(TIM4, &TIM_OCInitStructure);
TIM_OC1PreloadConfig(TIM4, TIM_OCPreload_Disable);
/* TIM Interrupts enable */
TIM_ITConfig(TIM4, TIM_IT_CC1 , ENABLE);
/* TIM4 enable counter */
TIM_Cmd(TIM4, ENABLE);
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* Infinite loop */
while (1)
{
}
}
#endif
/******************* (C) COPYRIGHT 2011 STMicroelectronics *****END OF FILE****/