/** ****************************************************************************** * @file startup_stm32f334x8.s * @author MCD Application Team * @version V2.3.0 * @date 29-April-2015 * @brief STM32F334x4/STM32F334x6/STM32F334x8 devices vector table for * Atollic TrueSTUDIO toolchain. * This module performs: * - Set the initial SP * - Set the initial PC == Reset_Handler, * - Set the vector table entries with the exceptions ISR address, * - Configure the clock system * - Branches to main in the C library (which eventually * calls main()). * After Reset the Cortex-M4 processor is in Thread mode, * priority is Privileged, and the Stack is set to Main. ****************************************************************************** * * Redistribution and use in source and binary forms, with or without modification, * are permitted provided that the following conditions are met: * 1. Redistributions of source code must retain the above copyright notice, * this list of conditions and the following disclaimer. * 2. Redistributions in binary form must reproduce the above copyright notice, * this list of conditions and the following disclaimer in the documentation * and/or other materials provided with the distribution. * 3. Neither the name of STMicroelectronics nor the names of its contributors * may be used to endorse or promote products derived from this software * without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE * DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE * FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL * DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR * SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER * CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * ****************************************************************************** */ .syntax unified .cpu cortex-m4 .fpu softvfp .thumb .global g_pfnVectors .global Default_Handler /* start address for the initialization values of the .data section. defined in linker script */ .word _sidata /* start address for the .data section. defined in linker script */ .word _sdata /* end address for the .data section. defined in linker script */ .word _edata /* start address for the initialization values of the .ccmidata section. defined in linker script */ .word _siccmram /* start address for the .ccmidata section. defined in linker script */ .word _sccmidata /* end address for the .ccmidata section. defined in linker script */ .word _eccmidata /* start address for the .bss section. defined in linker script */ .word _sbss /* end address for the .bss section. defined in linker script */ .word _ebss .equ BootRAM, 0xF1E0F85F /** * @brief This is the code that gets called when the processor first * starts execution following a reset event. Only the absolutely * necessary set is performed, after which the application * supplied main() routine is called. * @param None * @retval : None */ .section .text.Reset_Handler .weak Reset_Handler .type Reset_Handler, %function Reset_Handler: ldr sp, =_estack /* Atollic update: set stack pointer */ /* Copy the data segment initializers from flash to SRAM */ movs r1, #0 b LoopCopyDataInit CopyDataInit: ldr r3, =_sidata ldr r3, [r3, r1] str r3, [r0, r1] adds r1, r1, #4 LoopCopyDataInit: ldr r0, =_sdata ldr r3, =_edata adds r2, r0, r1 cmp r2, r3 bcc CopyDataInit //ldr r2, =_sbss //b LoopFillZerobss /* Copy the data segment initializers from flash to CCMRAM */ movs r1, #0 b LoopCopyCCMDataInit CopyCCMDataInit: ldr r3, =_siccmram ldr r3, [r3, r1] str r3, [r0, r1] adds r1, r1, #4 LoopCopyCCMDataInit: ldr r0, =_sccmidata ldr r3, =_eccmidata adds r2, r0, r1 cmp r2, r3 bcc CopyCCMDataInit ldr r2, =_sbss b LoopFillZerobss /* Zero fill the bss segment. */ FillZerobss: movs r3, #0 str r3, [r2], #4 LoopFillZerobss: ldr r3, = _ebss cmp r2, r3 bcc FillZerobss ldr r2, =_sccmram b LoopFillZeroCcm /* Zero fill the ccmram segment. */ FillZeroCcm: movs r3, #0 str r3, [r2] adds r2, r2, #4 LoopFillZeroCcm: ldr r3, = _eccmram cmp r2, r3 bcc FillZeroCcm /* Call the clock system intitialization function.*/ bl SystemInit /* Call static constructors */ bl __libc_init_array /* Call the application's entry point.*/ bl main LoopForever: b LoopForever .size Reset_Handler, .-Reset_Handler /** * @brief This is the code that gets called when the processor receives an * unexpected interrupt. This simply enters an infinite loop, preserving * the system state for examination by a debugger. * * @param None * @retval : None */ .section .text.Default_Handler,"ax",%progbits Default_Handler: Infinite_Loop: b Infinite_Loop .size Default_Handler, .-Default_Handler /****************************************************************************** * * The minimal vector table for a Cortex-M4. Note that the proper constructs * must be placed on this to ensure that it ends up at physical address * 0x0000.0000. * ******************************************************************************/ .section .isr_vector,"a",%progbits .type g_pfnVectors, %object .size g_pfnVectors, .-g_pfnVectors g_pfnVectors: .word _estack .word Reset_Handler .word NMI_Handler .word HardFault_Handler .word MemManage_Handler .word BusFault_Handler .word UsageFault_Handler .word 0 .word 0 .word 0 .word 0 .word SVC_Handler .word DebugMon_Handler .word 0 .word PendSV_Handler .word SysTick_Handler .word WWDG_IRQHandler .word PVD_IRQHandler .word TAMP_STAMP_IRQHandler .word RTC_WKUP_IRQHandler .word FLASH_IRQHandler .word RCC_IRQHandler .word EXTI0_IRQHandler .word EXTI1_IRQHandler .word EXTI2_TSC_IRQHandler .word EXTI3_IRQHandler .word EXTI4_IRQHandler .word DMA1_Channel1_IRQHandler .word DMA1_Channel2_IRQHandler .word DMA1_Channel3_IRQHandler .word DMA1_Channel4_IRQHandler .word DMA1_Channel5_IRQHandler .word DMA1_Channel6_IRQHandler .word DMA1_Channel7_IRQHandler .word ADC1_2_IRQHandler .word CAN_TX_IRQHandler .word CAN_RX0_IRQHandler .word CAN_RX1_IRQHandler .word CAN_SCE_IRQHandler .word EXTI9_5_IRQHandler .word TIM1_BRK_TIM15_IRQHandler .word TIM1_UP_TIM16_IRQHandler .word TIM1_TRG_COM_TIM17_IRQHandler .word TIM1_CC_IRQHandler .word TIM2_IRQHandler .word TIM3_IRQHandler .word 0 .word I2C1_EV_IRQHandler .word I2C1_ER_IRQHandler .word 0 .word 0 .word SPI1_IRQHandler .word 0 .word USART1_IRQHandler .word USART2_IRQHandler .word USART3_IRQHandler .word EXTI15_10_IRQHandler .word RTC_Alarm_IRQHandler .word 0 .word 0 .word 0 .word 0 .word 0 .word 0 .word 0 .word 0 .word 0 .word 0 .word 0 .word 0 .word TIM6_DAC1_IRQHandler .word TIM7_DAC2_IRQHandler .word 0 .word 0 .word 0 .word 0 .word 0 .word 0 .word 0 .word 0 .word COMP2_IRQHandler .word COMP4_6_IRQHandler .word 0 .word HRTIM1_Master_IRQHandler .word HRTIM1_TIMA_IRQHandler .word HRTIM1_TIMB_IRQHandler .word HRTIM1_TIMC_IRQHandler .word HRTIM1_TIMD_IRQHandler .word HRTIM1_TIME_IRQHandler .word HRTIM1_FLT_IRQHandler .word 0 .word 0 .word 0 .word 0 .word 0 .word 0 .word 0 .word FPU_IRQHandler /******************************************************************************* * * Provide weak aliases for each Exception handler to the Default_Handler. * As they are weak aliases, any function with the same name will override * this definition. * *******************************************************************************/ .weak NMI_Handler .thumb_set NMI_Handler,Default_Handler .weak HardFault_Handler .thumb_set HardFault_Handler,Default_Handler .weak MemManage_Handler .thumb_set MemManage_Handler,Default_Handler .weak BusFault_Handler .thumb_set BusFault_Handler,Default_Handler .weak UsageFault_Handler .thumb_set UsageFault_Handler,Default_Handler .weak SVC_Handler .thumb_set SVC_Handler,Default_Handler .weak DebugMon_Handler .thumb_set DebugMon_Handler,Default_Handler .weak PendSV_Handler .thumb_set PendSV_Handler,Default_Handler .weak SysTick_Handler .thumb_set SysTick_Handler,Default_Handler .weak WWDG_IRQHandler .thumb_set WWDG_IRQHandler,Default_Handler .weak PVD_IRQHandler .thumb_set PVD_IRQHandler,Default_Handler .weak TAMP_STAMP_IRQHandler .thumb_set TAMP_STAMP_IRQHandler,Default_Handler .weak RTC_WKUP_IRQHandler .thumb_set RTC_WKUP_IRQHandler,Default_Handler .weak FLASH_IRQHandler .thumb_set FLASH_IRQHandler,Default_Handler .weak RCC_IRQHandler .thumb_set RCC_IRQHandler,Default_Handler .weak EXTI0_IRQHandler .thumb_set EXTI0_IRQHandler,Default_Handler .weak EXTI1_IRQHandler .thumb_set EXTI1_IRQHandler,Default_Handler .weak EXTI2_TSC_IRQHandler .thumb_set EXTI2_TSC_IRQHandler,Default_Handler .weak EXTI3_IRQHandler .thumb_set EXTI3_IRQHandler,Default_Handler .weak EXTI4_IRQHandler .thumb_set EXTI4_IRQHandler,Default_Handler .weak DMA1_Channel1_IRQHandler .thumb_set DMA1_Channel1_IRQHandler,Default_Handler .weak DMA1_Channel2_IRQHandler .thumb_set DMA1_Channel2_IRQHandler,Default_Handler .weak DMA1_Channel3_IRQHandler .thumb_set DMA1_Channel3_IRQHandler,Default_Handler .weak DMA1_Channel4_IRQHandler .thumb_set DMA1_Channel4_IRQHandler,Default_Handler .weak DMA1_Channel5_IRQHandler .thumb_set DMA1_Channel5_IRQHandler,Default_Handler .weak DMA1_Channel6_IRQHandler .thumb_set DMA1_Channel6_IRQHandler,Default_Handler .weak DMA1_Channel7_IRQHandler .thumb_set DMA1_Channel7_IRQHandler,Default_Handler .weak ADC1_2_IRQHandler .thumb_set ADC1_2_IRQHandler,Default_Handler .weak CAN_TX_IRQHandler .thumb_set CAN_TX_IRQHandler,Default_Handler .weak CAN_RX0_IRQHandler .thumb_set CAN_RX0_IRQHandler,Default_Handler .weak CAN_RX1_IRQHandler .thumb_set CAN_RX1_IRQHandler,Default_Handler .weak CAN_SCE_IRQHandler .thumb_set CAN_SCE_IRQHandler,Default_Handler .weak EXTI9_5_IRQHandler .thumb_set EXTI9_5_IRQHandler,Default_Handler .weak TIM1_BRK_TIM15_IRQHandler .thumb_set TIM1_BRK_TIM15_IRQHandler,Default_Handler .weak TIM1_UP_TIM16_IRQHandler .thumb_set TIM1_UP_TIM16_IRQHandler,Default_Handler .weak TIM1_TRG_COM_TIM17_IRQHandler .thumb_set TIM1_TRG_COM_TIM17_IRQHandler,Default_Handler .weak TIM1_CC_IRQHandler .thumb_set TIM1_CC_IRQHandler,Default_Handler .weak TIM2_IRQHandler .thumb_set TIM2_IRQHandler,Default_Handler .weak TIM3_IRQHandler .thumb_set TIM3_IRQHandler,Default_Handler .weak I2C1_EV_IRQHandler .thumb_set I2C1_EV_IRQHandler,Default_Handler .weak I2C1_ER_IRQHandler .thumb_set I2C1_ER_IRQHandler,Default_Handler .weak SPI1_IRQHandler .thumb_set SPI1_IRQHandler,Default_Handler .weak USART1_IRQHandler .thumb_set USART1_IRQHandler,Default_Handler .weak USART2_IRQHandler .thumb_set USART2_IRQHandler,Default_Handler .weak USART3_IRQHandler .thumb_set USART3_IRQHandler,Default_Handler .weak EXTI15_10_IRQHandler .thumb_set EXTI15_10_IRQHandler,Default_Handler .weak RTC_Alarm_IRQHandler .thumb_set RTC_Alarm_IRQHandler,Default_Handler .weak TIM6_DAC1_IRQHandler .thumb_set TIM6_DAC1_IRQHandler,Default_Handler .weak TIM7_DAC2_IRQHandler .thumb_set TIM7_DAC2_IRQHandler,Default_Handler .weak COMP2_IRQHandler .thumb_set COMP2_IRQHandler,Default_Handler .weak COMP4_6_IRQHandler .thumb_set COMP4_6_IRQHandler,Default_Handler .weak HRTIM1_Master_IRQHandler .thumb_set HRTIM1_Master_IRQHandler,Default_Handler .weak HRTIM1_TIMA_IRQHandler .thumb_set HRTIM1_TIMA_IRQHandler,Default_Handler .weak HRTIM1_TIMB_IRQHandler .thumb_set HRTIM1_TIMB_IRQHandler,Default_Handler .weak HRTIM1_TIMC_IRQHandler .thumb_set HRTIM1_TIMC_IRQHandler,Default_Handler .weak HRTIM1_TIMD_IRQHandler .thumb_set HRTIM1_TIMD_IRQHandler,Default_Handler .weak HRTIM1_TIME_IRQHandler .thumb_set HRTIM1_TIME_IRQHandler,Default_Handler .weak HRTIM1_FLT_IRQHandler .thumb_set HRTIM1_FLT_IRQHandler,Default_Handler .weak FPU_IRQHandler .thumb_set FPU_IRQHandler,Default_Handler /************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/