Hi everyone;

I found an example in this example it used OV9655 camera and with this camera show environment in external lcd screen with using stm32f407.

I want to use stm32f429 without using external lcd screen however I did not change some important changings the example code is in the below (these tutorial is used OV9655 camera with STM32F407 and external LCD screen).

could anyone help me please... how can show environment in STM32F429 LCD screen...

thank you for your considerations...

#include "OV9655.h"
#include "stm32f4xx.h"
#include "I2C.h"
#include "main.h"

/** @addtogroup DCMI_OV9655_Camera
* @{
*/

/* Private typedef -----------------------------------------------------------*/
RCC_ClocksTypeDef RCC_Clocks;
/* Private define ------------------------------------------------------------*/
#define TIMEOUT 2
#define DCMI_DR_ADDRESS 0x50050028
#define FSMC_LCD_ADDRESS 0x60020000
/* Bits definitions ----------------------------------------------------------*/
/* Private macro -------------------------------------------------------------*/
/* Private variables ---------------------------------------------------------*/
/* Private function prototypes -----------------------------------------------*/
/* Private functions ---------------------------------------------------------*/
/* Pin Map -------------------------------------------------------------------*/
/*
DCMI D0 = PC6
DCMI D1 = PC7
DCMI D2 = PE0
DCMI D3 = PE1
DCMI D4 = PE4
DCMI D5 = PB6
DCMI D6 = PE5
DCMI D7 = PE6
DCMI HSYNC = PA4
DCMI VSYNC = PB7
DCMI XCLK = PC9
DCMI PXCLK = PA6
I2C_SCL = PB8
I2C_SDA = PB9
*/

/**
* @brief Configures the OV9655 DCMI
* @param None
* @retval None
*/
uint8_t OV9655_Configuration(void){
int i=0;
OV9655_IDTypeDef OV9655_ID;
/*OV9655 MCO Configuration*/
OV9655_MCO_Configuration();
/* I2C configuration */
Soft_I2C_Configuration();

for(i=0;i<10000;i++){}
/* Reset and check the presence of the OV9655 camera module */
if (DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x12, 0x80)==0xFF)
{
return (0xFF); //Camera Failed!
}
/* Camera Ok!*/
for(i=0;i<10000;i++){}

DCMI_OV9655_ReadID(&OV9655_ID);

/* OV9655 Camera size setup */
#if defined (QQVGA_SIZE)
DCMI_OV9655_QQVGASizeSetup();
#elif defined (QVGA_SIZE)
DCMI_OV9655_QVGASizeSetup();
#endif
/* Set the RGB565 mode */
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS, OV9655_COM7, 0x63);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS, OV9655_COM15, 0xd0);

/* Invert the HRef signal*/
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS, OV9655_COM10, 0x08);
/* OV9655 Camera DCMI setup */
OV9655_DCMI_Configuration();

return (0x00);
}

/**
* @brief Configures the MCO Module
* @param None
* @retval None
*/
void OV9655_MCO_Configuration(void){
GPIO_InitTypeDef GPIO_InitStructure;

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOC, &GPIO_InitStructure);

GPIO_PinAFConfig(GPIOC, GPIO_PinSource9, GPIO_AF_MCO);

RCC_PLLI2SCmd(DISABLE);

RCC_PLLI2SConfig(240, 5); // 192..432, 2..7, ie range of 27.429 Mhz to 192 MHz
/* PLLI2SSCLK = 240 / 5 = 48Mhz */
/* MCO2 Output Freq = 48 / 2 = 24Mhz*/
RCC_MCO2Config(RCC_MCO2Source_PLLI2SCLK, RCC_MCO2Div_2); // 24 MHz with default PLL fComp

RCC_PLLI2SCmd(ENABLE);

while(RCC_GetFlagStatus(RCC_FLAG_PLLI2SRDY) == RESET);
}

/**
* @brief Configures the DCMI to interface with the OV9655 camera module.
* @param None
* @retval None
*/
void OV9655_DCMI_Configuration(void)
{
DCMI_InitTypeDef DCMI_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
DMA_InitTypeDef DMA_InitStructure;
NVIC_InitTypeDef NVIC_InitStructure;

/* Enable DCMI GPIOs clocks */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC | RCC_AHB1Periph_GPIOE |
RCC_AHB1Periph_GPIOB | RCC_AHB1Periph_GPIOA, ENABLE);

/* Enable DCMI clock */
RCC_AHB2PeriphClockCmd(RCC_AHB2Periph_DCMI, ENABLE);

/* Connect DCMI pins to AF13 ************************************************/
/* PCLK */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_DCMI);
/* D0-D7 */
GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource7, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource0, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource1, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource4, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource6, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource5, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource6, GPIO_AF_DCMI);
/* VSYNC */
GPIO_PinAFConfig(GPIOB, GPIO_PinSource7, GPIO_AF_DCMI);
/* HSYNC */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource4, GPIO_AF_DCMI);

/* DCMI GPIO configuration **************************************************/
/* D0 D1(PC6/7) */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ;
GPIO_Init(GPIOC, &GPIO_InitStructure);

/* D2..D4(PE0/1/4) D6/D7(PE5/6) */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1
| GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_6;
GPIO_Init(GPIOE, &GPIO_InitStructure);

/* D5(PB6), VSYNC(PB7) */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7;
GPIO_Init(GPIOB, &GPIO_InitStructure);

/* PCLK(PA6) HSYNC(PA4)*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_6;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_Init(GPIOA, &GPIO_InitStructure);

/* DCMI configuration *******************************************************/
DCMI_InitStructure.DCMI_CaptureMode = DCMI_CaptureMode_Continuous;
DCMI_InitStructure.DCMI_SynchroMode = DCMI_SynchroMode_Hardware;
DCMI_InitStructure.DCMI_PCKPolarity = DCMI_PCKPolarity_Rising;
DCMI_InitStructure.DCMI_VSPolarity = DCMI_VSPolarity_High;
DCMI_InitStructure.DCMI_HSPolarity = DCMI_HSPolarity_High;
DCMI_InitStructure.DCMI_CaptureRate = DCMI_CaptureRate_All_Frame;
DCMI_InitStructure.DCMI_ExtendedDataMode = DCMI_ExtendedDataMode_8b;

DCMI_Init(&DCMI_InitStructure);

/* DCMI Interrupts config ***************************************************/
//DCMI_ITConfig(DCMI_IT_VSYNC, ENABLE);
//DCMI_ITConfig(DCMI_IT_LINE, ENABLE);
DCMI_ITConfig(DCMI_IT_FRAME, ENABLE);
//DCMI_ITConfig(DCMI_IT_ERR, ENABLE);

NVIC_PriorityGroupConfig(NVIC_PriorityGroup_1);
NVIC_InitStructure.NVIC_IRQChannel = DCMI_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);

/* Configures the DMA2 to transfer Data from DCMI to the LCD ****************/
/* Enable DMA2 clock */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE);

/* DMA2 Stream1 Configuration */
DMA_DeInit(DMA2_Stream1);

DMA_InitStructure.DMA_Channel = DMA_Channel_1;
DMA_InitStructure.DMA_PeripheralBaseAddr = DCMI_DR_ADDRESS;
DMA_InitStructure.DMA_Memory0BaseAddr = FSMC_LCD_ADDRESS;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;
DMA_InitStructure.DMA_BufferSize = 1;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Disable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Word;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Enable;
DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full;
DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;

DMA_Init(DMA2_Stream1, &DMA_InitStructure);
}

/**
* @brief Reset the OV9655 SCCB registers.
* @param None
* @retval None
*/
void DCMI_OV9655_Reset(void)
{
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS, OV9655_COM7, SCCB_REG_RESET);
}
/**
* @brief Set the QVGA size(240*320).
* @param None
* @retval None
*/
void DCMI_OV9655_QVGASizeSetup(void)
{
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x00, 0x12);//
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x01, 0x80);//78
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x02, 0x80);//48
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x03, 0x02);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x04, 0x03);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x05, 0x39);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x06, 0x39);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x07, 0x39);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x08, 0x38);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x09, 0x03);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x0a, 0x96);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x0b, 0x57);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x0c, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x0d, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x0e, 0x01);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x0f, 0x00);//old val 0xc0
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x10, 0x7b);//old val 7b
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x11, 0x00);//old val 0x80
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x12, 0x63);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x13, 0xEF);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x14, 0x2A);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x15, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x16, 0x24);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x17, 0x18);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x18, 0x04);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x19, 0x01);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x1a, 0x81);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x1b, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x1c, 0x7F);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x1d, 0xA2);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x1E, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x1F, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x20, 0x80);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x21, 0x80);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x22, 0x80);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x23, 0x80);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x24, 0x60);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x25, 0x36);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x26, 0x72);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x27, 0x08);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x28, 0x08);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x29, 0x15);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x2a, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x2b, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x2c, 0x08);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x2d, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x2e, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x2f, 0x38);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x30, 0x08);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x31, 0x30);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x32, 0x12);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x33, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x34, 0x3f);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x35, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x36, 0x3a);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x37, 0x04);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x38, 0x72);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x39, 0x57);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x3a, 0xca);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x3b, 0x04);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x3c, 0x0c);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x3d, 0x99);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x3e, 0x02);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x3f, 0xc1);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x40, 0xd0);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x41, 0x41);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x42, 0xc0);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x43, 0x0a);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x44, 0xf0);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x45, 0x46);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x46, 0x62);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x47, 0x2a);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x48, 0x3c);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x49, 0x48);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x4a, 0xec);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x4b, 0xfc);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x4c, 0x7f);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x4d, 0x7f);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x4e, 0x7f);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x4f, 0x98);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x50, 0x98);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x51, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x52, 0x28);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x53, 0x70);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x54, 0x98);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x55, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x56, 0x48);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x57, 0x80);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x58, 0x1a);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x59, 0x85);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x5a, 0xa9);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x5b, 0x64);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x5c, 0x84);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x5d, 0x53);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x5e, 0x0e);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x5f, 0xf0);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x60, 0xf0);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x61, 0xf0);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x62, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x63, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x64, 0x02);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x65, 0x20);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x66, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x67, 0x80);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x68, 0x80);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x69, 0x0a);//
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x6a, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x6b, 0x0a);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x6c, 0x04);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x6d, 0x55);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x6e, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x6f, 0x9d);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x70, 0x21);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x71, 0x78);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x72, 0x11);//
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x73, 0x01);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x74, 0x10);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x75, 0x10);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x76, 0x01);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x77, 0x02);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x78, 0x28);//Test
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x79, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x7A, 0x12);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x7B, 0x08);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x7C, 0x16);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x7D, 0x30);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x7E, 0x5e);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x7F, 0x72);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x80, 0x82);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x81, 0x8e);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x82, 0x9a);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x83, 0xa4);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x84, 0xac);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x85, 0xb8);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x86, 0xc3);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x87, 0xd6);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x88, 0xe6);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x89, 0xf2);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x8a, 0x24);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x8b, 0x04);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x8c, 0x80);
// Delay(TIMEOUT);
// DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x8d, 0x00);
// Delay(TIMEOUT);
// DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x8e, 0x00);
// Delay(TIMEOUT);
// DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x8f, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x90, 0x71);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x91, 0x6f);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x9d, 0x02);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x9e, 0x02);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x9f, 0x7a);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xa0, 0x6D);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xa1, 0x40);//
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xa2, 0x9D);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xa4, 0x50);//50
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xa5, 0x68);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xa6, 0x80);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xa8, 0xc1);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xa9, 0xef);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xaa, 0x92);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xab, 0x04);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xac, 0x80);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xad, 0x80);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xae, 0x80);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xaf, 0x80);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xb2, 0xf2);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xb3, 0x20);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xb4, 0x20);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xb5, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xb6, 0xaf);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xb7, 0xee);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xb8, 0xee);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xb9, 0x0c);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xbb, 0xae);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xbc, 0x7c);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xbd, 0x7d);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xbe, 0x7e);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xbf, 0x7f);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xc0, 0xaa);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xc1, 0xc0);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xc2, 0x01);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xc3, 0x4e);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xc5, 0x2e);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xc6, 0x05);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xc7, 0x81);//81
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xc8, 0x06);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xc9, 0xe0);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xca, 0xe8);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xcb, 0xf0);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xcc, 0xd8);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xcd, 0x93);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xce, 0xe3);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xcf, 0x74);
Delay(TIMEOUT);
}

/**
* @brief Set the QQVGA size(120*160).
* @param None
* @retval None
*/
void DCMI_OV9655_QQVGASizeSetup(void)
{
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x00, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x01, 0x80);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x02, 0x80);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x03, 0x02);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x04, 0x03);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x09, 0x01);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x0b, 0x57);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x0e, 0x61);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x0f, 0x40);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x11, 0x01);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x12, 0x62);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x13, 0xc7);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x14, 0x3a);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x15, 0x08);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x16, 0x24);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x17, 0x18);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x18, 0x04);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x19, 0x01);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x1a, 0x81);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x1e, 0x20);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x24, 0x3c);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x25, 0x36);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x26, 0x72);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x27, 0x08);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x28, 0x08);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x29, 0x15);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x2a, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x2b, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x2c, 0x08);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x32, 0xa4);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x33, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x34, 0x3f);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x35, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x36, 0x3a);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x38, 0x72);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x39, 0x57);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x3a, 0xcc);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x3b, 0x04);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x3d, 0x99);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x3e, 0x0e);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x3f, 0xc1);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x40, 0xc0);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x41, 0x41);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x42, 0xc0);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x43, 0x0a);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x44, 0xf0);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x45, 0x46);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x46, 0x62);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x47, 0x2a);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x48, 0x3c);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x4a, 0xfc);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x4b, 0xfc);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x4c, 0x7f);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x4d, 0x7f);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x4e, 0x7f);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x4f, 0x98);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x50, 0x98);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x51, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x52, 0x28);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x53, 0x70);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x54, 0x98);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x58, 0x1a);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x59, 0x85);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x5a, 0xa9);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x5b, 0x64);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x5c, 0x84);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x5d, 0x53);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x5e, 0x0e);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x5f, 0xf0);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x60, 0xf0);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x61, 0xf0);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x62, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x63, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x64, 0x02);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x65, 0x20);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x66, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x69, 0x0a);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x6b, 0x1a);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x6c, 0x04);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x6d, 0x55);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x6e, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x6f, 0x9d);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x70, 0x21);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x71, 0x78);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x72, 0x22);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x73, 0x02);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x74, 0x10);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x75, 0x10);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x76, 0x01);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x77, 0x02);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x7A, 0x12);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x7B, 0x08);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x7C, 0x16);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x7D, 0x30);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x7E, 0x5e);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x7F, 0x72);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x80, 0x82);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x81, 0x8e);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x82, 0x9a);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x83, 0xa4);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x84, 0xac);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x85, 0xb8);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x86, 0xc3);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x87, 0xd6);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x88, 0xe6);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x89, 0xf2);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x8a, 0x24);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x8c, 0x80);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x90, 0x7d);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x91, 0x7b);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x9d, 0x02);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x9e, 0x02);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0x9f, 0x7a);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xa0, 0x79);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xa1, 0x40);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xa4, 0x50);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xa5, 0x68);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xa6, 0x4a);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xa8, 0xc1);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xa9, 0xef);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xaa, 0x92);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xab, 0x04);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xac, 0x80);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xad, 0x80);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xae, 0x80);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xaf, 0x80);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xb2, 0xf2);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xb3, 0x20);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xb4, 0x20);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xb5, 0x00);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xb6, 0xaf);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xb6, 0xaf);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xbb, 0xae);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xbc, 0x7f);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xbd, 0x7f);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xbe, 0x7f);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xbf, 0x7f);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xbf, 0x7f);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xc0, 0xaa);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xc1, 0xc0);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xc2, 0x01);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xc3, 0x4e);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xc6, 0x05);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xc7, 0x82);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xc9, 0xe0);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xca, 0xe8);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xcb, 0xf0);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xcc, 0xd8);
Delay(TIMEOUT);
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS,0xcd, 0x93);
Delay(TIMEOUT);
}

/**
* @brief Read the OV9655 Manufacturer identifier.
* @param OV9655ID: pointer to the OV9655 Manufacturer identifier.
* @retval None
*/
void DCMI_OV9655_ReadID(OV9655_IDTypeDef* OV9655ID)
{
OV9655ID->Manufacturer_ID1 = DCMI_SingleRandomRead(OV9655_DEVICE_WRITE_ADDRESS, OV9655_MIDH);
OV9655ID->Manufacturer_ID2 = DCMI_SingleRandomRead(OV9655_DEVICE_WRITE_ADDRESS, OV9655_MIDL);
OV9655ID->Version = DCMI_SingleRandomRead(OV9655_DEVICE_WRITE_ADDRESS, OV9655_VER);
OV9655ID->PID = DCMI_SingleRandomRead(OV9655_DEVICE_WRITE_ADDRESS, OV9655_PID);
}

/**
* @brief Set the Internal Clock Prescaler.
* @param OV9655_Prescaler: the new value of the prescaler.
* This parameter can be a value between 0x0 and 0x1F
* @retval None
*/
void DCMI_OV9655_SetPrescaler(uint8_t OV9655_Prescaler)
{
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS, OV9655_CLKRC, OV9655_Prescaler);
}

/**
* @brief Select the Output Format.
* @param OV9655_OuputFormat: the Format of the ouput Data.
* This parameter can be a value between 0x0 and 0x1F
* @arg OUTPUT_FORMAT_RAWRGB_DATA
* @arg OUTPUT_FORMAT_RAWRGB_INTERP
* @arg OUTPUT_FORMAT_YUV
* @arg OUTPUT_FORMAT_RGB
* @retval None
*/
void DCMI_OV9655_SelectOutputFormat(uint8_t OV9655_OuputFormat)
{
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS, OV9655_COM7, OV9655_OuputFormat);
}

/**
* @brief Select the Output Format Resolution.
* @param OV9655_FormatResolution: the Resolution of the ouput Data.
* This parameter can FORMAT_CTRL_15fpsVGA a value between 0x0 and 0x1F
* @arg FORMAT_CTRL_15fpsVGA
* @arg FORMAT_CTRL_30fpsVGA_NoVArioPixel
* @arg FORMAT_CTRL_30fpsVGA_VArioPixel
* @retval None
*/
void DCMI_OV9655_SelectFormatResolution(uint8_t OV9655_FormatResolution)
{
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS, OV9655_COM7, OV9655_FormatResolution);
}

/**
* @brief Set the new value of OV9655 registers
* @param OV9655_Register: the OV9655 Register to be configured.
* @param Register_Val: The new value to be set
* @retval None
*/
void DCMI_OV9655_SetRegister(uint8_t OV9655_Register, uint8_t Register_Val)
{
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS, OV9655_Register, Register_Val);
}

/**
* @brief Select the HREF Control signal option
* @param OV9665_HREFControl: the HREF Control signal option.
* This parameter can FORMAT_CTRL_15fpsVGA a value between 0x0 and 0x1F
* @arg OV9665_HREFControl_Opt1: HREF edge offset to data output.
* @arg OV9665_HREFControl_Opt2: HREF end 3 LSB
* @arg OV9665_HREFControl_Opt3: HREF start 3 LSB
* @retval None
*/
void DCMI_OV9655_HREFControl(uint8_t OV9665_HREFControl)
{
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS, OV9655_HREF, OV9665_HREFControl);
}

/**
* @brief Select the RGB format option
* @param OV9665_RGBOption: the RGB Format option.
* This parameter can FORMAT_CTRL_15fpsVGA a value between 0x0 and 0x1F
* @arg RGB_NORMAL
* @arg RGB_565
* @arg RGB_555
* @retval None
*/
void DCMI_OV9655_SelectRGBOption(uint8_t OV9665_RGBOption)
{
DCMI_SingleRandomWrite(OV9655_DEVICE_WRITE_ADDRESS, OV9655_COM15, OV9665_RGBOption);
}

/**
* @brief Writes a byte at a specific Camera register
* @param Device: OV9655 write address.
* @param Addr: OV9655 register address.
* @param Data: data to be written to the specific register
* @retval None
*/
uint8_t DCMI_SingleRandomWrite(uint8_t Device, uint16_t Addr, uint8_t Data)
{
I2C_Delay();

I2C_Start();
I2C_SendByte(Device);
if(I2C_WaitAck()==0xFF) return(0xFF);
I2C_SendByte(Addr);
if(I2C_WaitAck()==0xFF) return(0xFF);
I2C_SendByte(Data);
if(I2C_WaitAck()==0xFF) return(0xFF);
I2C_Stop();

return(0x00);
}
/**
* @brief Reads a byte from a specific Camera register
* @param Device: OV9655 write address.
* @param Addr: OV9655 register address.
* @retval data read from the specific register
*/
uint8_t DCMI_SingleRandomRead(uint8_t Device, uint16_t Addr)
{
unsigned char Recieved_Data=0;
I2C_Delay();
I2C_Start();
I2C_SendByte(Device);
if(I2C_WaitAck()==0xFF) return(0xFF);
I2C_SendByte(Addr);
if(I2C_WaitAck()==0xFF) return(0xFF);
I2C_Stop();
I2C_Start();
I2C_SendByte(Device+1);
if(I2C_WaitAck()==0xFF) return(0xFF);
Recieved_Data=I2C_ReceiveByte();
I2C_Stop();
return Recieved_Data;
}