/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2025 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ #include "AD5263.h" #include "stdio.h" #include "string.h" /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ I2C_HandleTypeDef hi2c3; UART_HandleTypeDef huart4; /* USER CODE BEGIN PV */ extern uint8_t _O1, _O2; AD5263_t potentiometer; /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_UART4_Init(void); static void MX_I2C3_Init(void); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ int _write(int file, char *ptr, int len) { HAL_UART_Transmit(&huart4, (uint8_t*) ptr, (uint16_t) len, 50); return len; } /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_UART4_Init(); MX_I2C3_Init(); /* USER CODE BEGIN 2 */ HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, 1); HAL_GPIO_WritePin(LED2_GPIO_Port, LED2_Pin, 1); potentiometer.hi2c = &hi2c3; // Point to your I2C handle potentiometer.address = 0x2F; // Set the correct I2C address - AD0 =AD1=1 HAL_GPIO_WritePin(DIS_GPIO_Port, DIS_Pin, 1); //I2C HAL_GPIO_WritePin(AD0_GPIO_Port, AD0_Pin, 1); HAL_GPIO_WritePin(AD1_GPIO_Port, AD1_Pin, 1); I2C_Scan(&hi2c3); if (AD5263_SetAll(&potentiometer, 0) != 0) { printf("Failed to set all RDACs\n"); } /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ for (uint8_t i = 0; i < 255; i++) { if (AD5263_Write(&potentiometer, 0, i) != 0) { printf("Failed to write value %d to RDAC 0\n", i); } if (AD5263_Write(&potentiometer, 1, i) != 0) { printf("Failed to write value %d to RDAC 1\n", i); } if (AD5263_Write(&potentiometer, 2, i) != 0) { printf("Failed to write value %d to RDAC 2\n", i); } // if (AD5263_Write(&potentiometer, 3, i) != 0) { // printf("Failed to write value %d to RDAC 3\n", i); // } HAL_Delay(100); } } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Configure the main internal regulator output voltage */ __HAL_RCC_PWR_CLK_ENABLE(); __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1); /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK) { Error_Handler(); } } /** * @brief I2C3 Initialization Function * @param None * @retval None */ static void MX_I2C3_Init(void) { /* USER CODE BEGIN I2C3_Init 0 */ /* USER CODE END I2C3_Init 0 */ /* USER CODE BEGIN I2C3_Init 1 */ /* USER CODE END I2C3_Init 1 */ hi2c3.Instance = I2C3; hi2c3.Init.ClockSpeed = 400000; hi2c3.Init.DutyCycle = I2C_DUTYCYCLE_2; hi2c3.Init.OwnAddress1 = 0; hi2c3.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT; hi2c3.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE; hi2c3.Init.OwnAddress2 = 0; hi2c3.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE; hi2c3.Init.NoStretchMode = I2C_NOSTRETCH_ENABLE; if (HAL_I2C_Init(&hi2c3) != HAL_OK) { Error_Handler(); } /** Configure Analogue filter */ if (HAL_I2CEx_ConfigAnalogFilter(&hi2c3, I2C_ANALOGFILTER_ENABLE) != HAL_OK) { Error_Handler(); } /** Configure Digital filter */ if (HAL_I2CEx_ConfigDigitalFilter(&hi2c3, 0) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN I2C3_Init 2 */ /* USER CODE END I2C3_Init 2 */ } /** * @brief UART4 Initialization Function * @param None * @retval None */ static void MX_UART4_Init(void) { /* USER CODE BEGIN UART4_Init 0 */ /* USER CODE END UART4_Init 0 */ /* USER CODE BEGIN UART4_Init 1 */ /* USER CODE END UART4_Init 1 */ huart4.Instance = UART4; huart4.Init.BaudRate = 115200; huart4.Init.WordLength = UART_WORDLENGTH_8B; huart4.Init.StopBits = UART_STOPBITS_1; huart4.Init.Parity = UART_PARITY_NONE; huart4.Init.Mode = UART_MODE_TX_RX; huart4.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart4.Init.OverSampling = UART_OVERSAMPLING_16; if (HAL_UART_Init(&huart4) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN UART4_Init 2 */ /* USER CODE END UART4_Init 2 */ } /** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* USER CODE BEGIN MX_GPIO_Init_1 */ /* USER CODE END MX_GPIO_Init_1 */ /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOA, AD0_Pin|DIS_Pin, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(AD1_GPIO_Port, AD1_Pin, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOB, LED2_Pin|LED1_Pin, GPIO_PIN_RESET); /*Configure GPIO pins : AD0_Pin DIS_Pin */ GPIO_InitStruct.Pin = AD0_Pin|DIS_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /*Configure GPIO pin : AD1_Pin */ GPIO_InitStruct.Pin = AD1_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(AD1_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pins : LED2_Pin LED1_Pin */ GPIO_InitStruct.Pin = LED2_Pin|LED1_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); /* USER CODE BEGIN MX_GPIO_Init_2 */ /* USER CODE END MX_GPIO_Init_2 */ } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */