------------------------------------------------------------------- STM32CubeProgrammer v2.4.0 ------------------------------------------------------------------- Serial Port COM3 is successfully opened. Port configuration: parity = even, baudrate = 57600, data-bit = 8, stop-bit = 1.0, flow-control = off Activating device: OK Chip ID: 0x413 BootLoader protocol version: 3.1 Device name : STM32F405xx/F407xx/F415xx/F417xx Flash size : 1 MBytes (default) Device type : MCU Device CPU : Cortex-M4 UPLOADING ... File : test.hex Size : 1024 Bytes Address: : 0x8000000 Read progress: Error: Upload size is bigger than flash memory size.