> .\bin\STM32_Programmer_CLI.exe -c port=COM3 br=57600 P=EVEN db=8 sb=1 -w .\firmware_fails.hex -vb 3 ------------------------------------------------------------------- STM32CubeProgrammer v2.4.0 ------------------------------------------------------------------- Serial Port COM3 is successfully opened. Port configuration: parity = even, baudrate = 57600, data-bit = 8, stop-bit = 1.0, flow-control = off No Init bits value is : 0 Sending init command: byte 0x7F sent successfully to target Wait ends after 1 loop, dataready = 1, delay = 0 Received response from target: 0x79 Activating device: OK Sending GetID command and its XOR: byte 0x02 sent successfully to target byte 0xFD sent successfully to target Wait ends after 1 loop, dataready = 1, delay = 0 Received response from target: 0x79 Received response from target: 0x01041379 Chip ID: 0x413 Sending Get command and its XOR: byte 0x00 sent successfully to target byte 0xFF sent successfully to target Wait ends after 1 loop, dataready = 1, delay = 0 Received response from target: 0x79 Received response from target: 0x0b size of bytes in the response: 11 Received response from target: 0x31000102112131446373829279 Full received response: 0b31000102112131446373829279 BootLoader protocol version: 3.1 byte 0x11 sent successfully to target byte 0xEE sent successfully to target data sent successfully to target: 0x0800000008 byte 0x00 sent successfully to target byte 0xFF sent successfully to target Sending GetID command and its XOR: byte 0x02 sent successfully to target byte 0xFD sent successfully to target Wait ends after 1 loop, dataready = 1, delay = 0 Received response from target: 0x79 Received response from target: 0x01041379 byte 0x11 sent successfully to target byte 0xEE sent successfully to target data sent successfully to target: 0x0800000008 byte 0x00 sent successfully to target byte 0xFF sent successfully to target Memory Programming ... Opening and parsing file: firmware_fails.hex File : firmware_fails.hex Size : 1022 Bytes Address : 0x08000000 Erasing Segment <0> Address <0x08000000> Size <1022>Bytes Erasing memory corresponding to segment 0: erase: 0000ms