/**
******************************************************************************
* @file stm32l4xx_hal_conf.h
* @author MCD Application Team
* @brief HAL configuration template file.
* This file should be copied to the application folder and renamed
* to stm32l4xx_hal_conf.h.
******************************************************************************
* @attention
*
*
© Copyright (c) 2017 STMicroelectronics.
* All rights reserved.
*
* This software component is licensed by ST under BSD 3-Clause license,
* the "License"; You may not use this file except in compliance with the
* License. You may obtain a copy of the License at:
* opensource.org/licenses/BSD-3-Clause
*
******************************************************************************
*/
/* Define to prevent recursive inclusion -------------------------------------*/
#ifndef STM32L4xx_HAL_CONF_H
#define STM32L4xx_HAL_CONF_H
#ifdef __cplusplus
extern "C" {
#endif
/* Exported types ------------------------------------------------------------*/
/* Exported constants --------------------------------------------------------*/
/* ########################## Module Selection ############################## */
/**
* @brief This is the list of modules to be used in the HAL driver
*/
#define HAL_MODULE_ENABLED
/*#define HAL_ADC_MODULE_ENABLED */
/*#define HAL_CRYP_MODULE_ENABLED */
/*#define HAL_CAN_MODULE_ENABLED */
/*#define HAL_COMP_MODULE_ENABLED */
/*#define HAL_CRC_MODULE_ENABLED */
/*#define HAL_CRYP_MODULE_ENABLED */
/*#define HAL_DAC_MODULE_ENABLED */
/*#define HAL_DCMI_MODULE_ENABLED */
/*#define HAL_DMA2D_MODULE_ENABLED */
/*#define HAL_DFSDM_MODULE_ENABLED */
/*#define HAL_DSI_MODULE_ENABLED */
/*#define HAL_FIREWALL_MODULE_ENABLED */
/*#define HAL_GFXMMU_MODULE_ENABLED */
/*#define HAL_HCD_MODULE_ENABLED */
/*#define HAL_HASH_MODULE_ENABLED */
/*#define HAL_I2S_MODULE_ENABLED */
/*#define HAL_IRDA_MODULE_ENABLED */
/*#define HAL_IWDG_MODULE_ENABLED */
/*#define HAL_LTDC_MODULE_ENABLED */
/*#define HAL_LCD_MODULE_ENABLED */
/*#define HAL_LPTIM_MODULE_ENABLED */
/*#define HAL_MMC_MODULE_ENABLED */
/*#define HAL_NAND_MODULE_ENABLED */
/*#define HAL_NOR_MODULE_ENABLED */
/*#define HAL_OPAMP_MODULE_ENABLED */
/*#define HAL_OSPI_MODULE_ENABLED */
/*#define HAL_OSPI_MODULE_ENABLED */
/*#define HAL_PCD_MODULE_ENABLED */
/*#define HAL_PKA_MODULE_ENABLED */
/*#define HAL_QSPI_MODULE_ENABLED */
/*#define HAL_QSPI_MODULE_ENABLED */
/*#define HAL_RNG_MODULE_ENABLED */
/*#define HAL_RTC_MODULE_ENABLED */
/*#define HAL_SAI_MODULE_ENABLED */
/*#define HAL_SD_MODULE_ENABLED */
/*#define HAL_SMBUS_MODULE_ENABLED */
/*#define HAL_SMARTCARD_MODULE_ENABLED */
/*#define HAL_SPI_MODULE_ENABLED */
/*#define HAL_SRAM_MODULE_ENABLED */
/*#define HAL_SWPMI_MODULE_ENABLED */
#define HAL_TIM_MODULE_ENABLED
/*#define HAL_TSC_MODULE_ENABLED */
/*#define HAL_UART_MODULE_ENABLED */
/*#define HAL_USART_MODULE_ENABLED */
/*#define HAL_WWDG_MODULE_ENABLED */
/*#define HAL_EXTI_MODULE_ENABLED */
/*#define HAL_PSSI_MODULE_ENABLED */
#define HAL_GPIO_MODULE_ENABLED
#define HAL_EXTI_MODULE_ENABLED
#define HAL_I2C_MODULE_ENABLED
#define HAL_DMA_MODULE_ENABLED
#define HAL_RCC_MODULE_ENABLED
#define HAL_FLASH_MODULE_ENABLED
#define HAL_PWR_MODULE_ENABLED
#define HAL_CORTEX_MODULE_ENABLED
/* ########################## Oscillator Values adaptation ####################*/
/**
* @brief Adjust the value of External High Speed oscillator (HSE) used in your application.
* This value is used by the RCC HAL module to compute the system frequency
* (when HSE is used as system clock source, directly or through the PLL).
*/
#if !defined (HSE_VALUE)
#define HSE_VALUE ((uint32_t)8000000U) /*!< Value of the External oscillator in Hz */
#endif /* HSE_VALUE */
#if !defined (HSE_STARTUP_TIMEOUT)
#define HSE_STARTUP_TIMEOUT ((uint32_t)100U) /*!< Time out for HSE start up, in ms */
#endif /* HSE_STARTUP_TIMEOUT */
/**
* @brief Internal Multiple Speed oscillator (MSI) default value.
* This value is the default MSI range value after Reset.
*/
#if !defined (MSI_VALUE)
#define MSI_VALUE ((uint32_t)4000000U) /*!< Value of the Internal oscillator in Hz*/
#endif /* MSI_VALUE */
/**
* @brief Internal High Speed oscillator (HSI) value.
* This value is used by the RCC HAL module to compute the system frequency
* (when HSI is used as system clock source, directly or through the PLL).
*/
#if !defined (HSI_VALUE)
#define HSI_VALUE ((uint32_t)16000000U) /*!< Value of the Internal oscillator in Hz*/
#endif /* HSI_VALUE */
/**
* @brief Internal High Speed oscillator (HSI48) value for USB FS, SDMMC and RNG.
* This internal oscillator is mainly dedicated to provide a high precision clock to
* the USB peripheral by means of a special Clock Recovery System (CRS) circuitry.
* When the CRS is not used, the HSI48 RC oscillator runs on it default frequency
* which is subject to manufacturing process variations.
*/
#if !defined (HSI48_VALUE)
#define HSI48_VALUE ((uint32_t)48000000U) /*!< Value of the Internal High Speed oscillator for USB FS/SDMMC/RNG in Hz.
The real value my vary depending on manufacturing process variations.*/
#endif /* HSI48_VALUE */
/**
* @brief Internal Low Speed oscillator (LSI) value.
*/
#if !defined (LSI_VALUE)
#define LSI_VALUE 32000U /*!< LSI Typical Value in Hz*/
#endif /* LSI_VALUE */ /*!< Value of the Internal Low Speed oscillator in Hz
The real value may vary depending on the variations
in voltage and temperature.*/
/**
* @brief External Low Speed oscillator (LSE) value.
* This value is used by the UART, RTC HAL module to compute the system frequency
*/
#if !defined (LSE_VALUE)
#define LSE_VALUE 32768U /*!< Value of the External oscillator in Hz*/
#endif /* LSE_VALUE */
#if !defined (LSE_STARTUP_TIMEOUT)
#define LSE_STARTUP_TIMEOUT 5000U /*!< Time out for LSE start up, in ms */
#endif /* HSE_STARTUP_TIMEOUT */
/**
* @brief External clock source for SAI1 peripheral
* This value is used by the RCC HAL module to compute the SAI1 & SAI2 clock source
* frequency.
*/
#if !defined (EXTERNAL_SAI1_CLOCK_VALUE)
#define EXTERNAL_SAI1_CLOCK_VALUE 48000U /*!< Value of the SAI1 External clock source in Hz*/
#endif /* EXTERNAL_SAI1_CLOCK_VALUE */
/**
* @brief External clock source for SAI2 peripheral
* This value is used by the RCC HAL module to compute the SAI1 & SAI2 clock source
* frequency.
*/
#if !defined (EXTERNAL_SAI2_CLOCK_VALUE)
#define EXTERNAL_SAI2_CLOCK_VALUE 48000U /*!< Value of the SAI2 External clock source in Hz*/
#endif /* EXTERNAL_SAI2_CLOCK_VALUE */
/* Tip: To avoid modifying this file each time you need to use different HSE,
=== you can define the HSE value in your toolchain compiler preprocessor. */
/* ########################### System Configuration ######################### */
/**
* @brief This is the HAL system configuration section
*/
#define VDD_VALUE 3300U /*!< Value of VDD in mv */
#define TICK_INT_PRIORITY 0U /*!< tick interrupt priority */
#define USE_RTOS 0U
#define PREFETCH_ENABLE 0U
#define INSTRUCTION_CACHE_ENABLE 1U
#define DATA_CACHE_ENABLE 1U
/* ########################## Assert Selection ############################## */
/**
* @brief Uncomment the line below to expanse the "assert_param" macro in the
* HAL drivers code
*/
#define USE_FULL_ASSERT 1U
/* ################## Register callback feature configuration ############### */
/**
* @brief Set below the peripheral configuration to "1U" to add the support
* of HAL callback registration/deregistration feature for the HAL
* driver(s). This allows user application to provide specific callback
* functions thanks to HAL_PPP_RegisterCallback() rather than overwriting
* the default weak callback functions (see each stm32l4xx_hal_ppp.h file
* for possible callback identifiers defined in HAL_PPP_CallbackIDTypeDef
* for each PPP peripheral).
*/
#define USE_HAL_ADC_REGISTER_CALLBACKS 0U
#define USE_HAL_CAN_REGISTER_CALLBACKS 0U
#define USE_HAL_COMP_REGISTER_CALLBACKS 0U
#define USE_HAL_CRYP_REGISTER_CALLBACKS 0U
#define USE_HAL_DAC_REGISTER_CALLBACKS 0U
#define USE_HAL_DCMI_REGISTER_CALLBACKS 0U
#define USE_HAL_DFSDM_REGISTER_CALLBACKS 0U
#define USE_HAL_DMA2D_REGISTER_CALLBACKS 0U
#define USE_HAL_DSI_REGISTER_CALLBACKS 0U
#define USE_HAL_GFXMMU_REGISTER_CALLBACKS 0U
#define USE_HAL_HASH_REGISTER_CALLBACKS 0U
#define USE_HAL_HCD_REGISTER_CALLBACKS 0U
#define USE_HAL_I2C_REGISTER_CALLBACKS 0U
#define USE_HAL_IRDA_REGISTER_CALLBACKS 0U
#define USE_HAL_LPTIM_REGISTER_CALLBACKS 0U
#define USE_HAL_LTDC_REGISTER_CALLBACKS 0U
#define USE_HAL_MMC_REGISTER_CALLBACKS 0U
#define USE_HAL_OPAMP_REGISTER_CALLBACKS 0U
#define USE_HAL_OSPI_REGISTER_CALLBACKS 0U
#define USE_HAL_PCD_REGISTER_CALLBACKS 0U
#define USE_HAL_QSPI_REGISTER_CALLBACKS 0U
#define USE_HAL_RNG_REGISTER_CALLBACKS 0U
#define USE_HAL_RTC_REGISTER_CALLBACKS 0U
#define USE_HAL_SAI_REGISTER_CALLBACKS 0U
#define USE_HAL_SD_REGISTER_CALLBACKS 0U
#define USE_HAL_SMARTCARD_REGISTER_CALLBACKS 0U
#define USE_HAL_SMBUS_REGISTER_CALLBACKS 0U
#define USE_HAL_SPI_REGISTER_CALLBACKS 0U
#define USE_HAL_SWPMI_REGISTER_CALLBACKS 0U
#define USE_HAL_TIM_REGISTER_CALLBACKS 0U
#define USE_HAL_TSC_REGISTER_CALLBACKS 0U
#define USE_HAL_UART_REGISTER_CALLBACKS 0U
#define USE_HAL_USART_REGISTER_CALLBACKS 0U
#define USE_HAL_WWDG_REGISTER_CALLBACKS 0U
/* ################## SPI peripheral configuration ########################## */
/* CRC FEATURE: Use to activate CRC feature inside HAL SPI Driver
* Activated: CRC code is present inside driver
* Deactivated: CRC code cleaned from driver
*/
#define USE_SPI_CRC 0U
/* Includes ------------------------------------------------------------------*/
/**
* @brief Include module's header file
*/
#ifdef HAL_RCC_MODULE_ENABLED
#include "stm32l4xx_hal_rcc.h"
#endif /* HAL_RCC_MODULE_ENABLED */
#ifdef HAL_GPIO_MODULE_ENABLED
#include "stm32l4xx_hal_gpio.h"
#endif /* HAL_GPIO_MODULE_ENABLED */
#ifdef HAL_DMA_MODULE_ENABLED
#include "stm32l4xx_hal_dma.h"
#endif /* HAL_DMA_MODULE_ENABLED */
#ifdef HAL_DFSDM_MODULE_ENABLED
#include "stm32l4xx_hal_dfsdm.h"
#endif /* HAL_DFSDM_MODULE_ENABLED */
#ifdef HAL_CORTEX_MODULE_ENABLED
#include "stm32l4xx_hal_cortex.h"
#endif /* HAL_CORTEX_MODULE_ENABLED */
#ifdef HAL_ADC_MODULE_ENABLED
#include "stm32l4xx_hal_adc.h"
#endif /* HAL_ADC_MODULE_ENABLED */
#ifdef HAL_CAN_MODULE_ENABLED
#include "stm32l4xx_hal_can.h"
#endif /* HAL_CAN_MODULE_ENABLED */
#ifdef HAL_CAN_LEGACY_MODULE_ENABLED
#include "Legacy/stm32l4xx_hal_can_legacy.h"
#endif /* HAL_CAN_LEGACY_MODULE_ENABLED */
#ifdef HAL_COMP_MODULE_ENABLED
#include "stm32l4xx_hal_comp.h"
#endif /* HAL_COMP_MODULE_ENABLED */
#ifdef HAL_CRC_MODULE_ENABLED
#include "stm32l4xx_hal_crc.h"
#endif /* HAL_CRC_MODULE_ENABLED */
#ifdef HAL_CRYP_MODULE_ENABLED
#include "stm32l4xx_hal_cryp.h"
#endif /* HAL_CRYP_MODULE_ENABLED */
#ifdef HAL_DAC_MODULE_ENABLED
#include "stm32l4xx_hal_dac.h"
#endif /* HAL_DAC_MODULE_ENABLED */
#ifdef HAL_DCMI_MODULE_ENABLED
#include "stm32l4xx_hal_dcmi.h"
#endif /* HAL_DCMI_MODULE_ENABLED */
#ifdef HAL_DMA2D_MODULE_ENABLED
#include "stm32l4xx_hal_dma2d.h"
#endif /* HAL_DMA2D_MODULE_ENABLED */
#ifdef HAL_DSI_MODULE_ENABLED
#include "stm32l4xx_hal_dsi.h"
#endif /* HAL_DSI_MODULE_ENABLED */
#ifdef HAL_EXTI_MODULE_ENABLED
#include "stm32l4xx_hal_exti.h"
#endif /* HAL_EXTI_MODULE_ENABLED */
#ifdef HAL_GFXMMU_MODULE_ENABLED
#include "stm32l4xx_hal_gfxmmu.h"
#endif /* HAL_GFXMMU_MODULE_ENABLED */
#ifdef HAL_FIREWALL_MODULE_ENABLED
#include "stm32l4xx_hal_firewall.h"
#endif /* HAL_FIREWALL_MODULE_ENABLED */
#ifdef HAL_FLASH_MODULE_ENABLED
#include "stm32l4xx_hal_flash.h"
#endif /* HAL_FLASH_MODULE_ENABLED */
#ifdef HAL_HASH_MODULE_ENABLED
#include "stm32l4xx_hal_hash.h"
#endif /* HAL_HASH_MODULE_ENABLED */
#ifdef HAL_HCD_MODULE_ENABLED
#include "stm32l4xx_hal_hcd.h"
#endif /* HAL_HCD_MODULE_ENABLED */
#ifdef HAL_I2C_MODULE_ENABLED
#include "stm32l4xx_hal_i2c.h"
#endif /* HAL_I2C_MODULE_ENABLED */
#ifdef HAL_IRDA_MODULE_ENABLED
#include "stm32l4xx_hal_irda.h"
#endif /* HAL_IRDA_MODULE_ENABLED */
#ifdef HAL_IWDG_MODULE_ENABLED
#include "stm32l4xx_hal_iwdg.h"
#endif /* HAL_IWDG_MODULE_ENABLED */
#ifdef HAL_LCD_MODULE_ENABLED
#include "stm32l4xx_hal_lcd.h"
#endif /* HAL_LCD_MODULE_ENABLED */
#ifdef HAL_LPTIM_MODULE_ENABLED
#include "stm32l4xx_hal_lptim.h"
#endif /* HAL_LPTIM_MODULE_ENABLED */
#ifdef HAL_LTDC_MODULE_ENABLED
#include "stm32l4xx_hal_ltdc.h"
#endif /* HAL_LTDC_MODULE_ENABLED */
#ifdef HAL_MMC_MODULE_ENABLED
#include "stm32l4xx_hal_mmc.h"
#endif /* HAL_MMC_MODULE_ENABLED */
#ifdef HAL_NAND_MODULE_ENABLED
#include "stm32l4xx_hal_nand.h"
#endif /* HAL_NAND_MODULE_ENABLED */
#ifdef HAL_NOR_MODULE_ENABLED
#include "stm32l4xx_hal_nor.h"
#endif /* HAL_NOR_MODULE_ENABLED */
#ifdef HAL_OPAMP_MODULE_ENABLED
#include "stm32l4xx_hal_opamp.h"
#endif /* HAL_OPAMP_MODULE_ENABLED */
#ifdef HAL_OSPI_MODULE_ENABLED
#include "stm32l4xx_hal_ospi.h"
#endif /* HAL_OSPI_MODULE_ENABLED */
#ifdef HAL_PCD_MODULE_ENABLED
#include "stm32l4xx_hal_pcd.h"
#endif /* HAL_PCD_MODULE_ENABLED */
#ifdef HAL_PKA_MODULE_ENABLED
#include "stm32l4xx_hal_pka.h"
#endif /* HAL_PKA_MODULE_ENABLED */
#ifdef HAL_PSSI_MODULE_ENABLED
#include "stm32l4xx_hal_pssi.h"
#endif /* HAL_PSSI_MODULE_ENABLED */
#ifdef HAL_PWR_MODULE_ENABLED
#include "stm32l4xx_hal_pwr.h"
#endif /* HAL_PWR_MODULE_ENABLED */
#ifdef HAL_QSPI_MODULE_ENABLED
#include "stm32l4xx_hal_qspi.h"
#endif /* HAL_QSPI_MODULE_ENABLED */
#ifdef HAL_RNG_MODULE_ENABLED
#include "stm32l4xx_hal_rng.h"
#endif /* HAL_RNG_MODULE_ENABLED */
#ifdef HAL_RTC_MODULE_ENABLED
#include "stm32l4xx_hal_rtc.h"
#endif /* HAL_RTC_MODULE_ENABLED */
#ifdef HAL_SAI_MODULE_ENABLED
#include "stm32l4xx_hal_sai.h"
#endif /* HAL_SAI_MODULE_ENABLED */
#ifdef HAL_SD_MODULE_ENABLED
#include "stm32l4xx_hal_sd.h"
#endif /* HAL_SD_MODULE_ENABLED */
#ifdef HAL_SMARTCARD_MODULE_ENABLED
#include "stm32l4xx_hal_smartcard.h"
#endif /* HAL_SMARTCARD_MODULE_ENABLED */
#ifdef HAL_SMBUS_MODULE_ENABLED
#include "stm32l4xx_hal_smbus.h"
#endif /* HAL_SMBUS_MODULE_ENABLED */
#ifdef HAL_SPI_MODULE_ENABLED
#include "stm32l4xx_hal_spi.h"
#endif /* HAL_SPI_MODULE_ENABLED */
#ifdef HAL_SRAM_MODULE_ENABLED
#include "stm32l4xx_hal_sram.h"
#endif /* HAL_SRAM_MODULE_ENABLED */
#ifdef HAL_SWPMI_MODULE_ENABLED
#include "stm32l4xx_hal_swpmi.h"
#endif /* HAL_SWPMI_MODULE_ENABLED */
#ifdef HAL_TIM_MODULE_ENABLED
#include "stm32l4xx_hal_tim.h"
#endif /* HAL_TIM_MODULE_ENABLED */
#ifdef HAL_TSC_MODULE_ENABLED
#include "stm32l4xx_hal_tsc.h"
#endif /* HAL_TSC_MODULE_ENABLED */
#ifdef HAL_UART_MODULE_ENABLED
#include "stm32l4xx_hal_uart.h"
#endif /* HAL_UART_MODULE_ENABLED */
#ifdef HAL_USART_MODULE_ENABLED
#include "stm32l4xx_hal_usart.h"
#endif /* HAL_USART_MODULE_ENABLED */
#ifdef HAL_WWDG_MODULE_ENABLED
#include "stm32l4xx_hal_wwdg.h"
#endif /* HAL_WWDG_MODULE_ENABLED */
/* Exported macro ------------------------------------------------------------*/
#ifdef USE_FULL_ASSERT
/**
* @brief The assert_param macro is used for function's parameters check.
* @param expr If expr is false, it calls assert_failed function
* which reports the name of the source file and the source
* line number of the call that failed.
* If expr is true, it returns no value.
* @retval None
*/
#define assert_param(expr) ((expr) ? (void)0U : assert_failed((uint8_t *)__FILE__, __LINE__))
/* Exported functions ------------------------------------------------------- */
void assert_failed(uint8_t *file, uint32_t line);
#else
#define assert_param(expr) ((void)0U)
#endif /* USE_FULL_ASSERT */
#ifdef __cplusplus
}
#endif
#endif /* STM32L4xx_HAL_CONF_H */
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/