/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file stm32l4xx_hal_timebase_TIM.c * @brief HAL time base based on the hardware TIM. ****************************************************************************** * @attention * * Copyright (c) 2023 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "stm32l4xx_hal.h" #include "stm32l4xx_hal_tim.h" /* Private typedef -----------------------------------------------------------*/ /* Private define ------------------------------------------------------------*/ /* Private macro -------------------------------------------------------------*/ /* Private variables ---------------------------------------------------------*/ TIM_HandleTypeDef htim2; /* Private function prototypes -----------------------------------------------*/ /* Private functions ---------------------------------------------------------*/ /** * @brief This function configures the TIM2 as a time base source. * The time source is configured to have 1ms time base with a dedicated * Tick interrupt priority. * @note This function is called automatically at the beginning of program after * reset by HAL_Init() or at any time when clock is configured, by HAL_RCC_ClockConfig(). * @param TickPriority: Tick interrupt priority. * @retval HAL status */ HAL_StatusTypeDef HAL_InitTick(uint32_t TickPriority) { RCC_ClkInitTypeDef clkconfig; uint32_t uwTimclock = 0; uint32_t uwPrescalerValue = 0; uint32_t pFLatency; /*Configure the TIM2 IRQ priority */ HAL_NVIC_SetPriority(TIM2_IRQn, TickPriority ,0); /* Enable the TIM2 global Interrupt */ HAL_NVIC_EnableIRQ(TIM2_IRQn); /* Enable TIM2 clock */ __HAL_RCC_TIM2_CLK_ENABLE(); /* Get clock configuration */ HAL_RCC_GetClockConfig(&clkconfig, &pFLatency); /* Compute TIM2 clock */ uwTimclock = 2*HAL_RCC_GetPCLK1Freq(); /* Compute the prescaler value to have TIM2 counter clock equal to 1MHz */ uwPrescalerValue = (uint32_t) ((uwTimclock / 1000000U) - 1U); /* Initialize TIM2 */ htim2.Instance = TIM2; /* Initialize TIMx peripheral as follow: + Period = [(TIM2CLK/1000) - 1]. to have a (1/1000) s time base. + Prescaler = (uwTimclock/1000000 - 1) to have a 1MHz counter clock. + ClockDivision = 0 + Counter direction = Up */ htim2.Init.Period = (1000000U / 1000U) - 1U; htim2.Init.Prescaler = uwPrescalerValue; htim2.Init.ClockDivision = 0; htim2.Init.CounterMode = TIM_COUNTERMODE_UP; if(HAL_TIM_Base_Init(&htim2) == HAL_OK) { /* Start the TIM time Base generation in interrupt mode */ return HAL_TIM_Base_Start_IT(&htim2); } /* Return function status */ return HAL_ERROR; } /** * @brief Suspend Tick increment. * @note Disable the tick increment by disabling TIM2 update interrupt. * @param None * @retval None */ void HAL_SuspendTick(void) { /* Disable TIM2 update Interrupt */ __HAL_TIM_DISABLE_IT(&htim2, TIM_IT_UPDATE); } /** * @brief Resume Tick increment. * @note Enable the tick increment by Enabling TIM2 update interrupt. * @param None * @retval None */ void HAL_ResumeTick(void) { /* Enable TIM2 Update interrupt */ __HAL_TIM_ENABLE_IT(&htim2, TIM_IT_UPDATE); }