/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * *

© Copyright (c) 2021 STMicroelectronics. * All rights reserved.

* * This software component is licensed by ST under BSD 3-Clause license, * the "License"; You may not use this file except in compliance with the * License. You may obtain a copy of the License at: * opensource.org/licenses/BSD-3-Clause * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ ADC_HandleTypeDef hadc1; ADC_HandleTypeDef hadc2; ADC_HandleTypeDef hadc3; ADC_HandleTypeDef hadc5; HRTIM_HandleTypeDef hhrtim1; UART_HandleTypeDef hlpuart1; /* USER CODE BEGIN PV */ /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_ADC1_Init(void); static void MX_ADC2_Init(void); static void MX_ADC3_Init(void); static void MX_ADC5_Init(void); static void MX_HRTIM1_Init(void); static void MX_LPUART1_UART_Init(void); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_ADC1_Init(); MX_ADC2_Init(); MX_ADC3_Init(); MX_ADC5_Init(); MX_HRTIM1_Init(); MX_LPUART1_UART_Init(); /* USER CODE BEGIN 2 */ /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; RCC_PeriphCLKInitTypeDef PeriphClkInit = {0}; /** Configure the main internal regulator output voltage */ HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1_BOOST); /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI; RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV4; RCC_OscInitStruct.PLL.PLLN = 85; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2; RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK) { Error_Handler(); } /** Initializes the peripherals clocks */ PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_LPUART1|RCC_PERIPHCLK_ADC12 |RCC_PERIPHCLK_ADC345; PeriphClkInit.Lpuart1ClockSelection = RCC_LPUART1CLKSOURCE_PCLK1; PeriphClkInit.Adc12ClockSelection = RCC_ADC12CLKSOURCE_SYSCLK; PeriphClkInit.Adc345ClockSelection = RCC_ADC345CLKSOURCE_SYSCLK; if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK) { Error_Handler(); } } /** * @brief ADC1 Initialization Function * @param None * @retval None */ static void MX_ADC1_Init(void) { /* USER CODE BEGIN ADC1_Init 0 */ /* USER CODE END ADC1_Init 0 */ ADC_MultiModeTypeDef multimode = {0}; ADC_InjectionConfTypeDef sConfigInjected = {0}; /* USER CODE BEGIN ADC1_Init 1 */ /* USER CODE END ADC1_Init 1 */ /** Common config */ hadc1.Instance = ADC1; hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4; hadc1.Init.Resolution = ADC_RESOLUTION_12B; hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc1.Init.GainCompensation = 0; hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE; hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV; hadc1.Init.LowPowerAutoWait = DISABLE; hadc1.Init.ContinuousConvMode = DISABLE; hadc1.Init.NbrOfConversion = 1; hadc1.Init.DiscontinuousConvMode = DISABLE; hadc1.Init.DMAContinuousRequests = DISABLE; hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED; hadc1.Init.OversamplingMode = DISABLE; if (HAL_ADC_Init(&hadc1) != HAL_OK) { Error_Handler(); } /** Configure the ADC multi-mode */ multimode.Mode = ADC_MODE_INDEPENDENT; if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK) { Error_Handler(); } /** Configure Injected Channel */ sConfigInjected.InjectedChannel = ADC_CHANNEL_1; sConfigInjected.InjectedRank = ADC_INJECTED_RANK_1; sConfigInjected.InjectedSamplingTime = ADC_SAMPLETIME_2CYCLES_5; sConfigInjected.InjectedSingleDiff = ADC_SINGLE_ENDED; sConfigInjected.InjectedOffsetNumber = ADC_OFFSET_NONE; sConfigInjected.InjectedOffset = 0; sConfigInjected.InjectedNbrOfConversion = 2; sConfigInjected.InjectedDiscontinuousConvMode = DISABLE; sConfigInjected.AutoInjectedConv = DISABLE; sConfigInjected.QueueInjectedContext = DISABLE; sConfigInjected.ExternalTrigInjecConv = ADC_EXTERNALTRIGINJEC_HRTIM_TRG2; sConfigInjected.ExternalTrigInjecConvEdge = ADC_EXTERNALTRIGINJECCONV_EDGE_RISING; sConfigInjected.InjecOversamplingMode = DISABLE; if (HAL_ADCEx_InjectedConfigChannel(&hadc1, &sConfigInjected) != HAL_OK) { Error_Handler(); } /** Configure Injected Channel */ sConfigInjected.InjectedChannel = ADC_CHANNEL_2; sConfigInjected.InjectedRank = ADC_INJECTED_RANK_2; if (HAL_ADCEx_InjectedConfigChannel(&hadc1, &sConfigInjected) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN ADC1_Init 2 */ /* USER CODE END ADC1_Init 2 */ } /** * @brief ADC2 Initialization Function * @param None * @retval None */ static void MX_ADC2_Init(void) { /* USER CODE BEGIN ADC2_Init 0 */ /* USER CODE END ADC2_Init 0 */ ADC_InjectionConfTypeDef sConfigInjected = {0}; /* USER CODE BEGIN ADC2_Init 1 */ /* USER CODE END ADC2_Init 1 */ /** Common config */ hadc2.Instance = ADC2; hadc2.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4; hadc2.Init.Resolution = ADC_RESOLUTION_12B; hadc2.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc2.Init.GainCompensation = 0; hadc2.Init.ScanConvMode = ADC_SCAN_ENABLE; hadc2.Init.EOCSelection = ADC_EOC_SINGLE_CONV; hadc2.Init.LowPowerAutoWait = DISABLE; hadc2.Init.ContinuousConvMode = DISABLE; hadc2.Init.NbrOfConversion = 1; hadc2.Init.DiscontinuousConvMode = DISABLE; hadc2.Init.DMAContinuousRequests = DISABLE; hadc2.Init.Overrun = ADC_OVR_DATA_PRESERVED; hadc2.Init.OversamplingMode = DISABLE; if (HAL_ADC_Init(&hadc2) != HAL_OK) { Error_Handler(); } /** Configure Injected Channel */ sConfigInjected.InjectedChannel = ADC_CHANNEL_3; sConfigInjected.InjectedRank = ADC_INJECTED_RANK_1; sConfigInjected.InjectedSamplingTime = ADC_SAMPLETIME_2CYCLES_5; sConfigInjected.InjectedSingleDiff = ADC_SINGLE_ENDED; sConfigInjected.InjectedOffsetNumber = ADC_OFFSET_NONE; sConfigInjected.InjectedOffset = 0; sConfigInjected.InjectedNbrOfConversion = 2; sConfigInjected.InjectedDiscontinuousConvMode = DISABLE; sConfigInjected.AutoInjectedConv = DISABLE; sConfigInjected.QueueInjectedContext = DISABLE; sConfigInjected.ExternalTrigInjecConv = ADC_EXTERNALTRIGINJEC_HRTIM_TRG2; sConfigInjected.ExternalTrigInjecConvEdge = ADC_EXTERNALTRIGINJECCONV_EDGE_RISING; sConfigInjected.InjecOversamplingMode = DISABLE; if (HAL_ADCEx_InjectedConfigChannel(&hadc2, &sConfigInjected) != HAL_OK) { Error_Handler(); } /** Configure Injected Channel */ sConfigInjected.InjectedChannel = ADC_CHANNEL_4; sConfigInjected.InjectedRank = ADC_INJECTED_RANK_2; if (HAL_ADCEx_InjectedConfigChannel(&hadc2, &sConfigInjected) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN ADC2_Init 2 */ /* USER CODE END ADC2_Init 2 */ } /** * @brief ADC3 Initialization Function * @param None * @retval None */ static void MX_ADC3_Init(void) { /* USER CODE BEGIN ADC3_Init 0 */ /* USER CODE END ADC3_Init 0 */ ADC_MultiModeTypeDef multimode = {0}; ADC_InjectionConfTypeDef sConfigInjected = {0}; /* USER CODE BEGIN ADC3_Init 1 */ /* USER CODE END ADC3_Init 1 */ /** Common config */ hadc3.Instance = ADC3; hadc3.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4; hadc3.Init.Resolution = ADC_RESOLUTION_12B; hadc3.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc3.Init.GainCompensation = 0; hadc3.Init.ScanConvMode = ADC_SCAN_ENABLE; hadc3.Init.EOCSelection = ADC_EOC_SINGLE_CONV; hadc3.Init.LowPowerAutoWait = DISABLE; hadc3.Init.ContinuousConvMode = DISABLE; hadc3.Init.NbrOfConversion = 1; hadc3.Init.DiscontinuousConvMode = DISABLE; hadc3.Init.DMAContinuousRequests = DISABLE; hadc3.Init.Overrun = ADC_OVR_DATA_PRESERVED; hadc3.Init.OversamplingMode = DISABLE; if (HAL_ADC_Init(&hadc3) != HAL_OK) { Error_Handler(); } /** Configure the ADC multi-mode */ multimode.Mode = ADC_MODE_INDEPENDENT; if (HAL_ADCEx_MultiModeConfigChannel(&hadc3, &multimode) != HAL_OK) { Error_Handler(); } /** Configure Injected Channel */ sConfigInjected.InjectedChannel = ADC_CHANNEL_1; sConfigInjected.InjectedRank = ADC_INJECTED_RANK_1; sConfigInjected.InjectedSamplingTime = ADC_SAMPLETIME_2CYCLES_5; sConfigInjected.InjectedSingleDiff = ADC_SINGLE_ENDED; sConfigInjected.InjectedOffsetNumber = ADC_OFFSET_NONE; sConfigInjected.InjectedOffset = 0; sConfigInjected.InjectedNbrOfConversion = 2; sConfigInjected.InjectedDiscontinuousConvMode = DISABLE; sConfigInjected.AutoInjectedConv = DISABLE; sConfigInjected.QueueInjectedContext = DISABLE; sConfigInjected.ExternalTrigInjecConv = ADC_EXTERNALTRIGINJEC_HRTIM_TRG3; sConfigInjected.ExternalTrigInjecConvEdge = ADC_EXTERNALTRIGINJECCONV_EDGE_RISING; sConfigInjected.InjecOversamplingMode = DISABLE; if (HAL_ADCEx_InjectedConfigChannel(&hadc3, &sConfigInjected) != HAL_OK) { Error_Handler(); } /** Configure Injected Channel */ sConfigInjected.InjectedChannel = ADC_CHANNEL_12; sConfigInjected.InjectedRank = ADC_INJECTED_RANK_2; if (HAL_ADCEx_InjectedConfigChannel(&hadc3, &sConfigInjected) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN ADC3_Init 2 */ /* USER CODE END ADC3_Init 2 */ } /** * @brief ADC5 Initialization Function * @param None * @retval None */ static void MX_ADC5_Init(void) { /* USER CODE BEGIN ADC5_Init 0 */ /* USER CODE END ADC5_Init 0 */ ADC_InjectionConfTypeDef sConfigInjected = {0}; /* USER CODE BEGIN ADC5_Init 1 */ /* USER CODE END ADC5_Init 1 */ /** Common config */ hadc5.Instance = ADC5; hadc5.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4; hadc5.Init.Resolution = ADC_RESOLUTION_12B; hadc5.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc5.Init.GainCompensation = 0; hadc5.Init.ScanConvMode = ADC_SCAN_ENABLE; hadc5.Init.EOCSelection = ADC_EOC_SINGLE_CONV; hadc5.Init.LowPowerAutoWait = DISABLE; hadc5.Init.ContinuousConvMode = DISABLE; hadc5.Init.NbrOfConversion = 1; hadc5.Init.DiscontinuousConvMode = DISABLE; hadc5.Init.DMAContinuousRequests = DISABLE; hadc5.Init.Overrun = ADC_OVR_DATA_PRESERVED; hadc5.Init.OversamplingMode = DISABLE; if (HAL_ADC_Init(&hadc5) != HAL_OK) { Error_Handler(); } /** Configure Injected Channel */ sConfigInjected.InjectedChannel = ADC_CHANNEL_VBAT; sConfigInjected.InjectedRank = ADC_INJECTED_RANK_1; sConfigInjected.InjectedSamplingTime = ADC_SAMPLETIME_2CYCLES_5; sConfigInjected.InjectedSingleDiff = ADC_SINGLE_ENDED; sConfigInjected.InjectedOffsetNumber = ADC_OFFSET_NONE; sConfigInjected.InjectedOffset = 0; sConfigInjected.InjectedNbrOfConversion = 2; sConfigInjected.InjectedDiscontinuousConvMode = DISABLE; sConfigInjected.AutoInjectedConv = DISABLE; sConfigInjected.QueueInjectedContext = DISABLE; sConfigInjected.ExternalTrigInjecConv = ADC_EXTERNALTRIGINJEC_HRTIM_TRG3; sConfigInjected.ExternalTrigInjecConvEdge = ADC_EXTERNALTRIGINJECCONV_EDGE_RISING; sConfigInjected.InjecOversamplingMode = DISABLE; if (HAL_ADCEx_InjectedConfigChannel(&hadc5, &sConfigInjected) != HAL_OK) { Error_Handler(); } /** Configure Injected Channel */ sConfigInjected.InjectedChannel = ADC_CHANNEL_VREFINT; sConfigInjected.InjectedRank = ADC_INJECTED_RANK_2; if (HAL_ADCEx_InjectedConfigChannel(&hadc5, &sConfigInjected) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN ADC5_Init 2 */ /* USER CODE END ADC5_Init 2 */ } /** * @brief HRTIM1 Initialization Function * @param None * @retval None */ static void MX_HRTIM1_Init(void) { /* USER CODE BEGIN HRTIM1_Init 0 */ /* USER CODE END HRTIM1_Init 0 */ HRTIM_ADCTriggerCfgTypeDef pADCTriggerCfg = {0}; HRTIM_TimeBaseCfgTypeDef pTimeBaseCfg = {0}; HRTIM_TimerCfgTypeDef pTimerCfg = {0}; HRTIM_CompareCfgTypeDef pCompareCfg = {0}; HRTIM_TimerCtlTypeDef pTimerCtl = {0}; HRTIM_DeadTimeCfgTypeDef pDeadTimeCfg = {0}; HRTIM_OutputCfgTypeDef pOutputCfg = {0}; /* USER CODE BEGIN HRTIM1_Init 1 */ /* USER CODE END HRTIM1_Init 1 */ hhrtim1.Instance = HRTIM1; hhrtim1.Init.HRTIMInterruptResquests = HRTIM_IT_NONE; hhrtim1.Init.SyncOptions = HRTIM_SYNCOPTION_NONE; if (HAL_HRTIM_Init(&hhrtim1) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_DLLCalibrationStart(&hhrtim1, HRTIM_CALIBRATIONRATE_3) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_PollForDLLCalibration(&hhrtim1, 10) != HAL_OK) { Error_Handler(); } pADCTriggerCfg.UpdateSource = HRTIM_ADCTRIGGERUPDATE_MASTER; pADCTriggerCfg.Trigger = HRTIM_ADCTRIGGEREVENT24_TIMERA_CMP4|HRTIM_ADCTRIGGEREVENT24_TIMERD_CMP4; if (HAL_HRTIM_ADCTriggerConfig(&hhrtim1, HRTIM_ADCTRIGGER_2, &pADCTriggerCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_ADCPostScalerConfig(&hhrtim1, HRTIM_ADCTRIGGER_2, 0x0) != HAL_OK) { Error_Handler(); } pADCTriggerCfg.Trigger = HRTIM_ADCTRIGGEREVENT13_TIMERC_CMP4|HRTIM_ADCTRIGGEREVENT13_TIMERE_CMP4; if (HAL_HRTIM_ADCTriggerConfig(&hhrtim1, HRTIM_ADCTRIGGER_3, &pADCTriggerCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_ADCPostScalerConfig(&hhrtim1, HRTIM_ADCTRIGGER_3, 0x0) != HAL_OK) { Error_Handler(); } pTimeBaseCfg.Period = 0xFFDF; pTimeBaseCfg.RepetitionCounter = 0x00; pTimeBaseCfg.PrescalerRatio = HRTIM_PRESCALERRATIO_MUL32; pTimeBaseCfg.Mode = HRTIM_MODE_CONTINUOUS; if (HAL_HRTIM_TimeBaseConfig(&hhrtim1, HRTIM_TIMERINDEX_MASTER, &pTimeBaseCfg) != HAL_OK) { Error_Handler(); } pTimerCfg.InterruptRequests = HRTIM_MASTER_IT_NONE; pTimerCfg.DMARequests = HRTIM_MASTER_DMA_NONE; pTimerCfg.DMASrcAddress = 0x0000; pTimerCfg.DMADstAddress = 0x0000; pTimerCfg.DMASize = 0x1; pTimerCfg.HalfModeEnable = HRTIM_HALFMODE_DISABLED; pTimerCfg.InterleavedMode = HRTIM_INTERLEAVED_MODE_DISABLED; pTimerCfg.StartOnSync = HRTIM_SYNCSTART_DISABLED; pTimerCfg.ResetOnSync = HRTIM_SYNCRESET_DISABLED; pTimerCfg.DACSynchro = HRTIM_DACSYNC_NONE; pTimerCfg.PreloadEnable = HRTIM_PRELOAD_DISABLED; pTimerCfg.UpdateGating = HRTIM_UPDATEGATING_INDEPENDENT; pTimerCfg.BurstMode = HRTIM_TIMERBURSTMODE_MAINTAINCLOCK; pTimerCfg.RepetitionUpdate = HRTIM_UPDATEONREPETITION_DISABLED; pTimerCfg.ReSyncUpdate = HRTIM_TIMERESYNC_UPDATE_UNCONDITIONAL; if (HAL_HRTIM_WaveformTimerConfig(&hhrtim1, HRTIM_TIMERINDEX_MASTER, &pTimerCfg) != HAL_OK) { Error_Handler(); } pCompareCfg.CompareValue = 0xFFDF; if (HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_MASTER, HRTIM_COMPAREUNIT_1, &pCompareCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_MASTER, HRTIM_COMPAREUNIT_2, &pCompareCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_MASTER, HRTIM_COMPAREUNIT_3, &pCompareCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_MASTER, HRTIM_COMPAREUNIT_4, &pCompareCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_TimeBaseConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_A, &pTimeBaseCfg) != HAL_OK) { Error_Handler(); } pTimerCtl.UpDownMode = HRTIM_TIMERUPDOWNMODE_UP; pTimerCtl.TrigHalf = HRTIM_TIMERTRIGHALF_DISABLED; pTimerCtl.GreaterCMP3 = HRTIM_TIMERGTCMP3_EQUAL; pTimerCtl.GreaterCMP1 = HRTIM_TIMERGTCMP1_EQUAL; pTimerCtl.DualChannelDacEnable = HRTIM_TIMER_DCDE_DISABLED; if (HAL_HRTIM_WaveformTimerControl(&hhrtim1, HRTIM_TIMERINDEX_TIMER_A, &pTimerCtl) != HAL_OK) { Error_Handler(); } pTimerCfg.InterruptRequests = HRTIM_TIM_IT_CMP3; pTimerCfg.DMARequests = HRTIM_TIM_DMA_NONE; pTimerCfg.PreloadEnable = HRTIM_PRELOAD_ENABLED; pTimerCfg.PushPull = HRTIM_TIMPUSHPULLMODE_DISABLED; pTimerCfg.FaultEnable = HRTIM_TIMFAULTENABLE_NONE; pTimerCfg.FaultLock = HRTIM_TIMFAULTLOCK_READWRITE; pTimerCfg.DeadTimeInsertion = HRTIM_TIMDEADTIMEINSERTION_ENABLED; pTimerCfg.DelayedProtectionMode = HRTIM_TIMER_A_B_C_DELAYEDPROTECTION_DISABLED; pTimerCfg.UpdateTrigger = HRTIM_TIMUPDATETRIGGER_NONE; pTimerCfg.ResetTrigger = HRTIM_TIMRESETTRIGGER_MASTER_CMP1; pTimerCfg.ResetUpdate = HRTIM_TIMUPDATEONRESET_ENABLED; if (HAL_HRTIM_WaveformTimerConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_A, &pTimerCfg) != HAL_OK) { Error_Handler(); } pTimerCfg.ResetTrigger = HRTIM_TIMRESETTRIGGER_MASTER_CMP2; if (HAL_HRTIM_WaveformTimerConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_C, &pTimerCfg) != HAL_OK) { Error_Handler(); } pTimerCfg.DelayedProtectionMode = HRTIM_TIMER_D_E_DELAYEDPROTECTION_DISABLED; pTimerCfg.ResetTrigger = HRTIM_TIMRESETTRIGGER_MASTER_CMP3; if (HAL_HRTIM_WaveformTimerConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_D, &pTimerCfg) != HAL_OK) { Error_Handler(); } pTimerCfg.InterruptRequests = HRTIM_MASTER_IT_NONE; pTimerCfg.ResetTrigger = HRTIM_TIMRESETTRIGGER_MASTER_CMP4; if (HAL_HRTIM_WaveformTimerConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_E, &pTimerCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_A, HRTIM_COMPAREUNIT_1, &pCompareCfg) != HAL_OK) { Error_Handler(); } pCompareCfg.AutoDelayedMode = HRTIM_AUTODELAYEDMODE_REGULAR; pCompareCfg.AutoDelayedTimeout = 0x0000; if (HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_A, HRTIM_COMPAREUNIT_2, &pCompareCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_A, HRTIM_COMPAREUNIT_3, &pCompareCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_A, HRTIM_COMPAREUNIT_4, &pCompareCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_C, HRTIM_COMPAREUNIT_4, &pCompareCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_D, HRTIM_COMPAREUNIT_4, &pCompareCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_E, HRTIM_COMPAREUNIT_4, &pCompareCfg) != HAL_OK) { Error_Handler(); } pDeadTimeCfg.Prescaler = HRTIM_TIMDEADTIME_PRESCALERRATIO_MUL8; pDeadTimeCfg.RisingValue = 0x000; pDeadTimeCfg.RisingSign = HRTIM_TIMDEADTIME_RISINGSIGN_POSITIVE; pDeadTimeCfg.RisingLock = HRTIM_TIMDEADTIME_RISINGLOCK_WRITE; pDeadTimeCfg.RisingSignLock = HRTIM_TIMDEADTIME_RISINGSIGNLOCK_WRITE; pDeadTimeCfg.FallingValue = 0x000; pDeadTimeCfg.FallingSign = HRTIM_TIMDEADTIME_FALLINGSIGN_POSITIVE; pDeadTimeCfg.FallingLock = HRTIM_TIMDEADTIME_FALLINGLOCK_WRITE; pDeadTimeCfg.FallingSignLock = HRTIM_TIMDEADTIME_FALLINGSIGNLOCK_WRITE; if (HAL_HRTIM_DeadTimeConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_A, &pDeadTimeCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_DeadTimeConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_C, &pDeadTimeCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_DeadTimeConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_D, &pDeadTimeCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_DeadTimeConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_E, &pDeadTimeCfg) != HAL_OK) { Error_Handler(); } pOutputCfg.Polarity = HRTIM_OUTPUTPOLARITY_HIGH; pOutputCfg.SetSource = HRTIM_OUTPUTSET_MASTERCMP1; pOutputCfg.ResetSource = HRTIM_OUTPUTRESET_TIMCMP1|HRTIM_OUTPUTRESET_TIMCMP2; pOutputCfg.IdleMode = HRTIM_OUTPUTIDLEMODE_NONE; pOutputCfg.IdleLevel = HRTIM_OUTPUTIDLELEVEL_INACTIVE; pOutputCfg.FaultLevel = HRTIM_OUTPUTFAULTLEVEL_NONE; pOutputCfg.ChopperModeEnable = HRTIM_OUTPUTCHOPPERMODE_DISABLED; pOutputCfg.BurstModeEntryDelayed = HRTIM_OUTPUTBURSTMODEENTRY_REGULAR; if (HAL_HRTIM_WaveformOutputConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_A, HRTIM_OUTPUT_TA1, &pOutputCfg) != HAL_OK) { Error_Handler(); } pOutputCfg.SetSource = HRTIM_OUTPUTSET_MASTERCMP2; if (HAL_HRTIM_WaveformOutputConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_C, HRTIM_OUTPUT_TC1, &pOutputCfg) != HAL_OK) { Error_Handler(); } pOutputCfg.SetSource = HRTIM_OUTPUTSET_MASTERCMP3; if (HAL_HRTIM_WaveformOutputConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_D, HRTIM_OUTPUT_TD1, &pOutputCfg) != HAL_OK) { Error_Handler(); } pOutputCfg.SetSource = HRTIM_OUTPUTSET_MASTERCMP4; if (HAL_HRTIM_WaveformOutputConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_E, HRTIM_OUTPUT_TE1, &pOutputCfg) != HAL_OK) { Error_Handler(); } pOutputCfg.SetSource = HRTIM_OUTPUTSET_NONE; pOutputCfg.ResetSource = HRTIM_OUTPUTRESET_NONE; if (HAL_HRTIM_WaveformOutputConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_A, HRTIM_OUTPUT_TA2, &pOutputCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformOutputConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_C, HRTIM_OUTPUT_TC2, &pOutputCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformOutputConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_D, HRTIM_OUTPUT_TD2, &pOutputCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformOutputConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_E, HRTIM_OUTPUT_TE2, &pOutputCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_TimeBaseConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_C, &pTimeBaseCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformTimerControl(&hhrtim1, HRTIM_TIMERINDEX_TIMER_C, &pTimerCtl) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_C, HRTIM_COMPAREUNIT_1, &pCompareCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_C, HRTIM_COMPAREUNIT_2, &pCompareCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_C, HRTIM_COMPAREUNIT_3, &pCompareCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_TimeBaseConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_D, &pTimeBaseCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformTimerControl(&hhrtim1, HRTIM_TIMERINDEX_TIMER_D, &pTimerCtl) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_D, HRTIM_COMPAREUNIT_1, &pCompareCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_D, HRTIM_COMPAREUNIT_2, &pCompareCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_D, HRTIM_COMPAREUNIT_3, &pCompareCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_TimeBaseConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_E, &pTimeBaseCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformTimerControl(&hhrtim1, HRTIM_TIMERINDEX_TIMER_E, &pTimerCtl) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_E, HRTIM_COMPAREUNIT_1, &pCompareCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_E, HRTIM_COMPAREUNIT_2, &pCompareCfg) != HAL_OK) { Error_Handler(); } if (HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_E, HRTIM_COMPAREUNIT_3, &pCompareCfg) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN HRTIM1_Init 2 */ /* USER CODE END HRTIM1_Init 2 */ HAL_HRTIM_MspPostInit(&hhrtim1); } /** * @brief LPUART1 Initialization Function * @param None * @retval None */ static void MX_LPUART1_UART_Init(void) { /* USER CODE BEGIN LPUART1_Init 0 */ /* USER CODE END LPUART1_Init 0 */ /* USER CODE BEGIN LPUART1_Init 1 */ /* USER CODE END LPUART1_Init 1 */ hlpuart1.Instance = LPUART1; hlpuart1.Init.BaudRate = 115200; hlpuart1.Init.WordLength = UART_WORDLENGTH_8B; hlpuart1.Init.StopBits = UART_STOPBITS_1; hlpuart1.Init.Parity = UART_PARITY_NONE; hlpuart1.Init.Mode = UART_MODE_TX_RX; hlpuart1.Init.HwFlowCtl = UART_HWCONTROL_NONE; hlpuart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; hlpuart1.Init.ClockPrescaler = UART_PRESCALER_DIV1; hlpuart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; if (HAL_UART_Init(&hlpuart1) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_SetTxFifoThreshold(&hlpuart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_SetRxFifoThreshold(&hlpuart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_DisableFifoMode(&hlpuart1) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN LPUART1_Init 2 */ /* USER CODE END LPUART1_Init 2 */ } /** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOF_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOC, GPO_ISR2_Pin|GPO_ISR1_Pin|GPO_ISR3_Pin|GPO_ISR4_Pin, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET); /*Configure GPIO pin : B1_Pin */ GPIO_InitStruct.Pin = B1_Pin; GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pins : GPO_ISR2_Pin GPO_ISR1_Pin GPO_ISR3_Pin GPO_ISR4_Pin */ GPIO_InitStruct.Pin = GPO_ISR2_Pin|GPO_ISR1_Pin|GPO_ISR3_Pin|GPO_ISR4_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); /*Configure GPIO pin : LD2_Pin */ GPIO_InitStruct.Pin = LD2_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(LD2_GPIO_Port, &GPIO_InitStruct); /* EXTI interrupt init*/ HAL_NVIC_SetPriority(EXTI15_10_IRQn, 0, 0); HAL_NVIC_EnableIRQ(EXTI15_10_IRQn); } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */ /************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/