Console ErrorMessage: Open On-Chip Debugger 0.12.0-00017-gb153daa14 (2023-02-03-14:58) [https://github.com/STMicroelectronics/OpenOCD] Licensed under GNU GPL v2 For bug reports, read http://openocd.org/doc/doxygen/bugs.html swv Info : Listening on port 6666 for tcl connections Info : Listening on port 4444 for telnet connections Info : STLINK V2J41S7 (API v2) VID:PID 0483:3748 Info : Target voltage: 3.248073 Info : Unable to match requested speed 8000 kHz, using 4000 kHz Info : Unable to match requested speed 8000 kHz, using 4000 kHz Info : clock speed 4000 kHz Info : stlink_dap_op_connect(connect) Info : SWD DPIDR 0x6ba02477 Info : [STM32H7A3LIHxQ.cm7] Cortex-M7 r1p1 processor detected Info : [STM32H7A3LIHxQ.cm7] target has 8 breakpoints, 4 watchpoints Info : gdb port disabled Info : starting gdb server for STM32H7A3LIHxQ.cm7 on 3333 Info : Listening on port 3333 for gdb connections Info : [STM32H7A3LIHxQ.cm7] external reset detected Info : accepting 'gdb' connection on tcp/3333 [STM32H7A3LIHxQ.cm7] halted due to debug-request, current mode: Thread xPSR: 0x01000000 pc: 0x08009ffc msp: 0x24100000 Info : Unable to match requested speed 8000 kHz, using 4000 kHz Info : Unable to match requested speed 8000 kHz, using 4000 kHz Info : Device: STM32H7Ax/7Bx Info : flash size probed value 2048k Info : STM32H7 flash has dual banks Info : Bank (0) size is 1024 kb, base address is 0x08000000 Info : Device: STM32H7Ax/7Bx Info : flash size probed value 2048k Info : STM32H7 flash has dual banks Info : Bank (1) size is 1024 kb, base address is 0x08100000 Info : New GDB Connection: 1, Target STM32H7A3LIHxQ.cm7, state: halted Info : accepting 'gdb' connection on tcp/3333 Info : New GDB Connection: 2, Target STM32H7A3LIHxQ.cm7, state: halted Info : starting trace server for STM32H7A3LIHxQ.swo on 3344 Info : Listening on port 3344 for tpiu_swo_trace connections Info : accepting 'tpiu_swo_trace' connection on tcp/3344 [STM32H7A3LIHxQ.cm7] halted due to debug-request, current mode: Thread xPSR: 0x01000000 pc: 0x08009ffc msp: 0x24100000 Info : Unable to match requested speed 8000 kHz, using 4000 kHz Info : Unable to match requested speed 8000 kHz, using 4000 kHz Info : Padding image section 0 at 0x080002ac with 4 bytes [STM32H7A3LIHxQ.cm7] halted due to debug-request, current mode: Thread xPSR: 0x01000000 pc: 0x08009ffc msp: 0x24100000 Warn : target STM32H7A3LIHxQ.cm7 is not halted (gdb fileio) Polling target STM32H7A3LIHxQ.cm7 failed, trying to reexamine Error: Fail reading CTRL/STAT register. Force reconnect Examination failed, GDB will be halted. Polling again in 100ms Error: Fail reading CTRL/STAT register. Force reconnect Info : stlink_dap_op_connect(reconnect) Error: Failed to read memory and, additionally, failed to find out where Error: Fail reading CTRL/STAT register. Force reconnect Polling target STM32H7A3LIHxQ.cm7 failed, trying to reexamine Error: Fail reading CTRL/STAT register. Force reconnect Examination failed, GDB will be halted. Polling again in 300ms Error: libusb_bulk_read error: LIBUSB_ERROR_TIMEOUT Error: bulk trace read failed Warn : keep_alive() was not invoked in the 1000 ms timelimit. GDB alive packet not sent! (6125 ms). Workaround: increase "set remotetimeout" in GDB (MessageEnd)