/* USER CODE BEGIN Header */ /** ****************************************************************************** * File Name : LWIP.c * Description : This file provides initialization code for LWIP * middleWare. ****************************************************************************** * @attention * * Copyright (c) 2024 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "lwip.h" #include "lwip/init.h" #include "lwip/netif.h" #if defined ( __CC_ARM ) /* MDK ARM Compiler */ #include "lwip/sio.h" #endif /* MDK ARM Compiler */ #include "ethernetif.h" /* USER CODE BEGIN 0 */ /* USER CODE END 0 */ /* Private function prototypes -----------------------------------------------*/ static void ethernet_link_status_updated(struct netif *netif); static void Ethernet_Link_Periodic_Handle(struct netif *netif); /* ETH Variables initialization ----------------------------------------------*/ void Error_Handler(void); /* USER CODE BEGIN 1 */ void print_status(uint8_t status); /* USER CODE END 1 */ uint32_t EthernetLinkTimer; /* Variables Initialization */ struct netif gnetif; ip4_addr_t ipaddr; ip4_addr_t netmask; ip4_addr_t gw; uint8_t IP_ADDRESS[4]; uint8_t NETMASK_ADDRESS[4]; uint8_t GATEWAY_ADDRESS[4]; /* USER CODE BEGIN 2 */ /* USER CODE END 2 */ /** * LwIP initialization function */ void MX_LWIP_Init(void) { /* IP addresses initialization */ IP_ADDRESS[0] = 192; IP_ADDRESS[1] = 168; IP_ADDRESS[2] = 3; IP_ADDRESS[3] = 168; NETMASK_ADDRESS[0] = 255; NETMASK_ADDRESS[1] = 255; NETMASK_ADDRESS[2] = 255; NETMASK_ADDRESS[3] = 0; GATEWAY_ADDRESS[0] = 192; GATEWAY_ADDRESS[1] = 168; GATEWAY_ADDRESS[2] = 3; GATEWAY_ADDRESS[3] = 1; /* USER CODE BEGIN IP_ADDRESSES */ /* USER CODE END IP_ADDRESSES */ /* Initilialize the LwIP stack without RTOS */ lwip_init(); /* IP addresses initialization without DHCP (IPv4) */ IP4_ADDR(&ipaddr, IP_ADDRESS[0], IP_ADDRESS[1], IP_ADDRESS[2], IP_ADDRESS[3]); IP4_ADDR(&netmask, NETMASK_ADDRESS[0], NETMASK_ADDRESS[1] , NETMASK_ADDRESS[2], NETMASK_ADDRESS[3]); IP4_ADDR(&gw, GATEWAY_ADDRESS[0], GATEWAY_ADDRESS[1], GATEWAY_ADDRESS[2], GATEWAY_ADDRESS[3]); /* add the network interface (IPv4/IPv6) without RTOS */ netif_add(&gnetif, &ipaddr, &netmask, &gw, NULL, ðernetif_init, ðernet_input); /* Registers the default network interface */ netif_set_default(&gnetif); /* We must always bring the network interface up connection or not... */ netif_set_up(&gnetif); /* Set the link callback function, this function is called on change of link status*/ netif_set_link_callback(&gnetif, ethernet_link_status_updated); /* Create the Ethernet link handler thread */ /* USER CODE BEGIN 3 */ /* USER CODE END 3 */ } #ifdef USE_OBSOLETE_USER_CODE_SECTION_4 /* Kept to help code migration. (See new 4_1, 4_2... sections) */ /* Avoid to use this user section which will become obsolete. */ /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ #endif /** * @brief Ethernet Link periodic check * @param netif * @retval None */ static void Ethernet_Link_Periodic_Handle(struct netif *netif) { /* USER CODE BEGIN 4_4_1 */ /* USER CODE END 4_4_1 */ /* Ethernet Link every 100ms */ if (HAL_GetTick() - EthernetLinkTimer >= 100) { EthernetLinkTimer = HAL_GetTick(); ethernet_link_check_state(netif); } /* USER CODE BEGIN 4_4 */ /* USER CODE END 4_4 */ } /** * ---------------------------------------------------------------------- * Function given to help user to continue LwIP Initialization * Up to user to complete or change this function ... * Up to user to call this function in main.c in while (1) of main(void) *----------------------------------------------------------------------- * Read a received packet from the Ethernet buffers * Send it to the lwIP stack for handling * Handle timeouts if LWIP_TIMERS is set and without RTOS * Handle the llink status if LWIP_NETIF_LINK_CALLBACK is set and without RTOS */ void MX_LWIP_Process(void) { /* USER CODE BEGIN 4_1 */ /* USER CODE END 4_1 */ ethernetif_input(&gnetif); /* USER CODE BEGIN 4_2 */ /* USER CODE END 4_2 */ /* Handle timeouts */ sys_check_timeouts(); Ethernet_Link_Periodic_Handle(&gnetif); /* USER CODE BEGIN 4_3 */ /* USER CODE END 4_3 */ } /** * @brief Notify the User about the network interface config status * @param netif: the network interface * @retval None */ static void ethernet_link_status_updated(struct netif *netif) { if (netif_is_up(netif)) { /* USER CODE BEGIN 5 */ print_status(1); /* USER CODE END 5 */ } else /* netif is down */ { /* USER CODE BEGIN 6 */ print_status(2); /* USER CODE END 6 */ } } #if defined ( __CC_ARM ) /* MDK ARM Compiler */ /** * Opens a serial device for communication. * * @param devnum device number * @return handle to serial device if successful, NULL otherwise */ sio_fd_t sio_open(u8_t devnum) { sio_fd_t sd; /* USER CODE BEGIN 7 */ sd = 0; // dummy code /* USER CODE END 7 */ return sd; } /** * Sends a single character to the serial device. * * @param c character to send * @param fd serial device handle * * @note This function will block until the character can be sent. */ void sio_send(u8_t c, sio_fd_t fd) { /* USER CODE BEGIN 8 */ /* USER CODE END 8 */ } /** * Reads from the serial device. * * @param fd serial device handle * @param data pointer to data buffer for receiving * @param len maximum length (in bytes) of data to receive * @return number of bytes actually received - may be 0 if aborted by sio_read_abort * * @note This function will block until data can be received. The blocking * can be cancelled by calling sio_read_abort(). */ u32_t sio_read(sio_fd_t fd, u8_t *data, u32_t len) { u32_t recved_bytes; /* USER CODE BEGIN 9 */ recved_bytes = 0; // dummy code /* USER CODE END 9 */ return recved_bytes; } /** * Tries to read from the serial device. Same as sio_read but returns * immediately if no data is available and never blocks. * * @param fd serial device handle * @param data pointer to data buffer for receiving * @param len maximum length (in bytes) of data to receive * @return number of bytes actually received */ u32_t sio_tryread(sio_fd_t fd, u8_t *data, u32_t len) { u32_t recved_bytes; /* USER CODE BEGIN 10 */ recved_bytes = 0; // dummy code /* USER CODE END 10 */ return recved_bytes; } #endif /* MDK ARM Compiler */