/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2023 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" #include "stdlib.h" #include "time.h" #define led1 GPIO_PIN_0 #define led2 GPIO_PIN_1 #define led3 GPIO_PIN_2 #define led4 GPIO_PIN_3 #define led5 GPIO_PIN_4 #define led6 GPIO_PIN_5 #define led7 GPIO_PIN_6 int LEDS[] = {led1,led2,led3,led4,led5,led6,led7}; #define button GPIO_PIN_13 UART_HandleTypeDef huart2; /* USER CODE BEGIN PV */ /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_USART2_UART_Init(void); // // This function turns OFF all LEDS // void ALL_OFF() { int i; for (i = 0; i <7; i++) { HAL_GPIO_WritePin(GPIOC, LEDS[i], GPIO_PIN_RESET); } } int main(void) { int dice; HAL_Init(); SystemClock_Config(); MX_GPIO_Init(); MX_USART2_UART_Init(); srand(time(NULL)); // Random number seed while (1) // DO FOREVER { ALL_OFF(); // All LEDS OFF initially while(HAL_GPIO_ReadPin(GPIOC, button) == 1); // Wait for button dice = rand()%6 +1; // Get a dice number switch(dice){ case 1: // Is it 1? HAL_GPIO__WritePin(GPIOC,LEDS[3], GPIO_PIN_SET); break; case 2: // Is it 2? HAL_GPIO__WritePin(GPIOC,LEDS[1], GPIO_PIN_SET); HAL_GPIO__WritePin(GPIOC,LEDS[5], GPIO_PIN_SET); break; case 3: // Is it 3? HAL_GPIO__WritePin(GPIOC,LEDS[1], GPIO_PIN_SET); HAL_GPIO__WritePin(GPIOC,LEDS[3], GPIO_PIN_SET); HAL_GPIO__WritePin(GPIOC,LEDS[5], GPIO_PIN_SET); break; case 4: // Is it 4? HAL_GPIO__WritePin(GPIOC,LEDS[0], GPIO_PIN_SET); HAL_GPIO__WritePin(GPIOC,LEDS[2], GPIO_PIN_SET); HAL_GPIO__WritePin(GPIOC,LEDS[4], GPIO_PIN_SET); HAL_GPIO__WritePin(GPIOC,LEDS[6], GPIO_PIN_SET); break; case 5: // Is it 5? HAL_GPIO__WritePin(GPIOC,LEDS[0], GPIO_PIN_SET); HAL_GPIO__WritePin(GPIOC,LEDS[2], GPIO_PIN_SET); HAL_GPIO__WritePin(GPIOC,LEDS[3], GPIO_PIN_SET); HAL_GPIO__WritePin(GPIOC,LEDS[4], GPIO_PIN_SET); HAL_GPIO__WritePin(GPIOC,LEDS[6], GPIO_PIN_SET); break; case 6: // Is it 6? HAL_GPIO__WritePin(GPIOC,LEDS[0], GPIO_PIN_SET); HAL_GPIO__WritePin(GPIOC,LEDS[1], GPIO_PIN_SET); HAL_GPIO__WritePin(GPIOC,LEDS[2], GPIO_PIN_SET); HAL_GPIO__WritePin(GPIOC,LEDS[4], GPIO_PIN_SET); HAL_GPIO__WritePin(GPIOC,LEDS[5], GPIO_PIN_SET); HAL_GPIO__WritePin(GPIOC,LEDS[6], GPIO_PIN_SET); break; } HAL_Delay(3000); // Wait 3 seconds } } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Configure the main internal regulator output voltage */ if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK) { Error_Handler(); } /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI; RCC_OscInitStruct.PLL.PLLM = 1; RCC_OscInitStruct.PLL.PLLN = 10; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7; RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2; RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK) { Error_Handler(); } } /** * @brief USART2 Initialization Function * @param None * @retval None */ static void MX_USART2_UART_Init(void) { /* USER CODE BEGIN USART2_Init 0 */ /* USER CODE END USART2_Init 0 */ /* USER CODE BEGIN USART2_Init 1 */ /* USER CODE END USART2_Init 1 */ huart2.Instance = USART2; huart2.Init.BaudRate = 115200; huart2.Init.WordLength = UART_WORDLENGTH_8B; huart2.Init.StopBits = UART_STOPBITS_1; huart2.Init.Parity = UART_PARITY_NONE; huart2.Init.Mode = UART_MODE_TX_RX; huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart2.Init.OverSampling = UART_OVERSAMPLING_16; huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; if (HAL_UART_Init(&huart2) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN USART2_Init 2 */ /* USER CODE END USART2_Init 2 */ } /** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOH_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3 |GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET); /*Configure GPIO pin : PC13 */ GPIO_InitStruct.Pin = GPIO_PIN_13; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); /*Configure GPIO pins : PC0 PC1 PC2 PC3 PC4 PC5 PC6 */ GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3 |GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); /*Configure GPIO pin : LD2_Pin */ GPIO_InitStruct.Pin = LD2_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(LD2_GPIO_Port, &GPIO_InitStruct); } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */