// All credit to Carmine Noviello for this code // https://github.com/cnoviello/mastering-stm32/blob/master/nucleo-f030R8/system/src/retarget/retarget.c #include <_ansi.h> #include <_syslist.h> #include #include #include #include #include #include <../Inc/retarget.h> #include #include #if !defined(OS_USE_SEMIHOSTING) #define STDIN_FILENO 0 #define STDOUT_FILENO 1 #define STDERR_FILENO 2 UART_HandleTypeDef *gHuart; void RetargetInit(UART_HandleTypeDef *huart) { gHuart = huart; /* Disable I/O buffering for STDOUT stream, so that * chars are sent out as soon as they are printed. */ setvbuf(stdout, NULL, _IONBF, 0); } int _isatty(int fd) { if (fd >= STDIN_FILENO && fd <= STDERR_FILENO) return 1; errno = EBADF; return 0; } int _write(int fd, char* ptr, int len) { HAL_StatusTypeDef hstatus; if (fd == STDOUT_FILENO || fd == STDERR_FILENO) { hstatus = HAL_UART_Transmit(gHuart, (uint8_t *) ptr, len, HAL_MAX_DELAY); if (hstatus == HAL_OK) return len; else return EIO; } errno = EBADF; return -1; } int _close(int fd) { if (fd >= STDIN_FILENO && fd <= STDERR_FILENO) return 0; errno = EBADF; return -1; } int _lseek(int fd, int ptr, int dir) { (void) fd; (void) ptr; (void) dir; errno = EBADF; return -1; } int _read(int fd, char* ptr, int len) { HAL_StatusTypeDef hstatus; if (fd == STDIN_FILENO) { hstatus = HAL_UART_Receive(gHuart, (uint8_t *) ptr, 1, HAL_MAX_DELAY); if (hstatus == HAL_OK) return 1; else return EIO; } errno = EBADF; return -1; } int _fstat(int fd, struct stat* st) { if (fd >= STDIN_FILENO && fd <= STDERR_FILENO) { st->st_mode = S_IFCHR; return 0; } errno = EBADF; return 0; } #endif //#if !defined(OS_USE_SEMIHOSTING)