回路図を提示するまえに、STBB2の出力電圧が規格値より低くなる 要因をあげていただきたいと思います。 例:800mA以上の消費電流の負荷が接続されている。 その他の要因を記載してください。 このICは、25℃、消費電流500mA、800mAのとき、表面温度は何℃になるでしょうか。 Before presenting the circuit diagram, I would like to ask you to list the factors that cause the output voltage of STBB2 to be lower than the specified value. Before presenting the circuit diagram, I would like you to list the factors that cause the output voltage of STBB2 to be lower than the specified value. Example: A load with a current consumption of 800mA or more is connected. Please describe other factors. What will be the surface temperature of this IC at 25°C and 500mA and 800mA consumption current?