USBからの入力(5V)をSTBB2J30Rの入力に接続して、出力にマイコンのVDDを接続しています。基板を10台製作して、10台とも同じ現象です。 この情報から出力電圧が2.8Vとなる理由(原因)を教えてください。 負荷は800mAが流れるような大きなものは接続していません。 I'm using a product with a 3V output, but it only outputs 2.8V. Please list the possible causes. All of the 20 boards produced have this result.