/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2025 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ #include #include"socket.h" #include #include /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ FDCAN_HandleTypeDef hfdcan1; SPI_HandleTypeDef hspi1; DMA_HandleTypeDef hdma_spi1_rx; DMA_HandleTypeDef hdma_spi1_tx; /* USER CODE BEGIN PV */ #define Client //#define Server #define TCP_SOCKET 0 #define LOCAL_PORT 5555 #define BUFFER_SIZE 1456 #define MAX_MESSAGES (BUFFER_SIZE / sizeof(EulerAngles)) uint8_t current_index = 0; uint8_t S_ADDR[4] = {192,168,10,2}; uint16_t S_PORT = 9988; uint8_t RxData[8]; uint8_t rxBuffer[BUFFER_SIZE]; uint16_t buffer_index = 0; int total_size = 0; FDCAN_RxHeaderTypeDef RxHeader; bool Newmessage = false; volatile uint8_t spiTxComplete = 1; volatile uint8_t spiRxComplete = 1; /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_DMA_Init(void); static void MX_FDCAN1_Init(void); static void MX_SPI1_Init(void); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ //float bytesToFloat(uint8_t *bytes) { // // float value; // memcpy(&value, bytes, sizeof(float)); // return value; //} typedef struct { float roll; float pitch; float yaw; float accx; float accy; float accz; uint32_t timestamp; } EulerAngles; EulerAngles angles; EulerAngles txBuffer[MAX_MESSAGES]; uint8_t large_buffer[BUFFER_SIZE]; wiz_NetInfo netInfo={ .mac = {0x02, 0x00, 0x00, 0x00, 0x00, 0x01}, .ip = {192,168,10,1}, .sn = {255,255,255,0}, .dns = {0,0,0,0}, .dhcp = NETINFO_STATIC }; void W5500_Init(void); void W5500_Select(void); void W5500_Unselect(void); uint8_t W5500_ReadByte(void); void W5500_WriteByte(uint8_t byte); void W5500_ReadBuff(uint8_t *buff , uint16_t len); void W5500_WriteBuff(uint8_t *buff ,uint16_t len); void W5500_Init(){ reg_wizchip_cs_cbfunc(W5500_Select, W5500_Unselect); reg_wizchip_spi_cbfunc(W5500_ReadByte, W5500_WriteByte); reg_wizchip_spiburst_cbfunc(W5500_ReadBuff, W5500_WriteBuff); // uint8_t memsize[2][8] = {{2,2,2,2,2,2,2,2}, {2,2,2,2,2,2,2,2}}; uint8_t memsize[2][8] = {{16,0,0,0,0,0,0,0}, {16,0,0,0,0,0,0,0}}; if(wizchip_init(memsize[0], memsize[1]) < 0) { Error_Handler(); } } void W5500_Select(void) { HAL_GPIO_WritePin(GPIOB,GPIO_PIN_1,GPIO_PIN_RESET); } void W5500_Unselect(void) { HAL_GPIO_WritePin(GPIOB, GPIO_PIN_1, GPIO_PIN_SET); } uint8_t W5500_ReadByte(void) { uint8_t byte; HAL_SPI_Receive(&hspi1, &byte, 1, HAL_MAX_DELAY); return byte; } void W5500_WriteByte(uint8_t byte) { HAL_SPI_Transmit(&hspi1, &byte, 1, HAL_MAX_DELAY); } void W5500_ReadBuff(uint8_t* buff, uint16_t len) { spiRxComplete = 0; HAL_SPI_Receive_DMA(&hspi1, buff, len); while(HAL_SPI_GetState(&hspi1) != HAL_SPI_STATE_READY); } void W5500_WriteBuff(uint8_t* buff, uint16_t len) { spiTxComplete = 0; HAL_SPI_Transmit_DMA(&hspi1, buff, len); while(HAL_SPI_GetState(&hspi1) != HAL_SPI_STATE_READY); } void HAL_SPI_TxCpltCallback(SPI_HandleTypeDef *hspi) { if(hspi->Instance == SPI2) { spiTxComplete = 1; } } void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi) { if(hspi->Instance == SPI2) { spiRxComplete = 1; } } void HAL_FDCAN_RxFifo0Callback(FDCAN_HandleTypeDef *hfdcan, uint32_t RxFifo0ITs){ if(HAL_FDCAN_GetRxMessage(hfdcan,FDCAN_RX_FIFO0,&RxHeader,RxData)== HAL_OK){ switch(RxHeader.Identifier){ case 0x22: int16_t roll_rad = (RxData[0]<<8 ) | RxData[1]; int16_t pitch_rad= (RxData[2]<<8)| RxData[3]; int16_t yaw_rad = (RxData[4]<<8 )| RxData[5]; if((roll_rad>=0 && roll_rad<=23040) ||(pitch_rad>=0 && pitch_rad<=23040) || (yaw_rad>=0 && yaw_rad<=23040)){ angles.roll= (roll_rad * 0.0078f); angles.pitch= (pitch_rad * 0.0078f); angles.yaw = (yaw_rad * 0.0078f); } else if((roll_rad>=42496 && roll_rad<=65536) ||(pitch_rad>=42496 && pitch_rad<=65536) || (yaw_rad>=42496 && yaw_rad<=65536)){ angles.roll= (roll_rad - 65536)*0.0078; angles.pitch= (pitch_rad - 65536)*0.0078; angles.yaw = (yaw_rad - 65536)*0.0078; } angles.timestamp = HAL_GetTick(); Newmessage = true; case 0x34: int16_t accX = (RxData[0] << 8) | RxData[1]; int16_t accY = (RxData[2] << 8) | RxData[3]; int16_t accZ = (RxData[4] << 8) | RxData[5]; angles.accx = accX * 0.0039; angles.accy = accY * 0.0039; angles.accz = accZ * 0.0039; angles.timestamp = HAL_GetTick(); Newmessage = true; } } } void sendimudata() { if (Newmessage) { if (buffer_index < MAX_MESSAGES) { memcpy(&txBuffer[buffer_index], (void*)&angles, sizeof(EulerAngles)); buffer_index++; } if (buffer_index >= MAX_MESSAGES) { total_size = buffer_index * sizeof(EulerAngles); memcpy(large_buffer, txBuffer, total_size); buffer_index = 0; } Newmessage = false; } } /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_DMA_Init(); MX_FDCAN1_Init(); MX_SPI1_Init(); /* USER CODE BEGIN 2 */ if(HAL_FDCAN_Start(&hfdcan1)!= HAL_OK){ Error_Handler(); } if (HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0) != HAL_OK) { Error_Handler(); } W5500_Init(); wizchip_setnetinfo(&netInfo); #ifdef Server uint8_t socketStatus2 = socket(TCP_SOCKET,Sn_MR_TCP,LOCAL_PORT,0x00); if(socketStatus2==0){ listen(TCP_SOCKET); } #endif #ifdef Client uint8_t SOCKET = socket(TCP_SOCKET,Sn_MR_TCP,LOCAL_PORT,0); if(SOCKET == 0){ HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5,GPIO_PIN_SET); connect(TCP_SOCKET, S_ADDR, S_PORT); } #endif /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { #ifdef Client if(Newmessage) { sendimudata(); } switch(getSn_SR(TCP_SOCKET)){ case SOCK_ESTABLISHED: if(getSn_IR(TCP_SOCKET)& Sn_IR_CON){ setSn_IR(TCP_SOCKET,Sn_IR_CON); } if (total_size > 0) { if(send(TCP_SOCKET,large_buffer,total_size)>0){ HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5); total_size = 0; } } break; case SOCK_CLOSE_WAIT: disconnect(TCP_SOCKET); break; case SOCK_CLOSED: if(socket(TCP_SOCKET, Sn_MR_TCP, LOCAL_PORT, 0) == TCP_SOCKET){ connect(TCP_SOCKET, S_ADDR, S_PORT); total_size = 0; } break; } if (getSn_IR(TCP_SOCKET) & Sn_IR_TIMEOUT) { setSn_IR(TCP_SOCKET, Sn_IR_TIMEOUT); } #endif #ifdef Server switch (getSn_SR(TCP_SOCKET)) { case SOCK_ESTABLISHED: if(getSn_IR(TCP_SOCKET)& Sn_IR_CON){ setSn_IR(TCP_SOCKET,Sn_IR_CON); } uint16_t rxsize = getSn_RX_RSR(TCP_SOCKET); if(rxsize> 0){ if(rxsize > (BUFFER_SIZE-current_index)) rxsize = (BUFFER_SIZE-current_index); uint8_t rxlen = recv(TCP_SOCKET, rxBuffer+current_index,rxsize); if(rxlen > 0){ current_index += rxlen; if(memchr(rxBuffer,'\n',current_index)|| current_index>=BUFFER_SIZE-1){ data(); } } } break; case SOCK_CLOSE_WAIT: disconnect(TCP_SOCKET); break; case SOCK_CLOSED: socket(TCP_SOCKET,Sn_MR_TCP,LOCAL_PORT,0); listen(TCP_SOCKET); break; } if(getSn_IR(TCP_SOCKET)& Sn_IR_TIMEOUT){ setSn_IR(TCP_SOCKET,Sn_IR_TIMEOUT); } #endif /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Configure the main internal regulator output voltage */ HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1); /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV2; RCC_OscInitStruct.PLL.PLLN = 20; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV4; RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK) { Error_Handler(); } } /** * @brief FDCAN1 Initialization Function * @param None * @retval None */ static void MX_FDCAN1_Init(void) { /* USER CODE BEGIN FDCAN1_Init 0 */ /* USER CODE END FDCAN1_Init 0 */ /* USER CODE BEGIN FDCAN1_Init 1 */ /* USER CODE END FDCAN1_Init 1 */ hfdcan1.Instance = FDCAN1; hfdcan1.Init.ClockDivider = FDCAN_CLOCK_DIV1; hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC; hfdcan1.Init.Mode = FDCAN_MODE_NORMAL; hfdcan1.Init.AutoRetransmission = ENABLE; hfdcan1.Init.TransmitPause = DISABLE; hfdcan1.Init.ProtocolException = DISABLE; hfdcan1.Init.NominalPrescaler = 1; hfdcan1.Init.NominalSyncJumpWidth = 12; hfdcan1.Init.NominalTimeSeg1 = 47; hfdcan1.Init.NominalTimeSeg2 = 12; hfdcan1.Init.DataPrescaler = 2; hfdcan1.Init.DataSyncJumpWidth = 6; hfdcan1.Init.DataTimeSeg1 = 23; hfdcan1.Init.DataTimeSeg2 = 6; hfdcan1.Init.StdFiltersNbr = 1; hfdcan1.Init.ExtFiltersNbr = 0; hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION; if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN FDCAN1_Init 2 */ FDCAN_FilterTypeDef Filterconfigure; Filterconfigure.FilterConfig = FDCAN_FILTER_TO_RXFIFO0 ; Filterconfigure.FilterType = FDCAN_FILTER_MASK; Filterconfigure.IdType = FDCAN_STANDARD_ID ; Filterconfigure.FilterID1 = 0x000; Filterconfigure.FilterID2 = 0x000; Filterconfigure.FilterIndex = 0; if(HAL_FDCAN_ConfigFilter(&hfdcan1,&Filterconfigure)!= HAL_OK){ Error_Handler(); } /* USER CODE END FDCAN1_Init 2 */ } /** * @brief SPI1 Initialization Function * @param None * @retval None */ static void MX_SPI1_Init(void) { /* USER CODE BEGIN SPI1_Init 0 */ /* USER CODE END SPI1_Init 0 */ /* USER CODE BEGIN SPI1_Init 1 */ /* USER CODE END SPI1_Init 1 */ /* SPI1 parameter configuration*/ hspi1.Instance = SPI1; hspi1.Init.Mode = SPI_MODE_MASTER; hspi1.Init.Direction = SPI_DIRECTION_2LINES; hspi1.Init.DataSize = SPI_DATASIZE_8BIT; hspi1.Init.CLKPolarity = SPI_POLARITY_LOW; hspi1.Init.CLKPhase = SPI_PHASE_1EDGE; hspi1.Init.NSS = SPI_NSS_SOFT; hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_8; hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi1.Init.TIMode = SPI_TIMODE_DISABLE; hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi1.Init.CRCPolynomial = 7; hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE; hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE; if (HAL_SPI_Init(&hspi1) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN SPI1_Init 2 */ /* USER CODE END SPI1_Init 2 */ } /** * Enable DMA controller clock */ static void MX_DMA_Init(void) { /* DMA controller clock enable */ __HAL_RCC_DMAMUX1_CLK_ENABLE(); __HAL_RCC_DMA1_CLK_ENABLE(); /* DMA interrupt init */ /* DMA1_Channel1_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn); /* DMA1_Channel2_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA1_Channel2_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Channel2_IRQn); } /** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* USER CODE BEGIN MX_GPIO_Init_1 */ /* USER CODE END MX_GPIO_Init_1 */ /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOF_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOB, GPIO_PIN_1, GPIO_PIN_RESET); /*Configure GPIO pin : PA5 */ GPIO_InitStruct.Pin = GPIO_PIN_5; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /*Configure GPIO pin : PB1 */ GPIO_InitStruct.Pin = GPIO_PIN_1; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); /* USER CODE BEGIN MX_GPIO_Init_2 */ /* USER CODE END MX_GPIO_Init_2 */ } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */