/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file App/app_zigbee.h * @author MCD Application Team * @brief Header for Zigbee Application. ****************************************************************************** * @attention * * Copyright (c) 2024 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Define to prevent recursive inclusion -------------------------------------*/ #ifndef APP_ZIGBEE_H #define APP_ZIGBEE_H #ifdef __cplusplus extern "C" { #endif /* Includes ------------------------------------------------------------------*/ /* Private includes ----------------------------------------------------------*/ #include "tl.h" #include "tl_zigbee_hci.h" /* USER CODE BEGIN Includes */ /* USER CODE END Includes */ /* Exported types ------------------------------------------------------------*/ /* Application errors */ /*------------------------------------*/ /* * List of all errors tracked by the Zigbee application * running on M4. Some of these errors may be fatal * or just warnings */ typedef enum { ERR_ZIGBE_CMD_TO_M0, /* USER CODE BEGIN ERROR_APPLI_ENUM */ /* USER CODE END ERROR_APPLI_ENUM */ ERR_ZIGBEE_CHECK_WIRELESS } ErrAppliIdEnum_t; /* USER CODE BEGIN ET */ struct APP_ZIGBEE_cyclic_data{ int16_t temperature; int16_t humidity; int16_t soil_moisture_1; int16_t soil_moisture_2; }; /* USER CODE END ET */ /* Exported constants --------------------------------------------------------*/ /* USER CODE BEGIN EC */ /* USER CODE END EC */ /* External variables --------------------------------------------------------*/ /* USER CODE BEGIN EV */ /* USER CODE END EV */ /* Exported macros ------------------------------------------------------------*/ /* USER CODE BEGIN EM */ /* USER CODE END EM */ /* Exported functions ------------------------------------------------------- */ void APP_ZIGBEE_Init(void); void APP_ZIGBEE_Error(uint32_t ErrId, uint32_t ErrCode); void APP_ZIGBEE_RegisterCmdBuffer(TL_CmdPacket_t *p_buffer); void APP_ZIGBEE_TL_INIT(void); void Pre_ZigbeeCmdProcessing(void); /* USER CODE BEGIN EF */ void APP_ZIGBEE_cyclic_reporting(struct APP_ZIGBEE_cyclic_data *data); /* USER CODE END EF */ #ifdef __cplusplus } /* extern "C" */ #endif #endif /* APP_ZIGBEE_H */