/**
******************************************************************************
* @file startup_stm32wb55xx_cm4.s
* @author MCD Application Team
* @brief STM32WB55xx devices vector table GCC toolchain.
* This module performs:
* - Set the initial SP
* - Set the initial PC == Reset_Handler,
* - Set the vector table entries with the exceptions ISR address
* - Branches to main in the C library (which eventually
* calls main()).
* After Reset the Cortex-M4 processor is in Thread mode,
* priority is Privileged, and the Stack is set to Main.
******************************************************************************
* @attention
*
*
© Copyright (c) 2019 STMicroelectronics.
* All rights reserved.
*
* This software component is licensed by ST under BSD 3-Clause license,
* the "License"; You may not use this file except in compliance with the
* License. You may obtain a copy of the License at:
* opensource.org/licenses/BSD-3-Clause
*
******************************************************************************
*/
.syntax unified
.cpu cortex-m4
.fpu softvfp
.thumb
.global g_pfnVectors
.global Default_Handler
/* start address for the initialization values of the .data section.
defined in linker script */
.word _sidata
/* start address for the .data section. defined in linker script */
.word _sdata
/* end address for the .data section. defined in linker script */
.word _edata
/* start address for the .bss section. defined in linker script */
.word _sbss
/* end address for the .bss section. defined in linker script */
.word _ebss
/* start address for the .MB_MEM2 section. defined in linker script */
.word _sMB_MEM2
/* end address for the .MB_MEM2 section. defined in linker script */
.word _eMB_MEM2
/* INIT_BSS macro is used to fill the specified region [start : end] with zeros */
.macro INIT_BSS start, end
ldr r0, =\start
ldr r1, =\end
movs r3, #0
bl LoopFillZerobss
.endm
/* INIT_DATA macro is used to copy data in the region [start : end] starting from 'src' */
.macro INIT_DATA start, end, src
ldr r0, =\start
ldr r1, =\end
ldr r2, =\src
movs r3, #0
bl LoopCopyDataInit
.endm
.section .text.data_initializers
CopyDataInit:
ldr r4, [r2, r3]
str r4, [r0, r3]
adds r3, r3, #4
LoopCopyDataInit:
adds r4, r0, r3
cmp r4, r1
bcc CopyDataInit
bx lr
FillZerobss:
str r3, [r0]
adds r0, r0, #4
LoopFillZerobss:
cmp r0, r1
bcc FillZerobss
bx lr
.section .text.Reset_Handler
.weak Reset_Handler
.type Reset_Handler, %function
Reset_Handler:
ldr r0, =_estack
mov sp, r0 /* set stack pointer */
/* Copy the data segment initializers from flash to SRAM */
INIT_DATA _sdata, _edata, _sidata
/* Zero fill the bss segments. */
INIT_BSS _sbss, _ebss
INIT_BSS _sMB_MEM2, _eMB_MEM2
/* Call the clock system intitialization function.*/
bl SystemInit
/* Call static constructors */
bl __libc_init_array
/* Call the application s entry point.*/
bl main
LoopForever:
b LoopForever
.size Reset_Handler, .-Reset_Handler
/**
* @brief This is the code that gets called when the processor receives an
* unexpected interrupt. This simply enters an infinite loop, preserving
* the system state for examination by a debugger.
*
* @param None
* @retval None
*/
.section .text.Default_Handler,"ax",%progbits
Default_Handler:
Infinite_Loop:
b Infinite_Loop
.size Default_Handler, .-Default_Handler
/******************************************************************************
*
* The minimal vector table for a Cortex-M4. Note that the proper constructs
* must be placed on this to ensure that it ends up at physical address
* 0x0000.0000.
*
******************************************************************************/
.section .isr_vector,"a",%progbits
.type g_pfnVectors, %object
.size g_pfnVectors, .-g_pfnVectors
g_pfnVectors:
.word _estack
.word Reset_Handler
.word NMI_Handler
.word HardFault_Handler
.word MemManage_Handler
.word BusFault_Handler
.word UsageFault_Handler
.word 0
.word 0
.word 0
.word 0
.word SVC_Handler
.word DebugMon_Handler
.word 0
.word PendSV_Handler
.word SysTick_Handler
.word WWDG_IRQHandler
.word PVD_PVM_IRQHandler
.word TAMP_STAMP_LSECSS_IRQHandler
.word RTC_WKUP_IRQHandler
.word FLASH_IRQHandler
.word RCC_IRQHandler
.word EXTI0_IRQHandler
.word EXTI1_IRQHandler
.word EXTI2_IRQHandler
.word EXTI3_IRQHandler
.word EXTI4_IRQHandler
.word DMA1_Channel1_IRQHandler
.word DMA1_Channel2_IRQHandler
.word DMA1_Channel3_IRQHandler
.word DMA1_Channel4_IRQHandler
.word DMA1_Channel5_IRQHandler
.word DMA1_Channel6_IRQHandler
.word DMA1_Channel7_IRQHandler
.word ADC1_IRQHandler
.word USB_HP_IRQHandler
.word USB_LP_IRQHandler
.word C2SEV_PWR_C2H_IRQHandler
.word COMP_IRQHandler
.word EXTI9_5_IRQHandler
.word TIM1_BRK_IRQHandler
.word TIM1_UP_TIM16_IRQHandler
.word TIM1_TRG_COM_TIM17_IRQHandler
.word TIM1_CC_IRQHandler
.word TIM2_IRQHandler
.word PKA_IRQHandler
.word I2C1_EV_IRQHandler
.word I2C1_ER_IRQHandler
.word I2C3_EV_IRQHandler
.word I2C3_ER_IRQHandler
.word SPI1_IRQHandler
.word SPI2_IRQHandler
.word USART1_IRQHandler
.word LPUART1_IRQHandler
.word SAI1_IRQHandler
.word TSC_IRQHandler
.word EXTI15_10_IRQHandler
.word RTC_Alarm_IRQHandler
.word CRS_IRQHandler
.word PWR_SOTF_BLEACT_802ACT_RFPHASE_IRQHandler
.word IPCC_C1_RX_IRQHandler
.word IPCC_C1_TX_IRQHandler
.word HSEM_IRQHandler
.word LPTIM1_IRQHandler
.word LPTIM2_IRQHandler
.word LCD_IRQHandler
.word QUADSPI_IRQHandler
.word AES1_IRQHandler
.word AES2_IRQHandler
.word RNG_IRQHandler
.word FPU_IRQHandler
.word DMA2_Channel1_IRQHandler
.word DMA2_Channel2_IRQHandler
.word DMA2_Channel3_IRQHandler
.word DMA2_Channel4_IRQHandler
.word DMA2_Channel5_IRQHandler
.word DMA2_Channel6_IRQHandler
.word DMA2_Channel7_IRQHandler
.word DMAMUX1_OVR_IRQHandler
/*******************************************************************************
*
* Provide weak aliases for each Exception handler to the Default_Handler.
* As they are weak aliases, any function with the same name will override
* this definition.
*
*******************************************************************************/
.weak NMI_Handler
.thumb_set NMI_Handler,Default_Handler
.weak HardFault_Handler
.thumb_set HardFault_Handler,Default_Handler
.weak MemManage_Handler
.thumb_set MemManage_Handler,Default_Handler
.weak BusFault_Handler
.thumb_set BusFault_Handler,Default_Handler
.weak UsageFault_Handler
.thumb_set UsageFault_Handler,Default_Handler
.weak SVC_Handler
.thumb_set SVC_Handler,Default_Handler
.weak DebugMon_Handler
.thumb_set DebugMon_Handler,Default_Handler
.weak PendSV_Handler
.thumb_set PendSV_Handler,Default_Handler
.weak SysTick_Handler
.thumb_set SysTick_Handler,Default_Handler
.weak WWDG_IRQHandler
.thumb_set WWDG_IRQHandler,Default_Handler
.weak PVD_PVM_IRQHandler
.thumb_set PVD_PVM_IRQHandler,Default_Handler
.weak TAMP_STAMP_LSECSS_IRQHandler
.thumb_set TAMP_STAMP_LSECSS_IRQHandler,Default_Handler
.weak RTC_WKUP_IRQHandler
.thumb_set RTC_WKUP_IRQHandler,Default_Handler
.weak FLASH_IRQHandler
.thumb_set FLASH_IRQHandler,Default_Handler
.weak RCC_IRQHandler
.thumb_set RCC_IRQHandler,Default_Handler
.weak EXTI0_IRQHandler
.thumb_set EXTI0_IRQHandler,Default_Handler
.weak EXTI1_IRQHandler
.thumb_set EXTI1_IRQHandler,Default_Handler
.weak EXTI2_IRQHandler
.thumb_set EXTI2_IRQHandler,Default_Handler
.weak EXTI3_IRQHandler
.thumb_set EXTI3_IRQHandler,Default_Handler
.weak EXTI4_IRQHandler
.thumb_set EXTI4_IRQHandler,Default_Handler
.weak DMA1_Channel1_IRQHandler
.thumb_set DMA1_Channel1_IRQHandler,Default_Handler
.weak DMA1_Channel2_IRQHandler
.thumb_set DMA1_Channel2_IRQHandler,Default_Handler
.weak DMA1_Channel3_IRQHandler
.thumb_set DMA1_Channel3_IRQHandler,Default_Handler
.weak DMA1_Channel4_IRQHandler
.thumb_set DMA1_Channel4_IRQHandler,Default_Handler
.weak DMA1_Channel5_IRQHandler
.thumb_set DMA1_Channel5_IRQHandler,Default_Handler
.weak DMA1_Channel6_IRQHandler
.thumb_set DMA1_Channel6_IRQHandler,Default_Handler
.weak DMA1_Channel7_IRQHandler
.thumb_set DMA1_Channel7_IRQHandler,Default_Handler
.weak ADC1_IRQHandler
.thumb_set ADC1_IRQHandler,Default_Handler
.weak USB_HP_IRQHandler
.thumb_set USB_HP_IRQHandler,Default_Handler
.weak USB_LP_IRQHandler
.thumb_set USB_LP_IRQHandler,Default_Handler
.weak C2SEV_PWR_C2H_IRQHandler
.thumb_set C2SEV_PWR_C2H_IRQHandler,Default_Handler
.weak COMP_IRQHandler
.thumb_set COMP_IRQHandler,Default_Handler
.weak EXTI9_5_IRQHandler
.thumb_set EXTI9_5_IRQHandler,Default_Handler
.weak TIM1_BRK_IRQHandler
.thumb_set TIM1_BRK_IRQHandler,Default_Handler
.weak TIM1_UP_TIM16_IRQHandler
.thumb_set TIM1_UP_TIM16_IRQHandler,Default_Handler
.weak TIM1_TRG_COM_TIM17_IRQHandler
.thumb_set TIM1_TRG_COM_TIM17_IRQHandler,Default_Handler
.weak TIM1_CC_IRQHandler
.thumb_set TIM1_CC_IRQHandler,Default_Handler
.weak TIM2_IRQHandler
.thumb_set TIM2_IRQHandler,Default_Handler
.weak PKA_IRQHandler
.thumb_set PKA_IRQHandler,Default_Handler
.weak I2C1_EV_IRQHandler
.thumb_set I2C1_EV_IRQHandler,Default_Handler
.weak I2C1_ER_IRQHandler
.thumb_set I2C1_ER_IRQHandler,Default_Handler
.weak I2C3_EV_IRQHandler
.thumb_set I2C3_EV_IRQHandler,Default_Handler
.weak I2C3_ER_IRQHandler
.thumb_set I2C3_ER_IRQHandler,Default_Handler
.weak SPI1_IRQHandler
.thumb_set SPI1_IRQHandler,Default_Handler
.weak SPI2_IRQHandler
.thumb_set SPI2_IRQHandler,Default_Handler
.weak USART1_IRQHandler
.thumb_set USART1_IRQHandler,Default_Handler
.weak LPUART1_IRQHandler
.thumb_set LPUART1_IRQHandler,Default_Handler
.weak SAI1_IRQHandler
.thumb_set SAI1_IRQHandler,Default_Handler
.weak TSC_IRQHandler
.thumb_set TSC_IRQHandler,Default_Handler
.weak EXTI15_10_IRQHandler
.thumb_set EXTI15_10_IRQHandler,Default_Handler
.weak RTC_Alarm_IRQHandler
.thumb_set RTC_Alarm_IRQHandler,Default_Handler
.weak CRS_IRQHandler
.thumb_set CRS_IRQHandler,Default_Handler
.weak PWR_SOTF_BLEACT_802ACT_RFPHASE_IRQHandler
.thumb_set PWR_SOTF_BLEACT_802ACT_RFPHASE_IRQHandler,Default_Handler
.weak IPCC_C1_RX_IRQHandler
.thumb_set IPCC_C1_RX_IRQHandler,Default_Handler
.weak IPCC_C1_TX_IRQHandler
.thumb_set IPCC_C1_TX_IRQHandler,Default_Handler
.weak HSEM_IRQHandler
.thumb_set HSEM_IRQHandler,Default_Handler
.weak LPTIM1_IRQHandler
.thumb_set LPTIM1_IRQHandler,Default_Handler
.weak LPTIM2_IRQHandler
.thumb_set LPTIM2_IRQHandler,Default_Handler
.weak LCD_IRQHandler
.thumb_set LCD_IRQHandler,Default_Handler
.weak QUADSPI_IRQHandler
.thumb_set QUADSPI_IRQHandler,Default_Handler
.weak AES1_IRQHandler
.thumb_set AES1_IRQHandler,Default_Handler
.weak AES2_IRQHandler
.thumb_set AES2_IRQHandler,Default_Handler
.weak RNG_IRQHandler
.thumb_set RNG_IRQHandler,Default_Handler
.weak FPU_IRQHandler
.thumb_set FPU_IRQHandler,Default_Handler
.weak DMA2_Channel1_IRQHandler
.thumb_set DMA2_Channel1_IRQHandler,Default_Handler
.weak DMA2_Channel2_IRQHandler
.thumb_set DMA2_Channel2_IRQHandler,Default_Handler
.weak DMA2_Channel3_IRQHandler
.thumb_set DMA2_Channel3_IRQHandler,Default_Handler
.weak DMA2_Channel4_IRQHandler
.thumb_set DMA2_Channel4_IRQHandler,Default_Handler
.weak DMA2_Channel5_IRQHandler
.thumb_set DMA2_Channel5_IRQHandler,Default_Handler
.weak DMA2_Channel6_IRQHandler
.thumb_set DMA2_Channel6_IRQHandler,Default_Handler
.weak DMA2_Channel7_IRQHandler
.thumb_set DMA2_Channel7_IRQHandler,Default_Handler
.weak DMAMUX1_OVR_IRQHandler
.thumb_set DMAMUX1_OVR_IRQHandler,Default_Handler
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/