/* Functions called by the TouchGFX HAL to invoke the actual data transfer to ILI9488. * Pero, 2021 */ #ifndef TOUCHGFX_DATATRANSFER_H #define TOUCHGFX_DATATRANSFER_H #include #ifdef __cplusplus extern "C" { #endif void touchgfxDisplayDriverTransmitBlock(uint8_t* pixels, uint16_t x, uint16_t y, uint16_t w, uint16_t h); uint32_t touchgfxDisplayDriverTransmitActive(void); #ifdef __cplusplus } #endif #endif