/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2024 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" #include "cmsis_os.h" #include "app_touchgfx.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ #include "is42s32800j.h" /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ #ifndef HSEM_ID_0 #define HSEM_ID_0 (0U) /* HW semaphore 0*/ #endif #define SDRAM_ADDRESS_START 0xD0000000 #define SDRAM_SIZE 0x1000000 /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ CRC_HandleTypeDef hcrc; DMA2D_HandleTypeDef hdma2d; DSI_HandleTypeDef hdsi; LTDC_HandleTypeDef hltdc; QSPI_HandleTypeDef hqspi; SPI_HandleTypeDef hspi6; SDRAM_HandleTypeDef hsdram1; /* Definitions for defaultTask */ osThreadId_t defaultTaskHandle; const osThreadAttr_t defaultTask_attributes = { .name = "defaultTask", .stack_size = 128 * 4, .priority = (osPriority_t) osPriorityNormal, }; /* Definitions for touchGFXTask */ osThreadId_t touchGFXTaskHandle; const osThreadAttr_t touchGFXTask_attributes = { .name = "touchGFXTask", .stack_size = 8192 * 4, .priority = (osPriority_t) osPriorityNormal, }; /* USER CODE BEGIN PV */ OTM8009A_Object_t OTM8009AObj; OTM8009A_IO_t IOCtx; static RCC_PeriphCLKInitTypeDef PeriphClkInitStruct; static void *Lcd_CompObj = NULL; /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); void PeriphCommonClock_Config(void); static void MPU_Config(void); static void MX_GPIO_Init(void); static void MX_DMA_Init(void); static void MX_DSIHOST_DSI_Init(void); static void MX_LTDC_Init(void); static void MX_QUADSPI_Init(void); static void MX_DMA2D_Init(void); static void MX_CRC_Init(void); static void MX_SPI6_Init(void); static void MX_FMC_Init(void); void StartDefaultTask(void *argument); void startTGFXTask(void *argument); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ void FMC_Init(){ FMC_SDRAM_CommandTypeDef Command; HAL_StatusTypeDef status; Command.CommandMode = FMC_SDRAM_CMD_CLK_ENABLE; Command.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK2; Command.AutoRefreshNumber =1; Command.ModeRegisterDefinition =0; status = HAL_SDRAM_SendCommand(&hsdram1, &Command, 0xfff); HAL_Delay(1); Command.CommandMode =FMC_SDRAM_CMD_PALL; status = HAL_SDRAM_SendCommand(&hsdram1, &Command, 0xfff); Command.CommandMode =FMC_SDRAM_CMD_AUTOREFRESH_MODE; Command.AutoRefreshNumber =2; status = HAL_SDRAM_SendCommand(&hsdram1, &Command, 0xfff); Command.CommandMode =FMC_SDRAM_CMD_LOAD_MODE; Command.ModeRegisterDefinition = (uint32_t)0 | 0<<3| 2<<4|0<<7|1<<9; status = HAL_SDRAM_SendCommand(&hsdram1, &Command, 0xfff); HAL_SDRAM_ProgramRefreshRate(&hsdram1, 1542); } /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* USER CODE BEGIN Boot_Mode_Sequence_0 */ int32_t timeout; /* USER CODE END Boot_Mode_Sequence_0 */ /* MPU Configuration--------------------------------------------------------*/ MPU_Config(); /* Enable the CPU Cache */ /* Enable I-Cache---------------------------------------------------------*/ SCB_EnableICache(); /* Enable D-Cache---------------------------------------------------------*/ SCB_EnableDCache(); /* USER CODE BEGIN Boot_Mode_Sequence_1 */ /* Wait until CPU2 boots and enters in stop mode or timeout*/ timeout = 0xFFFF; while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) != RESET) && (timeout-- > 0)); if ( timeout < 0 ) { Error_Handler(); } /* USER CODE END Boot_Mode_Sequence_1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* Configure the peripherals common clocks */ PeriphCommonClock_Config(); /* USER CODE BEGIN Boot_Mode_Sequence_2 */ /* When system initialization is finished, Cortex-M7 will release Cortex-M4 by means of HSEM notification */ /*HW semaphore Clock enable*/ __HAL_RCC_HSEM_CLK_ENABLE(); /*Take HSEM */ HAL_HSEM_FastTake(HSEM_ID_0); /*Release HSEM in order to notify the CPU2(CM4)*/ HAL_HSEM_Release(HSEM_ID_0,0); /* wait until CPU2 wakes up from stop mode */ timeout = 0xFFFF; while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) == RESET) && (timeout-- > 0)); if ( timeout < 0 ) { Error_Handler(); } /* USER CODE END Boot_Mode_Sequence_2 */ /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_DMA_Init(); MX_DSIHOST_DSI_Init(); MX_LTDC_Init(); MX_QUADSPI_Init(); MX_DMA2D_Init(); MX_CRC_Init(); MX_SPI6_Init(); MX_FMC_Init(); MX_TouchGFX_Init(); /* Call PreOsInit function */ MX_TouchGFX_PreOSInit(); /* USER CODE BEGIN 2 */ /* HAL_DSI_ShortWrite(&(hdsi), 0, DSI_DCS_SHORT_PKT_WRITE_P1, OTM8009A_CMD_DISPON, 0x00); HAL_DSI_Refresh(&hdsi);*/ /* USER CODE END 2 */ /* Init scheduler */ osKernelInitialize(); /* USER CODE BEGIN RTOS_MUTEX */ /* add mutexes, ... */ /* USER CODE END RTOS_MUTEX */ /* USER CODE BEGIN RTOS_SEMAPHORES */ /* add semaphores, ... */ /* USER CODE END RTOS_SEMAPHORES */ /* USER CODE BEGIN RTOS_TIMERS */ /* start timers, add new ones, ... */ /* USER CODE END RTOS_TIMERS */ /* USER CODE BEGIN RTOS_QUEUES */ /* add queues, ... */ /* USER CODE END RTOS_QUEUES */ /* Create the thread(s) */ /* creation of defaultTask */ defaultTaskHandle = osThreadNew(StartDefaultTask, NULL, &defaultTask_attributes); /* creation of touchGFXTask */ touchGFXTaskHandle = osThreadNew(startTGFXTask, NULL, &touchGFXTask_attributes); /* USER CODE BEGIN RTOS_THREADS */ /* add threads, ... */ /* USER CODE END RTOS_THREADS */ /* USER CODE BEGIN RTOS_EVENTS */ /* add events, ... */ /* USER CODE END RTOS_EVENTS */ /* Start scheduler */ osKernelStart(); /* We should never get here as control is now taken by the scheduler */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Supply configuration update enable */ HAL_PWREx_ConfigSupply(PWR_DIRECT_SMPS_SUPPLY); /** Configure the main internal regulator output voltage */ __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1); while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {} /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.HSIState = RCC_HSI_DIV1; RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = 4; RCC_OscInitStruct.PLL.PLLN = 160; RCC_OscInitStruct.PLL.PLLP = 2; RCC_OscInitStruct.PLL.PLLQ = 2; RCC_OscInitStruct.PLL.PLLR = 4; RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_2; RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE; RCC_OscInitStruct.PLL.PLLFRACN = 0; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2 |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2; RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2; RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2; RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2; RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK) { Error_Handler(); } } /** * @brief Peripherals Common Clock Configuration * @retval None */ void PeriphCommonClock_Config(void) { RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0}; /** Initializes the peripherals clock */ PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_CKPER; PeriphClkInitStruct.CkperClockSelection = RCC_CLKPSOURCE_HSI; if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK) { Error_Handler(); } } /** * @brief CRC Initialization Function * @param None * @retval None */ static void MX_CRC_Init(void) { /* USER CODE BEGIN CRC_Init 0 */ /* USER CODE END CRC_Init 0 */ /* USER CODE BEGIN CRC_Init 1 */ /* USER CODE END CRC_Init 1 */ hcrc.Instance = CRC; hcrc.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_ENABLE; hcrc.Init.DefaultInitValueUse = DEFAULT_INIT_VALUE_ENABLE; hcrc.Init.InputDataInversionMode = CRC_INPUTDATA_INVERSION_NONE; hcrc.Init.OutputDataInversionMode = CRC_OUTPUTDATA_INVERSION_DISABLE; hcrc.InputDataFormat = CRC_INPUTDATA_FORMAT_BYTES; if (HAL_CRC_Init(&hcrc) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN CRC_Init 2 */ /* USER CODE END CRC_Init 2 */ } /** * @brief DMA2D Initialization Function * @param None * @retval None */ static void MX_DMA2D_Init(void) { /* USER CODE BEGIN DMA2D_Init 0 */ /* USER CODE END DMA2D_Init 0 */ /* USER CODE BEGIN DMA2D_Init 1 */ /* USER CODE END DMA2D_Init 1 */ hdma2d.Instance = DMA2D; hdma2d.Init.Mode = DMA2D_M2M; hdma2d.Init.ColorMode = DMA2D_OUTPUT_RGB888; hdma2d.Init.OutputOffset = 0; hdma2d.LayerCfg[1].InputOffset = 0; hdma2d.LayerCfg[1].InputColorMode = DMA2D_INPUT_RGB888; hdma2d.LayerCfg[1].AlphaMode = DMA2D_NO_MODIF_ALPHA; hdma2d.LayerCfg[1].InputAlpha = 0; hdma2d.LayerCfg[1].AlphaInverted = DMA2D_REGULAR_ALPHA; hdma2d.LayerCfg[1].RedBlueSwap = DMA2D_RB_REGULAR; hdma2d.LayerCfg[1].ChromaSubSampling = DMA2D_NO_CSS; if (HAL_DMA2D_Init(&hdma2d) != HAL_OK) { Error_Handler(); } if (HAL_DMA2D_ConfigLayer(&hdma2d, 1) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN DMA2D_Init 2 */ /* USER CODE END DMA2D_Init 2 */ } /** * @brief DSIHOST Initialization Function * @param None * @retval None */ static void MX_DSIHOST_DSI_Init(void) { /* USER CODE BEGIN DSIHOST_Init 0 */ //THIS USES A RESET LINE TO RESET THE DSI - WE DON@T HAVE THIS HAL_GPIO_WritePin(LCD_RST_GPIO_Port , LCD_RST_Pin , GPIO_PIN_RESET); HAL_Delay(20);/* wait 20 ms */ HAL_GPIO_WritePin(LCD_RST_GPIO_Port , LCD_RST_Pin, GPIO_PIN_SET);/* Deactivate XRES */ HAL_Delay(10);/* Wait for 10ms after releasing XRES before sending commands */ /* USER CODE END DSIHOST_Init 0 */ DSI_PLLInitTypeDef PLLInit = {0}; DSI_HOST_TimeoutTypeDef HostTimeouts = {0}; DSI_PHY_TimerTypeDef PhyTimings = {0}; DSI_LPCmdTypeDef LPCmd = {0}; DSI_CmdCfgTypeDef CmdCfg = {0}; /* USER CODE BEGIN DSIHOST_Init 1 */ /* USER CODE END DSIHOST_Init 1 */ hdsi.Instance = DSI; hdsi.Init.AutomaticClockLaneControl = DSI_AUTO_CLK_LANE_CTRL_DISABLE; hdsi.Init.TXEscapeCkdiv = 4; hdsi.Init.NumberOfLanes = DSI_TWO_DATA_LANES; PLLInit.PLLNDIV = 99; PLLInit.PLLIDF = DSI_PLL_IN_DIV2; PLLInit.PLLODF = DSI_PLL_OUT_DIV2; if (HAL_DSI_Init(&hdsi, &PLLInit) != HAL_OK) { Error_Handler(); } HostTimeouts.TimeoutCkdiv = 1; HostTimeouts.HighSpeedTransmissionTimeout = 0; HostTimeouts.LowPowerReceptionTimeout = 0; HostTimeouts.HighSpeedReadTimeout = 0; HostTimeouts.LowPowerReadTimeout = 0; HostTimeouts.HighSpeedWriteTimeout = 0; HostTimeouts.HighSpeedWritePrespMode = DSI_HS_PM_DISABLE; HostTimeouts.LowPowerWriteTimeout = 0; HostTimeouts.BTATimeout = 0; if (HAL_DSI_ConfigHostTimeouts(&hdsi, &HostTimeouts) != HAL_OK) { Error_Handler(); } PhyTimings.ClockLaneHS2LPTime = 28; PhyTimings.ClockLaneLP2HSTime = 33; PhyTimings.DataLaneHS2LPTime = 15; PhyTimings.DataLaneLP2HSTime = 21; PhyTimings.DataLaneMaxReadTime = 0; PhyTimings.StopWaitTime = 10; if (HAL_DSI_ConfigPhyTimer(&hdsi, &PhyTimings) != HAL_OK) { Error_Handler(); } if (HAL_DSI_SetLowPowerRXFilter(&hdsi, 10000) != HAL_OK) { Error_Handler(); } if (HAL_DSI_ConfigErrorMonitor(&hdsi, HAL_DSI_ERROR_NONE) != HAL_OK) { Error_Handler(); } LPCmd.LPGenShortWriteNoP = DSI_LP_GSW0P_DISABLE; LPCmd.LPGenShortWriteOneP = DSI_LP_GSW1P_DISABLE; LPCmd.LPGenShortWriteTwoP = DSI_LP_GSW2P_DISABLE; LPCmd.LPGenShortReadNoP = DSI_LP_GSR0P_DISABLE; LPCmd.LPGenShortReadOneP = DSI_LP_GSR1P_DISABLE; LPCmd.LPGenShortReadTwoP = DSI_LP_GSR2P_DISABLE; LPCmd.LPGenLongWrite = DSI_LP_GLW_DISABLE; LPCmd.LPDcsShortWriteNoP = DSI_LP_DSW0P_DISABLE; LPCmd.LPDcsShortWriteOneP = DSI_LP_DSW1P_DISABLE; LPCmd.LPDcsShortReadNoP = DSI_LP_DSR0P_DISABLE; LPCmd.LPDcsLongWrite = DSI_LP_DLW_DISABLE; LPCmd.LPMaxReadPacket = DSI_LP_MRDP_DISABLE; LPCmd.AcknowledgeRequest = DSI_ACKNOWLEDGE_DISABLE; if (HAL_DSI_ConfigCommand(&hdsi, &LPCmd) != HAL_OK) { Error_Handler(); } CmdCfg.VirtualChannelID = 0; CmdCfg.ColorCoding = DSI_RGB888; CmdCfg.CommandSize = 800; CmdCfg.TearingEffectSource = DSI_TE_DSILINK; CmdCfg.TearingEffectPolarity = DSI_TE_RISING_EDGE; CmdCfg.HSPolarity = DSI_HSYNC_ACTIVE_LOW; CmdCfg.VSPolarity = DSI_VSYNC_ACTIVE_LOW; CmdCfg.DEPolarity = DSI_DATA_ENABLE_ACTIVE_HIGH; CmdCfg.VSyncPol = DSI_VSYNC_FALLING; CmdCfg.AutomaticRefresh = DSI_AR_DISABLE; CmdCfg.TEAcknowledgeRequest = DSI_TE_ACKNOWLEDGE_ENABLE; if (HAL_DSI_ConfigAdaptedCommandMode(&hdsi, &CmdCfg) != HAL_OK) { Error_Handler(); } if (HAL_DSI_SetGenericVCID(&hdsi, 0) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN DSIHOST_Init 2 */ HAL_DSI_SetLanePinsConfiguration(&hdsi, DSI_SWAP_LANE_PINS, DSI_CLK_LANE, ENABLE); HAL_DSI_SetLanePinsConfiguration(&hdsi, DSI_SWAP_LANE_PINS, DSI_DATA_LANE0, ENABLE); HAL_DSI_SetLanePinsConfiguration(&hdsi, DSI_SWAP_LANE_PINS, DSI_DATA_LANE1, ENABLE); HAL_DSI_Start(&hdsi); PhyTimings.ClockLaneHS2LPTime = 35; PhyTimings.ClockLaneLP2HSTime = 35; PhyTimings.DataLaneHS2LPTime = 35; PhyTimings.DataLaneLP2HSTime = 35; PhyTimings.DataLaneMaxReadTime = 0; PhyTimings.StopWaitTime = 10; HAL_DSI_ConfigPhyTimer(&hdsi, &PhyTimings); /* Initialize the OTM8009A LCD Display IC Driver (KoD LCD IC Driver) */ IOCtx.Address = 0; IOCtx.GetTick = HAL_GetTick; IOCtx.WriteReg = DSI_IO_Write; IOCtx.ReadReg = DSI_IO_Read; OTM8009A_RegisterBusIO(&OTM8009AObj, &IOCtx); Lcd_CompObj=(&OTM8009AObj); OTM8009A_Init(Lcd_CompObj, OTM8009A_COLMOD_RGB888, OTM8009A_ORIENTATION_LANDSCAPE); HAL_DSI_ConfigFlowControl(&hdsi, DSI_FLOW_CONTROL_BTA); HAL_DSI_ForceRXLowPower(&hdsi, ENABLE); uint8_t pScanCol[] = {0x02, 0x15}; /* Scan @ 533 */ HAL_DSI_LongWrite(&hdsi, 0, DSI_DCS_LONG_PKT_WRITE, 2, OTM8009A_CMD_WRTESCN, pScanCol); /* Send Display On DCS Command to display */ //HAL_DSI_ShortWrite(&(hdsi), // 0, // DSI_DCS_SHORT_PKT_WRITE_P1, // OTM8009A_CMD_DISPON, // 0x00); //HAL_DSI_Refresh(&hdsi); return; /* USER CODE END DSIHOST_Init 2 */ } /** * @brief LTDC Initialization Function * @param None * @retval None */ static void MX_LTDC_Init(void) { /* USER CODE BEGIN LTDC_Init 0 */ /* USER CODE END LTDC_Init 0 */ LTDC_LayerCfgTypeDef pLayerCfg = {0}; /* USER CODE BEGIN LTDC_Init 1 */ /* USER CODE END LTDC_Init 1 */ hltdc.Instance = LTDC; hltdc.Init.HSPolarity = LTDC_HSPOLARITY_AL; hltdc.Init.VSPolarity = LTDC_VSPOLARITY_AL; hltdc.Init.DEPolarity = LTDC_DEPOLARITY_AL; hltdc.Init.PCPolarity = LTDC_PCPOLARITY_IPC; hltdc.Init.HorizontalSync = 0; hltdc.Init.VerticalSync = 0; hltdc.Init.AccumulatedHBP = 2; hltdc.Init.AccumulatedVBP = 2; hltdc.Init.AccumulatedActiveW = 802; hltdc.Init.AccumulatedActiveH = 482; hltdc.Init.TotalWidth = 803; hltdc.Init.TotalHeigh = 483; hltdc.Init.Backcolor.Blue = 0; hltdc.Init.Backcolor.Green = 0; hltdc.Init.Backcolor.Red = 0; if (HAL_LTDC_Init(&hltdc) != HAL_OK) { Error_Handler(); } pLayerCfg.WindowX0 = 0; pLayerCfg.WindowX1 = 800; pLayerCfg.WindowY0 = 0; pLayerCfg.WindowY1 = 480; pLayerCfg.PixelFormat = LTDC_PIXEL_FORMAT_RGB888; pLayerCfg.Alpha = 255; pLayerCfg.Alpha0 = 0; pLayerCfg.BlendingFactor1 = LTDC_BLENDING_FACTOR1_PAxCA; pLayerCfg.BlendingFactor2 = LTDC_BLENDING_FACTOR2_PAxCA; pLayerCfg.FBStartAdress = 0xD0000000; pLayerCfg.ImageWidth = 800; pLayerCfg.ImageHeight = 480; pLayerCfg.Backcolor.Blue = 0; pLayerCfg.Backcolor.Green = 0; pLayerCfg.Backcolor.Red = 0; if (HAL_LTDC_ConfigLayer(&hltdc, &pLayerCfg, 0) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN LTDC_Init 2 */ /* USER CODE END LTDC_Init 2 */ } /** * @brief QUADSPI Initialization Function * @param None * @retval None */ static void MX_QUADSPI_Init(void) { /* USER CODE BEGIN QUADSPI_Init 0 */ /* USER CODE END QUADSPI_Init 0 */ /* USER CODE BEGIN QUADSPI_Init 1 */ /* USER CODE END QUADSPI_Init 1 */ /* QUADSPI parameter configuration*/ hqspi.Instance = QUADSPI; hqspi.Init.ClockPrescaler = 3; hqspi.Init.FifoThreshold = 1; hqspi.Init.SampleShifting = QSPI_SAMPLE_SHIFTING_NONE; hqspi.Init.FlashSize = 1; hqspi.Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_1_CYCLE; hqspi.Init.ClockMode = QSPI_CLOCK_MODE_0; hqspi.Init.DualFlash = QSPI_DUALFLASH_ENABLE; if (HAL_QSPI_Init(&hqspi) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN QUADSPI_Init 2 */ //TODO: Crib QSPI init from BSP MT25QL512ABB_Interface_t mode = MT25QL512ABB_SPI_MODE; MT25QL512ABB_DualFlash_t dualFlash = MT25QL512ABB_DUALFLASH_DISABLE; MT25QL512ABB_Transfer_t transferRate = MT25QL512ABB_DTR_TRANSFER; //TODO: Crib QSPI init from BSP //if (BSP_QSPI_Init(0,&init) != BSP_ERROR_NONE) //{ // Error_Handler(); //} //if (BSP_QSPI_EnableMemoryMappedMode(0) != BSP_ERROR_NONE) //{ // Error_Handler(); //} /* USER CODE END QUADSPI_Init 2 */ } /** * @brief SPI6 Initialization Function * @param None * @retval None */ static void MX_SPI6_Init(void) { /* USER CODE BEGIN SPI6_Init 0 */ /* USER CODE END SPI6_Init 0 */ /* USER CODE BEGIN SPI6_Init 1 */ /* USER CODE END SPI6_Init 1 */ /* SPI6 parameter configuration*/ hspi6.Instance = SPI6; hspi6.Init.Mode = SPI_MODE_MASTER; hspi6.Init.Direction = SPI_DIRECTION_2LINES_TXONLY; hspi6.Init.DataSize = SPI_DATASIZE_4BIT; hspi6.Init.CLKPolarity = SPI_POLARITY_LOW; hspi6.Init.CLKPhase = SPI_PHASE_1EDGE; hspi6.Init.NSS = SPI_NSS_SOFT; hspi6.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2; hspi6.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi6.Init.TIMode = SPI_TIMODE_DISABLE; hspi6.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi6.Init.CRCPolynomial = 0x0; hspi6.Init.NSSPMode = SPI_NSS_PULSE_ENABLE; hspi6.Init.NSSPolarity = SPI_NSS_POLARITY_LOW; hspi6.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA; hspi6.Init.TxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN; hspi6.Init.RxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN; hspi6.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE; hspi6.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE; hspi6.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE; hspi6.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE; hspi6.Init.IOSwap = SPI_IO_SWAP_DISABLE; if (HAL_SPI_Init(&hspi6) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN SPI6_Init 2 */ /* USER CODE END SPI6_Init 2 */ } /** * Enable DMA controller clock */ static void MX_DMA_Init(void) { /* DMA controller clock enable */ __HAL_RCC_DMA1_CLK_ENABLE(); } /* FMC initialization function */ void MX_FMC_Init(void) { /* USER CODE BEGIN FMC_Init 0 */ /* USER CODE END FMC_Init 0 */ FMC_SDRAM_TimingTypeDef SdramTiming = {0}; /* USER CODE BEGIN FMC_Init 1 */ /* USER CODE END FMC_Init 1 */ /** Perform the SDRAM1 memory initialization sequence */ hsdram1.Instance = FMC_SDRAM_DEVICE; /* hsdram1.Init */ hsdram1.Init.SDBank = FMC_SDRAM_BANK2; hsdram1.Init.ColumnBitsNumber = FMC_SDRAM_COLUMN_BITS_NUM_9; hsdram1.Init.RowBitsNumber = FMC_SDRAM_ROW_BITS_NUM_12; hsdram1.Init.MemoryDataWidth = FMC_SDRAM_MEM_BUS_WIDTH_32; hsdram1.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4; hsdram1.Init.CASLatency = FMC_SDRAM_CAS_LATENCY_3; hsdram1.Init.WriteProtection = FMC_SDRAM_WRITE_PROTECTION_DISABLE; hsdram1.Init.SDClockPeriod = FMC_SDRAM_CLOCK_PERIOD_2; hsdram1.Init.ReadBurst = FMC_SDRAM_RBURST_ENABLE; hsdram1.Init.ReadPipeDelay = FMC_SDRAM_RPIPE_DELAY_0; /* SdramTiming */ SdramTiming.LoadToActiveDelay = 2; SdramTiming.ExitSelfRefreshDelay = 7; SdramTiming.SelfRefreshTime = 4; SdramTiming.RowCycleDelay = 6; SdramTiming.WriteRecoveryTime = 2; SdramTiming.RPDelay = 2; SdramTiming.RCDDelay = 2; if (HAL_SDRAM_Init(&hsdram1, &SdramTiming) != HAL_OK) { Error_Handler( ); } /* USER CODE BEGIN FMC_Init 2 */ /* USER CODE END FMC_Init 2 */ } /** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* USER CODE BEGIN MX_GPIO_Init_1 */ /* USER CODE END MX_GPIO_Init_1 */ /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOI_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOE_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOH_CLK_ENABLE(); __HAL_RCC_GPIOG_CLK_ENABLE(); __HAL_RCC_GPIOD_CLK_ENABLE(); __HAL_RCC_GPIOF_CLK_ENABLE(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(QSPI_RST_GPIO_Port, QSPI_RST_Pin, GPIO_PIN_SET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(LCD_RST_GPIO_Port, LCD_RST_Pin, GPIO_PIN_SET); /*Configure GPIO pin : QSPI_RST_Pin */ GPIO_InitStruct.Pin = QSPI_RST_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(QSPI_RST_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pin : LCD_RST_Pin */ GPIO_InitStruct.Pin = LCD_RST_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; HAL_GPIO_Init(LCD_RST_GPIO_Port, &GPIO_InitStruct); /* USER CODE BEGIN MX_GPIO_Init_2 */ /* USER CODE END MX_GPIO_Init_2 */ } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /* USER CODE BEGIN Header_StartDefaultTask */ /** * @brief Function implementing the defaultTask thread. * @param argument: Not used * @retval None */ /* USER CODE END Header_StartDefaultTask */ void StartDefaultTask(void *argument) { /* USER CODE BEGIN 5 */ /* Infinite loop */ for(;;) { osDelay(400); } /* USER CODE END 5 */ } /* USER CODE BEGIN Header_startTGFXTask */ /** * @brief Function implementing the touchGFXTask thread. * @param argument: Not used * @retval None */ /* USER CODE END Header_startTGFXTask */ void startTGFXTask(void *argument) { /* USER CODE BEGIN startTGFXTask */ MX_TouchGFX_Process(); /* Infinite loop */ for(;;) { osDelay(1); } /* USER CODE END startTGFXTask */ } /* MPU Configuration */ void MPU_Config(void) { MPU_Region_InitTypeDef MPU_InitStruct = {0}; /* Disables the MPU */ HAL_MPU_Disable(); /** Initializes and configures the Region and the memory to be protected */ MPU_InitStruct.Enable = MPU_REGION_ENABLE; MPU_InitStruct.Number = MPU_REGION_NUMBER0; MPU_InitStruct.BaseAddress = 0x90000000; MPU_InitStruct.Size = MPU_REGION_SIZE_256MB; MPU_InitStruct.SubRegionDisable = 0x0; MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0; MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS; MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE; MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE; MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE; MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE; HAL_MPU_ConfigRegion(&MPU_InitStruct); /** Initializes and configures the Region and the memory to be protected */ MPU_InitStruct.Number = MPU_REGION_NUMBER1; MPU_InitStruct.Size = MPU_REGION_SIZE_128MB; HAL_MPU_ConfigRegion(&MPU_InitStruct); /** Initializes and configures the Region and the memory to be protected */ MPU_InitStruct.Number = MPU_REGION_NUMBER2; MPU_InitStruct.BaseAddress = 0xD0000000; MPU_InitStruct.Size = MPU_REGION_SIZE_32MB; MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE; HAL_MPU_ConfigRegion(&MPU_InitStruct); /** Initializes and configures the Region and the memory to be protected */ MPU_InitStruct.Number = MPU_REGION_NUMBER3; MPU_InitStruct.BaseAddress = 0x24000000; MPU_InitStruct.Size = MPU_REGION_SIZE_512KB; MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE; HAL_MPU_ConfigRegion(&MPU_InitStruct); /** Initializes and configures the Region and the memory to be protected */ MPU_InitStruct.Number = MPU_REGION_NUMBER4; MPU_InitStruct.BaseAddress = 0x10000000; MPU_InitStruct.Size = MPU_REGION_SIZE_256KB; HAL_MPU_ConfigRegion(&MPU_InitStruct); /** Initializes and configures the Region and the memory to be protected */ MPU_InitStruct.Number = MPU_REGION_NUMBER5; MPU_InitStruct.BaseAddress = 0x10040000; MPU_InitStruct.Size = MPU_REGION_SIZE_32KB; MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE; HAL_MPU_ConfigRegion(&MPU_InitStruct); /* Enables the MPU */ HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT); } /** * @brief Period elapsed callback in non blocking mode * @note This function is called when TIM6 interrupt took place, inside * HAL_TIM_IRQHandler(). It makes a direct call to HAL_IncTick() to increment * a global variable "uwTick" used as application time base. * @param htim : TIM handle * @retval None */ void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim) { /* USER CODE BEGIN Callback 0 */ /* USER CODE END Callback 0 */ if (htim->Instance == TIM6) { HAL_IncTick(); } /* USER CODE BEGIN Callback 1 */ /* USER CODE END Callback 1 */ } /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */