/* ****************************************************************************** ** ** @file : LinkerScript.ld ** ** @author : STM32CubeIDE ** ** Abstract : Linker script for STM32H7Sxx Device ** 128KBytes FLASH ** 456KBytes RAM ** ** Set heap size, stack size and stack location according ** to application requirements. ** ** Set memory bank area and size if external memory is used ** ** Target : STMicroelectronics STM32 ** ** Distribution: The file is distributed as is, without any warranty ** of any kind. ** ****************************************************************************** ** @attention ** ** Copyright (c) 2024 STMicroelectronics. ** All rights reserved. ** ** This software is licensed under terms that can be found in the LICENSE file ** in the root directory of this software component. ** If no LICENSE file comes with this software, it is provided AS-IS. ** ****************************************************************************** */ /* Entry Point */ ENTRY(Reset_Handler) /* Highest address of the user mode stack */ _estack = ORIGIN(DTCM) + LENGTH(DTCM); /* end of "DTCM" Ram type memory */ _Min_Heap_Size = 0x1000; /* required amount of heap */ _Min_Stack_Size = 0x1000; /* required amount of stack */ /* Memories definition */ MEMORY { RAM (rw) : ORIGIN = 0x24000000, LENGTH = 0x0006e000 RAM_CMD (rw) : ORIGIN = 0x2406e000, LENGTH = 0x00004000 ITCM (rw) : ORIGIN = 0x00000000, LENGTH = 0x00010000 DTCM (rw) : ORIGIN = 0x20000000, LENGTH = 0x00003000 DTCM_RTOS (rw) : ORIGIN = 0x20003000, LENGTH = 0x0000D000 SRAMAHB (rw) : ORIGIN = 0x30000000, LENGTH = 0x00008000 BKPSRAM (rw) : ORIGIN = 0x38800000, LENGTH = 0x00001000 FLASH (xr) : ORIGIN = 0x70000000, LENGTH = 0x00200000 FLASH_GFX (r) : ORIGIN = 0x70200000, LENGTH = 0x07e00000 EXTRAM (rw) : ORIGIN = 0x90000000, LENGTH = 0x02000000 } /* Sections */ SECTIONS { /* The startup code into "FLASH" FLASH type memory */ .isr_vector : { . = ALIGN(4); KEEP(*(.isr_vector)) /* Startup code */ . = ALIGN(4); } >FLASH /* The program code and other data into "FLASH" FLASH type memory */ .text : { . = ALIGN(4); *(.text) /* .text sections (code) */ *(.text*) /* .text* sections (code) */ *(.glue_7) /* glue arm to thumb code */ *(.glue_7t) /* glue thumb to arm code */ *(.eh_frame) KEEP (*(.init)) KEEP (*(.fini)) . = ALIGN(4); _etext = .; /* define a global symbols at end of code */ } >FLASH /* Constant data into "FLASH" FLASH type memory */ .rodata : { . = ALIGN(4); *(.rodata) /* .rodata sections (constants, strings, etc.) */ *(.rodata*) /* .rodata* sections (constants, strings, etc.) */ . = ALIGN(4); } >FLASH .ARM.extab : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */ { . = ALIGN(4); *(.ARM.extab* .gnu.linkonce.armextab.*) . = ALIGN(4); } >FLASH .ARM : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */ { . = ALIGN(4); __exidx_start = .; *(.ARM.exidx*) __exidx_end = .; . = ALIGN(4); } >FLASH .preinit_array : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */ { . = ALIGN(4); PROVIDE_HIDDEN (__preinit_array_start = .); KEEP (*(.preinit_array*)) PROVIDE_HIDDEN (__preinit_array_end = .); . = ALIGN(4); } >FLASH .init_array : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */ { . = ALIGN(4); PROVIDE_HIDDEN (__init_array_start = .); KEEP (*(SORT(.init_array.*))) KEEP (*(.init_array*)) PROVIDE_HIDDEN (__init_array_end = .); . = ALIGN(4); } >FLASH .fini_array : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */ { . = ALIGN(4); PROVIDE_HIDDEN (__fini_array_start = .); KEEP (*(SORT(.fini_array.*))) KEEP (*(.fini_array*)) PROVIDE_HIDDEN (__fini_array_end = .); . = ALIGN(4); } >FLASH /* Used by the startup to initialize data */ _sidata = LOADADDR(.data); FreeRtosHeapSection : { *(.bss.ucHeap) . = ALIGN(0x8); } >DTCM_RTOS /* Initialized data sections into "RAM" Ram type memory */ .data : { . = ALIGN(4); _sdata = .; /* create a global symbol at data start */ *(.data) /* .data sections */ *(.data*) /* .data* sections */ *(.RamFunc) /* .RamFunc sections */ *(.RamFunc*) /* .RamFunc* sections */ . = ALIGN(4); _edata = .; /* define a global symbol at data end */ } >RAM AT> FLASH /* Uninitialized data section into "RAM" Ram type memory */ . = ALIGN(4); .bss : { /* This is used by the startup in order to initialize the .bss section */ _sbss = .; /* define a global symbol at bss start */ __bss_start__ = _sbss; *(.bss) *(.bss*) *(COMMON) . = ALIGN(4); _ebss = .; /* define a global symbol at bss end */ __bss_end__ = _ebss; } >RAM /* User_heap_stack section, used to check that there is enough "RAM" Ram type memory left */ ._user_heap_stack : { . = ALIGN(8); PROVIDE ( end = . ); PROVIDE ( _end = . ); . = . + _Min_Heap_Size; . = . + _Min_Stack_Size; . = ALIGN(8); } >DTCM /* Remove information from the compiler libraries */ /DISCARD/ : { libc.a ( * ) libm.a ( * ) libgcc.a ( * ) } .ARM.attributes 0 : { *(.ARM.attributes) } BufferSection (NOLOAD) : { *(TouchGFX_Framebuffer TouchGFX_Framebuffer.*) *(.gnu.linkonce.r.*) . = ALIGN(0x8); *(Nemagfx_Stencil_Buffer Nemagfx_Stencil_Buffer.*) *(.gnu.linkonce.r.*) . = ALIGN(0x8); *(MyImage MyImage.*) *(.gnu.linkonce.r.*) . = ALIGN(0x8); } >EXTRAM UncachedSection (NOLOAD) : { *(Nemagfx_Memory_Pool_Buffer Nemagfx_Memory_Pool_Buffer.*) *(.gnu.linkonce.r.*) . = ALIGN(0x8); } >RAM_CMD FontFlashSection : { *(FontFlashSection FontFlashSection.*) *(.gnu.linkonce.r.*) . = ALIGN(0x4); } >FLASH_GFX TextFlashSection : { *(TextFlashSection TextFlashSection.*) *(.gnu.linkonce.r.*) . = ALIGN(0x4); } >FLASH_GFX ExtFlashSection : { *(ExtFlashSection ExtFlashSection.*) *(.gnu.linkonce.r.*) . = ALIGN(0x4); } >FLASH_GFX }