/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.h * @brief : Header for main.c file. * This file contains the common defines of the application. ****************************************************************************** * @attention * * Copyright (c) 2024 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Define to prevent recursive inclusion -------------------------------------*/ #ifndef __MAIN_H #define __MAIN_H #ifdef __cplusplus extern "C" { #endif /* Includes ------------------------------------------------------------------*/ #include "stm32l4xx_hal.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ /* USER CODE END Includes */ /* Exported types ------------------------------------------------------------*/ /* USER CODE BEGIN ET */ extern SPI_HandleTypeDef hspi2; extern TIM_HandleTypeDef htim7; extern DMA_HandleTypeDef hdma_spi2_tx; extern int count;; /* USER CODE END ET */ /* Exported constants --------------------------------------------------------*/ /* USER CODE BEGIN EC */ /* USER CODE END EC */ /* Exported macro ------------------------------------------------------------*/ /* USER CODE BEGIN EM */ /* USER CODE END EM */ /* Exported functions prototypes ---------------------------------------------*/ void Error_Handler(void); /* USER CODE BEGIN EFP */ /* USER CODE END EFP */ /* Private defines -----------------------------------------------------------*/ #define LCD_Rst_Pin GPIO_PIN_7 #define LCD_Rst_GPIO_Port GPIOI #define SPI2_MISO_Pin GPIO_PIN_2 #define SPI2_MISO_GPIO_Port GPIOI #define SPI_MOSI_Pin GPIO_PIN_3 #define SPI_MOSI_GPIO_Port GPIOI #define LCD_WR_Pin GPIO_PIN_8 #define LCD_WR_GPIO_Port GPIOG #define STMOD_INT_Pin GPIO_PIN_6 #define STMOD_INT_GPIO_Port GPIOC #define STMOD_INT_EXTI_IRQn EXTI9_5_IRQn #define LCD_RD_Pin GPIO_PIN_7 #define LCD_RD_GPIO_Port GPIOG #define LED_GREEN_Pin GPIO_PIN_4 #define LED_GREEN_GPIO_Port GPIOH #define SPI2_CS_Pin GPIO_PIN_6 #define SPI2_CS_GPIO_Port GPIOA #define MFX_WAKEUP_Pin GPIO_PIN_2 #define MFX_WAKEUP_GPIO_Port GPIOB #define SPI2_CLK_Pin GPIO_PIN_13 #define SPI2_CLK_GPIO_Port GPIOB /* USER CODE BEGIN Private defines */ /* USER CODE END Private defines */ #ifdef __cplusplus } #endif #endif /* __MAIN_H */