/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * *

© Copyright (c) 2021 STMicroelectronics. * All rights reserved.

* * This software component is licensed by ST under BSD 3-Clause license, * the "License"; You may not use this file except in compliance with the * License. You may obtain a copy of the License at: * opensource.org/licenses/BSD-3-Clause * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" #include"KS0108.h" #include "stdio.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ ADC_HandleTypeDef hadc1; ADC_HandleTypeDef hadc2; ADC_HandleTypeDef hadc3; DMA_HandleTypeDef hdma_adc1; DMA_HandleTypeDef hdma_adc2; DMA_HandleTypeDef hdma_adc3; TIM_HandleTypeDef htim2; TIM_HandleTypeDef htim3; UART_HandleTypeDef huart3; uint32_t tim_redge1[4]={0}; uint32_t tim_fedge1[4]={0}; uint32_t tim_redge2[4]={0}; uint32_t tim_fedge2[4]={0}; uint32_t tim_redge3[4]={0}; uint32_t tim_fedge3[4]={0}; uint32_t tim_redge4[4]={0}; uint32_t tim_fedge4[4]={0}; uint32_t alen1=16; uint32_t alen2=16; uint32_t alen3=16; uint8_t show_tim=0; uint8_t adc_counter=0; /* USER CODE BEGIN PV */ /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_DMA_Init(void); static void MX_ADC1_Init(void); static void MX_ADC2_Init(void); static void MX_ADC3_Init(void); static void MX_TIM2_Init(void); static void TIMER3_INIT(void); static void MX_USART3_UART_Init(void); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ char st1[50]="ABCDF"; uint16_t num1[100]={0},num2[100]={0},num3[100]={0}; /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ //sprintf(st1,"number is %.3f",num1); /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_DMA_Init(); MX_ADC1_Init(); MX_ADC2_Init(); MX_ADC3_Init(); MX_TIM2_Init(); MX_USART3_UART_Init(); TIMER3_INIT(); /* USER CODE BEGIN 2 */ /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ GLCD_Initalize(); GLCD_ClearScreen(); GLCD_GoTo(0,1); GLCD_WriteString("::5552:55"); HAL_Delay(2000); GLCD_GoTo(65,1); GLCD_WriteString(st1); HAL_Delay(2000); //GLCD_ClearScreen(); HAL_ADC_Start(&hadc3); HAL_ADC_Start(&hadc2); for(int ii=0;ii<=49;ii++) { st1[ii]=0; } /* num1 = HAL_ADC_GetValue(&hadc1); num2 = HAL_ADC_GetValue(&hadc2); num3 = HAL_ADC_GetValue(&hadc3);*/ //HAL_ADC_Start(&hadc2);//(&hadc2,(uint32_t*)num3, 10 ); //HAL_ADC_Start(&hadc3);//(&hadc3,(uint32_t*)num2, 10 ); if( HAL_TIM_PWM_Start_IT(&htim2,TIM_CHANNEL_1)!=HAL_OK) { Error_Handler(); } while (1) { // GLCD_ClearScreen(); // show_tim=1; //HAL_DMA_Start_IT(&hdma_adc1, (uint16_t)num1, (uint16_t)&huart2.Instance->TDR, strlen(num1)); if(show_tim==1) { for(int j=0;j<14;j++) { GLCD_ClearScreen(); sprintf(st1,"ad1,%d=%d",j,num1[j]); GLCD_GoTo(0,0); HAL_Delay(80); GLCD_WriteString(st1); sprintf(st1,"ad2,%d=%d",j,num2[j]); GLCD_GoTo(0,1); HAL_Delay(80); GLCD_WriteString(st1); sprintf(st1,"ad3,%d=%d",j,num3[j]); GLCD_GoTo(0,2); HAL_Delay(80); GLCD_WriteString(st1); HAL_Delay(2000); } /* if(HAL_ADC_Start_DMA(&hadc1, (uint32_t*)num1, alen1)!=HAL_OK) { Error_Handler(); }*/ show_tim=0; HAL_ADC_Start(&hadc2); HAL_ADC_Start(&hadc3); if( HAL_TIM_PWM_Start_IT(&htim2,TIM_CHANNEL_1)!=HAL_OK) { Error_Handler(); } } // HAL_Delay(1); /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void HAL_TIM_PWM_PulseFinishedCallback(TIM_HandleTypeDef *htim) { /* Prevent unused argument(s) compilation warning */ if(htim->Instance==TIM2) { if(HAL_ADCEx_MultiModeStart_DMA(&hadc1, (uint32_t*)num1, 10)!=HAL_OK) { Error_Handler(); } if( HAL_TIM_PWM_Stop_IT(&htim2,TIM_CHANNEL_1)!=HAL_OK) { Error_Handler(); } //HAL_ADC_Stop(&hadc1); //show_tim=1; /*if(HAL_ADC_Start_DMA(&hadc1, (uint32_t*)num1, alen1)!=HAL_OK) { Error_Handler(); }*/ } /* NOTE : This function should not be modified, when the callback is needed, the HAL_TIM_PeriodElapsedCallback could be implemented in the user file */ } void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc) { if( HAL_ADCEx_MultiModeStop_DMA(&hadc1)!=HAL_OK) { Error_Handler(); } HAL_ADC_Stop_DMA(&hadc2); HAL_ADC_Stop_DMA(&hadc3); show_tim=1; } void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0}; /** Configure LSE Drive Capability */ HAL_PWR_EnableBkUpAccess(); /** Configure the main internal regulator output voltage */ __HAL_RCC_PWR_CLK_ENABLE(); __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3); /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = 4; RCC_OscInitStruct.PLL.PLLN = 72; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = 3; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK) { Error_Handler(); } PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USART3; PeriphClkInitStruct.Usart3ClockSelection = RCC_USART3CLKSOURCE_PCLK1; if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK) { Error_Handler(); } } /** * @brief ADC1 Initialization Function * @param None * @retval None */ static void TIMER3_INIT(void) { TIM_IC_InitTypeDef TIMER3_ICCONF; htim3.Instance=TIM3; htim3.Init.CounterMode=TIM_COUNTERMODE_UP; htim3.Init.Prescaler=1; htim3.Init.Period=0xFFFFFFFF; if(HAL_TIM_IC_Init(&htim3)!=HAL_OK) { Error_Handler(); } TIMER3_ICCONF.ICFilter=0; TIMER3_ICCONF.ICPolarity=TIM_ICPOLARITY_RISING ; TIMER3_ICCONF.ICPrescaler=TIM_ICPSC_DIV1; TIMER3_ICCONF.ICSelection=TIM_ICSELECTION_DIRECTTI; if(HAL_TIM_IC_ConfigChannel(&htim3, &TIMER3_ICCONF, TIM_CHANNEL_1)!=HAL_OK) { Error_Handler(); } TIMER3_ICCONF.ICFilter=0; TIMER3_ICCONF.ICPolarity=TIM_ICPOLARITY_RISING ; TIMER3_ICCONF.ICPrescaler=TIM_ICPSC_DIV1; TIMER3_ICCONF.ICSelection=TIM_ICSELECTION_DIRECTTI; if(HAL_TIM_IC_ConfigChannel(&htim3, &TIMER3_ICCONF, TIM_CHANNEL_2)!=HAL_OK) { Error_Handler(); } TIMER3_ICCONF.ICFilter=0; TIMER3_ICCONF.ICPolarity=TIM_ICPOLARITY_FALLING ; TIMER3_ICCONF.ICPrescaler=TIM_ICPSC_DIV1; TIMER3_ICCONF.ICSelection=TIM_ICSELECTION_DIRECTTI; if(HAL_TIM_IC_ConfigChannel(&htim3, &TIMER3_ICCONF, TIM_CHANNEL_3)!=HAL_OK) { Error_Handler(); } TIMER3_ICCONF.ICFilter=0; TIMER3_ICCONF.ICPolarity=TIM_ICPOLARITY_BOTHEDGE ; TIMER3_ICCONF.ICPrescaler=TIM_ICPSC_DIV1; TIMER3_ICCONF.ICSelection=TIM_ICSELECTION_DIRECTTI; if(HAL_TIM_IC_ConfigChannel(&htim3, &TIMER3_ICCONF, TIM_CHANNEL_4)!=HAL_OK) { Error_Handler(); } } void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim) { if(htim->Instance==TIM3) { if(htim->Channel== HAL_TIM_ACTIVE_CHANNEL_1) { // __HAL_TIM_SET_CAPTUREPOLARITY(&htim2, TIM_CHANNEL_4, TIM_INPUTCHANNELPOLARITY_FALLING); tim_redge1[4]=__HAL_TIM_GET_COMPARE(htim,TIM_CHANNEL_1); } else if (htim->Channel== HAL_TIM_ACTIVE_CHANNEL_2) { } else if (htim->Channel== HAL_TIM_ACTIVE_CHANNEL_3) { } else if (htim->Channel== HAL_TIM_ACTIVE_CHANNEL_4) { } } } static void MX_ADC1_Init(void) { /* USER CODE BEGIN ADC1_Init 0 */ /* USER CODE END ADC1_Init 0 */ ADC_MultiModeTypeDef multimode = {0}; ADC_ChannelConfTypeDef sConfig = {0}; /* USER CODE BEGIN ADC1_Init 1 */ /* USER CODE END ADC1_Init 1 */ /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion) */ hadc1.Instance = ADC1; hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2; hadc1.Init.Resolution = ADC_RESOLUTION_12B; hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE; hadc1.Init.ContinuousConvMode = ENABLE; hadc1.Init.DiscontinuousConvMode = DISABLE; hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START; hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc1.Init.NbrOfConversion = 1; hadc1.Init.DMAContinuousRequests = ENABLE; hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV; if (HAL_ADC_Init(&hadc1) != HAL_OK) { Error_Handler(); } /** Configure the ADC multi-mode */ multimode.Mode = ADC_TRIPLEMODE_INTERL; multimode.DMAAccessMode = ADC_DMAACCESSMODE_1 ; multimode.TwoSamplingDelay = ADC_TWOSAMPLINGDELAY_5CYCLES; if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK) { Error_Handler(); } /** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time. */ sConfig.Channel = ADC_CHANNEL_12; sConfig.Rank = ADC_REGULAR_RANK_1; sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN ADC1_Init 2 */ /* USER CODE END ADC1_Init 2 */ } /** * @brief ADC2 Initialization Function * @param None * @retval None */ static void MX_ADC2_Init(void) { /* USER CODE BEGIN ADC2_Init 0 */ /* USER CODE END ADC2_Init 0 */ ADC_ChannelConfTypeDef sConfig = {0}; /* USER CODE BEGIN ADC2_Init 1 */ /* USER CODE END ADC2_Init 1 */ /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion) */ hadc2.Instance = ADC2; hadc2.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2; hadc2.Init.Resolution = ADC_RESOLUTION_12B; hadc2.Init.ScanConvMode = ADC_SCAN_DISABLE; hadc2.Init.ContinuousConvMode = ENABLE; hadc2.Init.DiscontinuousConvMode = DISABLE; hadc2.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc2.Init.NbrOfConversion = 1; hadc2.Init.DMAContinuousRequests = ENABLE; hadc2.Init.EOCSelection = ADC_EOC_SINGLE_CONV; if (HAL_ADC_Init(&hadc2) != HAL_OK) { Error_Handler(); } /** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time. */ sConfig.Channel = ADC_CHANNEL_9; sConfig.Rank = ADC_REGULAR_RANK_1; sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES; if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN ADC2_Init 2 */ /* USER CODE END ADC2_Init 2 */ } /** * @brief ADC3 Initialization Function * @param None * @retval None */ static void MX_ADC3_Init(void) { /* USER CODE BEGIN ADC3_Init 0 */ /* USER CODE END ADC3_Init 0 */ ADC_ChannelConfTypeDef sConfig = {0}; /* USER CODE BEGIN ADC3_Init 1 */ /* USER CODE END ADC3_Init 1 */ /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion) */ hadc3.Instance = ADC3; hadc3.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2; hadc3.Init.Resolution = ADC_RESOLUTION_12B; hadc3.Init.ScanConvMode = ADC_SCAN_DISABLE; hadc3.Init.ContinuousConvMode = ENABLE; hadc3.Init.DiscontinuousConvMode = DISABLE; hadc3.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc3.Init.NbrOfConversion = 1; hadc3.Init.DMAContinuousRequests = ENABLE; hadc3.Init.EOCSelection = ADC_EOC_SINGLE_CONV; if (HAL_ADC_Init(&hadc3) != HAL_OK) { Error_Handler(); } /** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time. */ sConfig.Channel = ADC_CHANNEL_13; sConfig.Rank = ADC_REGULAR_RANK_1; sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES; if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN ADC3_Init 2 */ /* USER CODE END ADC3_Init 2 */ } /** * @brief TIM2 Initialization Function * @param None * @retval None */ static void MX_TIM2_Init(void) { /* USER CODE BEGIN TIM2_Init 0 */ /* USER CODE END TIM2_Init 0 */ TIM_MasterConfigTypeDef sMasterConfig = {0}; TIM_OC_InitTypeDef sConfigOC = {0}; /* USER CODE BEGIN TIM2_Init 1 */ /* USER CODE END TIM2_Init 1 */ htim2.Instance = TIM2; htim2.Init.Prescaler = 0; htim2.Init.CounterMode = TIM_COUNTERMODE_UP; htim2.Init.Period = 400; htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE; if (HAL_TIM_PWM_Init(&htim2) != HAL_OK) { Error_Handler(); } sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK) { Error_Handler(); } sConfigOC.OCMode = TIM_OCMODE_PWM1; sConfigOC.Pulse = 180; sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH; sConfigOC.OCFastMode = TIM_OCFAST_DISABLE; if (HAL_TIM_PWM_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_1) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN TIM2_Init 2 */ /* USER CODE END TIM2_Init 2 */ HAL_TIM_MspPostInit(&htim2); } /** * @brief USART3 Initialization Function * @param None * @retval None */ static void MX_USART3_UART_Init(void) { /* USER CODE BEGIN USART3_Init 0 */ /* USER CODE END USART3_Init 0 */ /* USER CODE BEGIN USART3_Init 1 */ /* USER CODE END USART3_Init 1 */ huart3.Instance = USART3; huart3.Init.BaudRate = 115200; huart3.Init.WordLength = UART_WORDLENGTH_8B; huart3.Init.StopBits = UART_STOPBITS_1; huart3.Init.Parity = UART_PARITY_NONE; huart3.Init.Mode = UART_MODE_TX_RX; huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart3.Init.OverSampling = UART_OVERSAMPLING_16; huart3.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; huart3.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; if (HAL_UART_Init(&huart3) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN USART3_Init 2 */ /* USER CODE END USART3_Init 2 */ } /** * Enable DMA controller clock */ static void MX_DMA_Init(void) { /* DMA controller clock enable */ __HAL_RCC_DMA2_CLK_ENABLE(); /* DMA interrupt init */ /* DMA2_Stream0_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA2_Stream0_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA2_Stream0_IRQn); /* DMA2_Stream1_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA2_Stream1_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA2_Stream1_IRQn); /* DMA2_Stream2_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA2_Stream2_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA2_Stream2_IRQn); } /** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOF_CLK_ENABLE(); __HAL_RCC_GPIOH_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); __HAL_RCC_GPIOD_CLK_ENABLE(); __HAL_RCC_GPIOG_CLK_ENABLE(); __HAL_RCC_GPIOE_CLK_ENABLE(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOF, GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3 |GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7 |GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10|GPIO_PIN_11 |GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOB, LD1_Pin|LD3_Pin|LD2_Pin, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(USB_PowerSwitchOn_GPIO_Port, USB_PowerSwitchOn_Pin, GPIO_PIN_RESET); /*Configure GPIO pin : USER_Btn_Pin */ GPIO_InitStruct.Pin = USER_Btn_Pin; GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(USER_Btn_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pins : PF0 PF1 PF2 PF3 PF4 PF5 PF6 PF7 PF8 PF9 PF10 PF11 PF12 PF13 PF14 PF15 */ GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3 |GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7 |GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10|GPIO_PIN_11 |GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOF, &GPIO_InitStruct); /*Configure GPIO pins : RMII_MDC_Pin RMII_RXD0_Pin RMII_RXD1_Pin */ GPIO_InitStruct.Pin = RMII_MDC_Pin|RMII_RXD0_Pin|RMII_RXD1_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF11_ETH; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); /*Configure GPIO pins : RMII_REF_CLK_Pin RMII_MDIO_Pin RMII_CRS_DV_Pin */ GPIO_InitStruct.Pin = RMII_REF_CLK_Pin|RMII_MDIO_Pin|RMII_CRS_DV_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF11_ETH; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); //configure channel 1,2,3,4 timer3 input capture GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7|GPIO_PIN_8|GPIO_PIN_9; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF2_TIM3; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); /*Configure GPIO pins : LD1_Pin LD3_Pin LD2_Pin */ GPIO_InitStruct.Pin = LD1_Pin|LD3_Pin|LD2_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); /*Configure GPIO pin : RMII_TXD1_Pin */ GPIO_InitStruct.Pin = RMII_TXD1_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF11_ETH; HAL_GPIO_Init(RMII_TXD1_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pin : USB_PowerSwitchOn_Pin */ GPIO_InitStruct.Pin = USB_PowerSwitchOn_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(USB_PowerSwitchOn_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pin : USB_OverCurrent_Pin */ GPIO_InitStruct.Pin = USB_OverCurrent_Pin; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(USB_OverCurrent_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pins : USB_SOF_Pin USB_ID_Pin USB_DM_Pin USB_DP_Pin */ GPIO_InitStruct.Pin = USB_SOF_Pin|USB_ID_Pin|USB_DM_Pin|USB_DP_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF10_OTG_FS; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /*Configure GPIO pin : USB_VBUS_Pin */ GPIO_InitStruct.Pin = USB_VBUS_Pin; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(USB_VBUS_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pins : RMII_TX_EN_Pin RMII_TXD0_Pin */ GPIO_InitStruct.Pin = RMII_TX_EN_Pin|RMII_TXD0_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF11_ETH; HAL_GPIO_Init(GPIOG, &GPIO_InitStruct); /*Configure GPIO pin : PB9 */ GPIO_InitStruct.Pin = GPIO_PIN_9; GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); /*Configure GPIO pins : PE0 PE1 */ GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1; GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOE, &GPIO_InitStruct); } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { __NOP(); /* sprintf(st1,"ERROR1",num1); HAL_Delay(1); GLCD_GoTo(0,1); GLCD_WriteString(st1);*/ } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */ /************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/