/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2024 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" #include "cmsis_os.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ #include "vcu.h" #include "gpio.h" /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ // #if defined( __ICCARM__ ) /* #define DMA_BUFFER \*/ // _Pragma("location=\".dma_buffer\"") // #else // #define DMA_BUFFER __attribute__((section(".dma_buffer123"))) // #endif /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ FDCAN_HandleTypeDef hfdcan1; UART_HandleTypeDef huart3; DMA_HandleTypeDef hdma_usart3_tx; DMA_HandleTypeDef hdma_usart3_rx; osThreadId fsm_taskHandle; /* USER CODE BEGIN PV */ /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MPU_Config(void); static void MX_GPIO_Init(void); static void MX_DMA_Init(void); static void MX_FDCAN1_Init(void); static void MX_USART3_UART_Init(void); void start_fsm_task(void const * argument); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ uint32_t uart_error_code = 0; uint32_t dma_error_code = 0; uint32_t uart_gstate = 0; uint32_t *ptr; uint8_t data5678[8] /*__ALIGNED(32)*/ __attribute__((section(".dma_buffer"))) = "abcdefg"; /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ __HAL_RCC_D2SRAM1_CLK_ENABLE(); // __HAL_RCC_AHBSRAM1_CLK_DISABLE(); // __HAL_RCC_D2SRAM1_CLK_ENABLE(); // __HAL_RCC_D2SRAM2_CLK_ENABLE(); // __HAL_RCC_D2SRAM3_CLK_ENABLE(); /* USER CODE END 1 */ /* MPU Configuration--------------------------------------------------------*/ MPU_Config(); /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_DMA_Init(); MX_FDCAN1_Init(); MX_USART3_UART_Init(); /* USER CODE BEGIN 2 */ // __HAL_RCC_D2SRAM1_CLK_ENABLE(); // __HAL_RCC_D2SRAM2_CLK_ENABLE(); // __HAL_RCC_D2SRAM3_CLK_ENABLE(); init_vcu(); /* USER CODE END 2 */ /* USER CODE BEGIN RTOS_MUTEX */ /* add mutexes, ... */ /* USER CODE END RTOS_MUTEX */ /* USER CODE BEGIN RTOS_SEMAPHORES */ /* add semaphores, ... */ /* USER CODE END RTOS_SEMAPHORES */ /* USER CODE BEGIN RTOS_TIMERS */ /* start timers, add new ones, ... */ /* USER CODE END RTOS_TIMERS */ /* USER CODE BEGIN RTOS_QUEUES */ /* add queues, ... */ /* USER CODE END RTOS_QUEUES */ /* Create the thread(s) */ /* definition and creation of fsm_task */ // osThreadDef(fsm_task, start_fsm_task, osPriorityRealtime, 0, 512); // fsm_taskHandle = osThreadCreate(osThread(fsm_task), NULL); /* USER CODE BEGIN RTOS_THREADS */ /* add threads, ... */ /* USER CODE END RTOS_THREADS */ /* Start scheduler */ // osKernelStart(); /* We should never get here as control is now taken by the scheduler */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ // uint8_t data[8] = "abcdefg"; uint32_t test1234 = 8; ptr = &test1234; while (1) { /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ // SCB_CleanDCache_by_Addr((uint32_t*)(((uint32_t)data5678) & ~(uint32_t)0x1F), 8+32); HAL_UART_Transmit_DMA(&huart3, data5678, test1234); HAL_Delay(1000); dma_error_code = hdma_usart3_tx.ErrorCode; uart_error_code = huart3.ErrorCode; uart_gstate = huart3.gState; GPIO_SET(LED_YELLOW, dma_error_code == 0); (void)(dma_error_code); if(HAL_GetTick() < 0) test1234 += 1; } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Supply configuration update enable */ HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY); /** Configure the main internal regulator output voltage */ __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3); while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {} /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_DIV1; RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI; RCC_OscInitStruct.PLL.PLLM = 4; RCC_OscInitStruct.PLL.PLLN = 9; RCC_OscInitStruct.PLL.PLLP = 2; RCC_OscInitStruct.PLL.PLLQ = 3; RCC_OscInitStruct.PLL.PLLR = 2; RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3; RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOMEDIUM; RCC_OscInitStruct.PLL.PLLFRACN = 3072; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2 |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI; RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2; RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2; RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV1; RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK) { Error_Handler(); } } /** * @brief FDCAN1 Initialization Function * @param None * @retval None */ static void MX_FDCAN1_Init(void) { /* USER CODE BEGIN FDCAN1_Init 0 */ /* USER CODE END FDCAN1_Init 0 */ /* USER CODE BEGIN FDCAN1_Init 1 */ /* USER CODE END FDCAN1_Init 1 */ hfdcan1.Instance = FDCAN1; hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC; hfdcan1.Init.Mode = FDCAN_MODE_NORMAL; hfdcan1.Init.AutoRetransmission = DISABLE; hfdcan1.Init.TransmitPause = DISABLE; hfdcan1.Init.ProtocolException = ENABLE; hfdcan1.Init.NominalPrescaler = 10; hfdcan1.Init.NominalSyncJumpWidth = 1; hfdcan1.Init.NominalTimeSeg1 = 7; hfdcan1.Init.NominalTimeSeg2 = 2; hfdcan1.Init.DataPrescaler = 1; hfdcan1.Init.DataSyncJumpWidth = 1; hfdcan1.Init.DataTimeSeg1 = 1; hfdcan1.Init.DataTimeSeg2 = 1; hfdcan1.Init.MessageRAMOffset = 0; hfdcan1.Init.StdFiltersNbr = 1; hfdcan1.Init.ExtFiltersNbr = 0; hfdcan1.Init.RxFifo0ElmtsNbr = 1; hfdcan1.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_8; hfdcan1.Init.RxFifo1ElmtsNbr = 0; hfdcan1.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8; hfdcan1.Init.RxBuffersNbr = 1; hfdcan1.Init.RxBufferSize = FDCAN_DATA_BYTES_8; hfdcan1.Init.TxEventsNbr = 0; hfdcan1.Init.TxBuffersNbr = 32; hfdcan1.Init.TxFifoQueueElmtsNbr = 32; hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION; hfdcan1.Init.TxElmtSize = FDCAN_DATA_BYTES_8; if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN FDCAN1_Init 2 */ /* USER CODE END FDCAN1_Init 2 */ } /** * @brief USART3 Initialization Function * @param None * @retval None */ static void MX_USART3_UART_Init(void) { /* USER CODE BEGIN USART3_Init 0 */ /* USER CODE END USART3_Init 0 */ /* USER CODE BEGIN USART3_Init 1 */ /* USER CODE END USART3_Init 1 */ huart3.Instance = USART3; huart3.Init.BaudRate = 115200; huart3.Init.WordLength = UART_WORDLENGTH_8B; huart3.Init.StopBits = UART_STOPBITS_1; huart3.Init.Parity = UART_PARITY_NONE; huart3.Init.Mode = UART_MODE_TX_RX; huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart3.Init.OverSampling = UART_OVERSAMPLING_16; huart3.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; huart3.Init.ClockPrescaler = UART_PRESCALER_DIV1; huart3.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; if (HAL_UART_Init(&huart3) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_SetTxFifoThreshold(&huart3, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_SetRxFifoThreshold(&huart3, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_DisableFifoMode(&huart3) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN USART3_Init 2 */ /* USER CODE END USART3_Init 2 */ } /** * Enable DMA controller clock */ static void MX_DMA_Init(void) { /* DMA controller clock enable */ __HAL_RCC_DMA1_CLK_ENABLE(); /* DMA interrupt init */ /* DMA1_Stream0_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA1_Stream0_IRQn, 10, 0); HAL_NVIC_EnableIRQ(DMA1_Stream0_IRQn); /* DMA1_Stream1_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA1_Stream1_IRQn, 10, 0); HAL_NVIC_EnableIRQ(DMA1_Stream1_IRQn); } /** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* USER CODE BEGIN MX_GPIO_Init_1 */ /* USER CODE END MX_GPIO_Init_1 */ /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); __HAL_RCC_GPIOD_CLK_ENABLE(); __HAL_RCC_GPIOE_CLK_ENABLE(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOB, LED_GREEN_Pin|LED_RED_Pin, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(LED_YELLOW_GPIO_Port, LED_YELLOW_Pin, GPIO_PIN_RESET); /*Configure GPIO pin : USER_BUTTON_Pin */ GPIO_InitStruct.Pin = USER_BUTTON_Pin; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(USER_BUTTON_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pins : LED_GREEN_Pin LED_RED_Pin */ GPIO_InitStruct.Pin = LED_GREEN_Pin|LED_RED_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); /*Configure GPIO pin : LED_YELLOW_Pin */ GPIO_InitStruct.Pin = LED_YELLOW_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(LED_YELLOW_GPIO_Port, &GPIO_InitStruct); /* USER CODE BEGIN MX_GPIO_Init_2 */ /* USER CODE END MX_GPIO_Init_2 */ } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /* USER CODE BEGIN Header_start_fsm_task */ /** * @brief Function implementing the fsm_task thread. * @param argument: Not used * @retval None */ /* USER CODE END Header_start_fsm_task */ __weak void start_fsm_task(void const * argument) { /* USER CODE BEGIN 5 */ /* Infinite loop */ for(;;) { osDelay(1); } /* USER CODE END 5 */ } /* MPU Configuration */ void MPU_Config(void) { MPU_Region_InitTypeDef MPU_InitStruct = {0}; /* Disables the MPU */ HAL_MPU_Disable(); /** Initializes and configures the Region and the memory to be protected */ MPU_InitStruct.Enable = MPU_REGION_ENABLE; MPU_InitStruct.Number = MPU_REGION_NUMBER0; MPU_InitStruct.BaseAddress = 0x30000000; MPU_InitStruct.Size = MPU_REGION_SIZE_128B; MPU_InitStruct.SubRegionDisable = 0x0; MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0; MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS; MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE; MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE; MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE; MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE; HAL_MPU_ConfigRegion(&MPU_InitStruct); /** Initializes and configures the Region and the memory to be protected */ HAL_MPU_ConfigRegion(&MPU_InitStruct); /* Enables the MPU */ HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT); } /** * @brief Period elapsed callback in non blocking mode * @note This function is called when TIM1 interrupt took place, inside * HAL_TIM_IRQHandler(). It makes a direct call to HAL_IncTick() to increment * a global variable "uwTick" used as application time base. * @param htim : TIM handle * @retval None */ void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim) { /* USER CODE BEGIN Callback 0 */ /* USER CODE END Callback 0 */ if (htim->Instance == TIM1) { HAL_IncTick(); } /* USER CODE BEGIN Callback 1 */ /* USER CODE END Callback 1 */ } /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */