/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file stm32f0xx_hal_conf.h * @brief HAL configuration file. ****************************************************************************** * @attention * * Copyright (c) 2016 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Define to prevent recursive inclusion -------------------------------------*/ #ifndef __STM32F0xx_HAL_CONF_H #define __STM32F0xx_HAL_CONF_H #ifdef __cplusplus extern "C" { #endif /* Exported types ------------------------------------------------------------*/ /* Exported constants --------------------------------------------------------*/ /* ########################## Module Selection ############################## */ /** * @brief This is the list of modules to be used in the HAL driver */ #define HAL_MODULE_ENABLED /*#define HAL_ADC_MODULE_ENABLED */ /*#define HAL_CRYP_MODULE_ENABLED */ /*#define HAL_CAN_MODULE_ENABLED */ /*#define HAL_CEC_MODULE_ENABLED */ /*#define HAL_COMP_MODULE_ENABLED */ /*#define HAL_CRC_MODULE_ENABLED */ /*#define HAL_CRYP_MODULE_ENABLED */ /*#define HAL_TSC_MODULE_ENABLED */ /*#define HAL_DAC_MODULE_ENABLED */ /*#define HAL_I2S_MODULE_ENABLED */ /*#define HAL_IWDG_MODULE_ENABLED */ /*#define HAL_LCD_MODULE_ENABLED */ /*#define HAL_LPTIM_MODULE_ENABLED */ /*#define HAL_RNG_MODULE_ENABLED */ /*#define HAL_RTC_MODULE_ENABLED */ /*#define HAL_SPI_MODULE_ENABLED */ /*#define HAL_TIM_MODULE_ENABLED */ /*#define HAL_UART_MODULE_ENABLED */ /*#define HAL_USART_MODULE_ENABLED */ /*#define HAL_IRDA_MODULE_ENABLED */ /*#define HAL_SMARTCARD_MODULE_ENABLED */ /*#define HAL_SMBUS_MODULE_ENABLED */ /*#define HAL_WWDG_MODULE_ENABLED */ /*#define HAL_PCD_MODULE_ENABLED */ #define HAL_CORTEX_MODULE_ENABLED #define HAL_DMA_MODULE_ENABLED #define HAL_FLASH_MODULE_ENABLED #define HAL_GPIO_MODULE_ENABLED #define HAL_EXTI_MODULE_ENABLED #define HAL_PWR_MODULE_ENABLED #define HAL_RCC_MODULE_ENABLED #define HAL_I2C_MODULE_ENABLED /* ########################## HSE/HSI Values adaptation ##################### */ /** * @brief Adjust the value of External High Speed oscillator (HSE) used in your application. * This value is used by the RCC HAL module to compute the system frequency * (when HSE is used as system clock source, directly or through the PLL). */ #if !defined (HSE_VALUE) #define HSE_VALUE ((uint32_t)8000000) /*!< Value of the External oscillator in Hz */ #endif /* HSE_VALUE */ /** * @brief In the following line adjust the External High Speed oscillator (HSE) Startup * Timeout value */ #if !defined (HSE_STARTUP_TIMEOUT) #define HSE_STARTUP_TIMEOUT ((uint32_t)100) /*!< Time out for HSE start up, in ms */ #endif /* HSE_STARTUP_TIMEOUT */ /** * @brief Internal High Speed oscillator (HSI) value. * This value is used by the RCC HAL module to compute the system frequency * (when HSI is used as system clock source, directly or through the PLL). */ #if !defined (HSI_VALUE) #define HSI_VALUE ((uint32_t)8000000) /*!< Value of the Internal oscillator in Hz*/ #endif /* HSI_VALUE */ /** * @brief In the following line adjust the Internal High Speed oscillator (HSI) Startup * Timeout value */ #if !defined (HSI_STARTUP_TIMEOUT) #define HSI_STARTUP_TIMEOUT ((uint32_t)5000) /*!< Time out for HSI start up */ #endif /* HSI_STARTUP_TIMEOUT */ /** * @brief Internal High Speed oscillator for ADC (HSI14) value. */ #if !defined (HSI14_VALUE) #define HSI14_VALUE ((uint32_t)14000000) /*!< Value of the Internal High Speed oscillator for ADC in Hz. The real value may vary depending on the variations in voltage and temperature. */ #endif /* HSI14_VALUE */ /** * @brief Internal High Speed oscillator for USB (HSI48) value. */ #if !defined (HSI48_VALUE) #define HSI48_VALUE ((uint32_t)48000000) /*!< Value of the Internal High Speed oscillator for USB in Hz. The real value may vary depending on the variations in voltage and temperature. */ #endif /* HSI48_VALUE */ /** * @brief Internal Low Speed oscillator (LSI) value. */ #if !defined (LSI_VALUE) #define LSI_VALUE ((uint32_t)40000) #endif /* LSI_VALUE */ /*!< Value of the Internal Low Speed oscillator in Hz The real value may vary depending on the variations in voltage and temperature. */ /** * @brief External Low Speed oscillator (LSI) value. */ #if !defined (LSE_VALUE) #define LSE_VALUE ((uint32_t)32768) /*!< Value of the External Low Speed oscillator in Hz */ #endif /* LSE_VALUE */ /** * @brief Time out for LSE start up value in ms. */ #if !defined (LSE_STARTUP_TIMEOUT) #define LSE_STARTUP_TIMEOUT ((uint32_t)5000) /*!< Time out for LSE start up, in ms */ #endif /* LSE_STARTUP_TIMEOUT */ /* Tip: To avoid modifying this file each time you need to use different HSE, === you can define the HSE value in your toolchain compiler preprocessor. */ /* ########################### System Configuration ######################### */ /** * @brief This is the HAL system configuration section */ #define VDD_VALUE ((uint32_t)3300) /*!< Value of VDD in mv */ #define TICK_INT_PRIORITY ((uint32_t)3) /*!< tick interrupt priority (lowest by default) */ /* Warning: Must be set to higher priority for HAL_Delay() */ /* and HAL_GetTick() usage under interrupt context */ #define USE_RTOS 0 #define PREFETCH_ENABLE 1 #define INSTRUCTION_CACHE_ENABLE 0 #define DATA_CACHE_ENABLE 0 #define USE_SPI_CRC 0U #define USE_HAL_ADC_REGISTER_CALLBACKS 0U /* ADC register callback disabled */ #define USE_HAL_CAN_REGISTER_CALLBACKS 0U /* CAN register callback disabled */ #define USE_HAL_COMP_REGISTER_CALLBACKS 0U /* COMP register callback disabled */ #define USE_HAL_CEC_REGISTER_CALLBACKS 0U /* CEC register callback disabled */ #define USE_HAL_DAC_REGISTER_CALLBACKS 0U /* DAC register callback disabled */ #define USE_HAL_I2C_REGISTER_CALLBACKS 1U /* I2C register callback enabled */ #define USE_HAL_SMBUS_REGISTER_CALLBACKS 0U /* SMBUS register callback disabled */ #define USE_HAL_UART_REGISTER_CALLBACKS 0U /* UART register callback disabled */ #define USE_HAL_USART_REGISTER_CALLBACKS 0U /* USART register callback disabled */ #define USE_HAL_IRDA_REGISTER_CALLBACKS 0U /* IRDA register callback disabled */ #define USE_HAL_SMARTCARD_REGISTER_CALLBACKS 0U /* SMARTCARD register callback disabled */ #define USE_HAL_WWDG_REGISTER_CALLBACKS 0U /* WWDG register callback disabled */ #define USE_HAL_RTC_REGISTER_CALLBACKS 0U /* RTC register callback disabled */ #define USE_HAL_SPI_REGISTER_CALLBACKS 0U /* SPI register callback disabled */ #define USE_HAL_I2S_REGISTER_CALLBACKS 0U /* I2S register callback disabled */ #define USE_HAL_TIM_REGISTER_CALLBACKS 0U /* TIM register callback disabled */ #define USE_HAL_TSC_REGISTER_CALLBACKS 0U /* TSC register callback disabled */ #define USE_HAL_PCD_REGISTER_CALLBACKS 0U /* PCD register callback disabled */ /* ########################## Assert Selection ############################## */ /** * @brief Uncomment the line below to expanse the "assert_param" macro in the * HAL drivers code */ /* #define USE_FULL_ASSERT 1U */ /* Includes ------------------------------------------------------------------*/ /** * @brief Include module's header file */ #ifdef HAL_RCC_MODULE_ENABLED #include "stm32f0xx_hal_rcc.h" #endif /* HAL_RCC_MODULE_ENABLED */ #ifdef HAL_GPIO_MODULE_ENABLED #include "stm32f0xx_hal_gpio.h" #endif /* HAL_GPIO_MODULE_ENABLED */ #ifdef HAL_EXTI_MODULE_ENABLED #include "stm32f0xx_hal_exti.h" #endif /* HAL_EXTI_MODULE_ENABLED */ #ifdef HAL_DMA_MODULE_ENABLED #include "stm32f0xx_hal_dma.h" #endif /* HAL_DMA_MODULE_ENABLED */ #ifdef HAL_CORTEX_MODULE_ENABLED #include "stm32f0xx_hal_cortex.h" #endif /* HAL_CORTEX_MODULE_ENABLED */ #ifdef HAL_ADC_MODULE_ENABLED #include "stm32f0xx_hal_adc.h" #endif /* HAL_ADC_MODULE_ENABLED */ #ifdef HAL_CAN_MODULE_ENABLED #include "stm32f0xx_hal_can.h" #endif /* HAL_CAN_MODULE_ENABLED */ #ifdef HAL_CEC_MODULE_ENABLED #include "stm32f0xx_hal_cec.h" #endif /* HAL_CEC_MODULE_ENABLED */ #ifdef HAL_COMP_MODULE_ENABLED #include "stm32f0xx_hal_comp.h" #endif /* HAL_COMP_MODULE_ENABLED */ #ifdef HAL_CRC_MODULE_ENABLED #include "stm32f0xx_hal_crc.h" #endif /* HAL_CRC_MODULE_ENABLED */ #ifdef HAL_DAC_MODULE_ENABLED #include "stm32f0xx_hal_dac.h" #endif /* HAL_DAC_MODULE_ENABLED */ #ifdef HAL_FLASH_MODULE_ENABLED #include "stm32f0xx_hal_flash.h" #endif /* HAL_FLASH_MODULE_ENABLED */ #ifdef HAL_I2C_MODULE_ENABLED #include "stm32f0xx_hal_i2c.h" #endif /* HAL_I2C_MODULE_ENABLED */ #ifdef HAL_I2S_MODULE_ENABLED #include "stm32f0xx_hal_i2s.h" #endif /* HAL_I2S_MODULE_ENABLED */ #ifdef HAL_IRDA_MODULE_ENABLED #include "stm32f0xx_hal_irda.h" #endif /* HAL_IRDA_MODULE_ENABLED */ #ifdef HAL_IWDG_MODULE_ENABLED #include "stm32f0xx_hal_iwdg.h" #endif /* HAL_IWDG_MODULE_ENABLED */ #ifdef HAL_PCD_MODULE_ENABLED #include "stm32f0xx_hal_pcd.h" #endif /* HAL_PCD_MODULE_ENABLED */ #ifdef HAL_PWR_MODULE_ENABLED #include "stm32f0xx_hal_pwr.h" #endif /* HAL_PWR_MODULE_ENABLED */ #ifdef HAL_RTC_MODULE_ENABLED #include "stm32f0xx_hal_rtc.h" #endif /* HAL_RTC_MODULE_ENABLED */ #ifdef HAL_SMARTCARD_MODULE_ENABLED #include "stm32f0xx_hal_smartcard.h" #endif /* HAL_SMARTCARD_MODULE_ENABLED */ #ifdef HAL_SMBUS_MODULE_ENABLED #include "stm32f0xx_hal_smbus.h" #endif /* HAL_SMBUS_MODULE_ENABLED */ #ifdef HAL_SPI_MODULE_ENABLED #include "stm32f0xx_hal_spi.h" #endif /* HAL_SPI_MODULE_ENABLED */ #ifdef HAL_TIM_MODULE_ENABLED #include "stm32f0xx_hal_tim.h" #endif /* HAL_TIM_MODULE_ENABLED */ #ifdef HAL_TSC_MODULE_ENABLED #include "stm32f0xx_hal_tsc.h" #endif /* HAL_TSC_MODULE_ENABLED */ #ifdef HAL_UART_MODULE_ENABLED #include "stm32f0xx_hal_uart.h" #endif /* HAL_UART_MODULE_ENABLED */ #ifdef HAL_USART_MODULE_ENABLED #include "stm32f0xx_hal_usart.h" #endif /* HAL_USART_MODULE_ENABLED */ #ifdef HAL_WWDG_MODULE_ENABLED #include "stm32f0xx_hal_wwdg.h" #endif /* HAL_WWDG_MODULE_ENABLED */ /* Exported macro ------------------------------------------------------------*/ #ifdef USE_FULL_ASSERT /** * @brief The assert_param macro is used for function's parameters check. * @param expr If expr is false, it calls assert_failed function * which reports the name of the source file and the source * line number of the call that failed. * If expr is true, it returns no value. * @retval None */ #define assert_param(expr) ((expr) ? (void)0U : assert_failed((uint8_t *)__FILE__, __LINE__)) /* Exported functions ------------------------------------------------------- */ void assert_failed(uint8_t* file, uint32_t line); #else #define assert_param(expr) ((void)0U) #endif /* USE_FULL_ASSERT */ #ifdef __cplusplus } #endif #endif /* __STM32F0xx_HAL_CONF_H */