HAL_StatusTypeDef HAL_InitTick(uint32_t TickPriority) { RCC_ClkInitTypeDef clkconfig; uint32_t uwTimclock, uwAPB1Prescaler = 0U; uint32_t uwPrescalerValue = 0U; uint32_t pFLatency; HAL_StatusTypeDef status; /*Configure the TIM6 IRQ priority */ HAL_NVIC_SetPriority(TIM6_DAC_IRQn, TickPriority ,0); /* Enable the TIM6 global Interrupt */ HAL_NVIC_EnableIRQ(TIM6_DAC_IRQn); /* Enable TIM6 clock */ __HAL_RCC_TIM6_CLK_ENABLE(); /* Get clock configuration */ HAL_RCC_GetClockConfig(&clkconfig, &pFLatency); /* Get APB1 prescaler */ uwAPB1Prescaler = clkconfig.APB1CLKDivider; /* Compute TIM6 clock */ if (uwAPB1Prescaler == RCC_HCLK_DIV1) { uwTimclock = HAL_RCC_GetPCLK1Freq(); } else { uwTimclock = 2UL * HAL_RCC_GetPCLK1Freq(); } /* Compute the prescaler value to have TIM6 counter clock equal to 1MHz */ uwPrescalerValue = (uint32_t) ((uwTimclock / 1000000U) - 1U); /* Initialize TIM6 */ htim6.Instance = TIM6; /* Initialize TIMx peripheral as follow: + Period = [(TIM6CLK/1000) - 1]. to have a (1/1000) s time base. + Prescaler = (uwTimclock/1000000 - 1) to have a 1MHz counter clock. + ClockDivision = 0 + Counter direction = Up */ htim6.Init.Period = (1000000U / 1000U) - 1U; htim6.Init.Prescaler = uwPrescalerValue; htim6.Init.ClockDivision = 0; htim6.Init.CounterMode = TIM_COUNTERMODE_UP; htim6.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE; status = HAL_TIM_Base_Init(&htim6); if (status == HAL_OK) { /* Start the TIM time Base generation in interrupt mode */ status = HAL_TIM_Base_Start_IT(&htim6); if (status == HAL_OK) { /* Enable the TIM6 global Interrupt */ //HAL_NVIC_EnableIRQ(TIM6_DAC_IRQn); /* Configure the SysTick IRQ priority */ if (TickPriority < (1UL << __NVIC_PRIO_BITS)) { /* Configure the TIM IRQ priority */ HAL_NVIC_SetPriority(TIM6_DAC_IRQn, TickPriority, 0U); /* Enable the TIM6 global Interrupt */ HAL_NVIC_EnableIRQ(TIM6_DAC_IRQn); //uwTickPrio = TickPriority; } else { status = HAL_ERROR; } } } /* Return function status */ return status; }