/* tpm_io_st.c * * Copyright (C) 2006-2022 wolfSSL Inc. * * This file is part of wolfTPM. * * wolfTPM is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License as published by * the Free Software Foundation; either version 2 of the License, or * (at your option) any later version. * * wolfTPM is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA 02110-1335, USA */ /* This example shows IO interfaces for STM32 CubeMX HAL */ #include #include #include "tpm_io.h" /******************************************************************************/ /* --- BEGIN IO Callback Logic -- */ /******************************************************************************/ /* Included via tpm_io.c if WOLFTPM_INCLUDE_IO_FILE is defined */ #ifdef WOLFTPM_INCLUDE_IO_FILE #if ! (defined(WOLFTPM_LINUX_DEV) || \ defined(WOLFTPM_SWTPM) || \ defined(WOLFTPM_WINAPI) ) #if defined(WOLFSSL_STM32_CUBEMX) #ifdef WOLFTPM_I2C #ifndef TPM_I2C_TRIES #define TPM_I2C_TRIES 10 #endif #ifndef TPM2_I2C_ADDR #define TPM2_I2C_ADDR 0x2e #endif #ifndef STM32_CUBEMX_I2C_TIMEOUT #define STM32_CUBEMX_I2C_TIMEOUT 250 /* ticks/ms */ #endif /* STM32 CubeMX HAL I2C */ static int i2c_read(void* userCtx, word32 reg, byte* data, int len) { int ret = TPM_RC_FAILURE; HAL_StatusTypeDef status; I2C_HandleTypeDef* hi2c = (I2C_HandleTypeDef*)userCtx; int i2cAddr = (TPM2_I2C_ADDR << 1) | 0x01; /* For I2C read LSB is 1 */ int timeout = TPM_I2C_TRIES; byte buf[1]; /* TIS layer should never provide a buffer larger than this, but double check for good coding practice */ if (len > MAX_SPI_FRAMESIZE) return BAD_FUNC_ARG; buf[0] = (reg & 0xFF); /* convert to simple 8-bit address for I2C */ /* The I2C takes about 80us to wake up and will NAK until it is ready */ do { /* Write address to read from - retry until ack */ status = HAL_I2C_Master_Transmit(hi2c, i2cAddr, buf, sizeof(buf), STM32_CUBEMX_I2C_TIMEOUT); HAL_Delay(1); /* guard time - should be 250us */ } while (status != HAL_OK && --timeout > 0); if (status == HAL_OK) { timeout = TPM_I2C_TRIES; /* Perform read with retry */ do { status = HAL_I2C_Master_Receive(hi2c, i2cAddr, data, len, STM32_CUBEMX_I2C_TIMEOUT); if (status != HAL_OK) HAL_Delay(1); /* guard time - should be 250us */ } while (status != HAL_OK && --timeout > 0); } if (status == HAL_OK) { ret = TPM_RC_SUCCESS; } else { printf("I2C Read failure %d (tries %d)\n", status, TPM_I2C_TRIES - timeout); } return ret; } static int i2c_write(void* userCtx, word32 reg, byte* data, int len) { int ret = TPM_RC_FAILURE; HAL_StatusTypeDef status; I2C_HandleTypeDef* hi2c = (I2C_HandleTypeDef*)userCtx; int i2cAddr = (TPM2_I2C_ADDR << 1); /* I2C write operation, LSB is 0 */ int timeout = TPM_I2C_TRIES; byte buf[MAX_SPI_FRAMESIZE+1]; /* TIS layer should never provide a buffer larger than this, but double check for good coding practice */ if (len > MAX_SPI_FRAMESIZE) return BAD_FUNC_ARG; /* Build packet with TPM register and data */ buf[0] = (reg & 0xFF); /* convert to simple 8-bit address for I2C */ XMEMCPY(buf + 1, data, len); /* The I2C takes about 80us to wake up and will NAK until it is ready */ do { status = HAL_I2C_Master_Transmit(hi2c, i2cAddr, buf, len+1, STM32_CUBEMX_I2C_TIMEOUT); if (status != HAL_OK) HAL_Delay(1); /* guard time - should be 250us */ } while (status != HAL_OK && --timeout > 0); if (status == HAL_OK) { ret = TPM_RC_SUCCESS; } else { printf("I2C Write failure %d\n", status); } return ret; } int TPM2_IoCb_STCubeMX_I2C(TPM2_CTX* ctx, int isRead, word32 addr, byte* buf, word16 size, void* userCtx) { int ret = TPM_RC_FAILURE; if (userCtx != NULL) { if (isRead) ret = i2c_read(userCtx, addr, buf, size); else ret = i2c_write(userCtx, addr, buf, size); } (void)ctx; return ret; } #else /* STM32 CubeMX Hal SPI */ #define STM32_CUBEMX_SPI_TIMEOUT 250 int TPM2_IoCb_STCubeMX_SPI(TPM2_CTX* ctx, const byte* txBuf, byte* rxBuf, word16 xferSz, void* userCtx) { int ret = TPM_RC_FAILURE; SPI_HandleTypeDef* hspi = (SPI_HandleTypeDef*)userCtx; HAL_StatusTypeDef status; #ifdef WOLFTPM_CHECK_WAIT_STATE int timeout = TPM_SPI_WAIT_RETRY; #endif __HAL_SPI_ENABLE(hspi); #ifndef USE_HW_SPI_CS HAL_GPIO_WritePin(GPIOA, GPIO_PIN_15, GPIO_PIN_RESET); /* active low */ #endif #ifdef WOLFTPM_CHECK_WAIT_STATE /* Send Header */ status = HAL_SPI_TransmitReceive(hspi, (byte*)txBuf, rxBuf, TPM_TIS_HEADER_SZ, STM32_CUBEMX_SPI_TIMEOUT); if (status != HAL_OK) { #ifndef USE_HW_SPI_CS HAL_GPIO_WritePin(GPIOA, GPIO_PIN_15, GPIO_PIN_SET); #endif __HAL_SPI_DISABLE(hspi); return TPM_RC_FAILURE; } /* Check for wait states */ if ((rxBuf[TPM_TIS_HEADER_SZ-1] & TPM_TIS_READY_MASK) == 0) { do { /* Check for SPI ready */ status = HAL_SPI_TransmitReceive(hspi, (byte*)txBuf, rxBuf, 1, STM32_CUBEMX_SPI_TIMEOUT); if (rxBuf[0] & TPM_TIS_READY_MASK) break; } while (status == HAL_OK && --timeout > 0); #ifdef WOLFTPM_DEBUG_TIMEOUT printf("SPI Ready Wait %d\n", TPM_SPI_WAIT_RETRY - timeout); #endif if (timeout <= 0) { #ifndef USE_HW_SPI_CS HAL_GPIO_WritePin(GPIOA, GPIO_PIN_15, GPIO_PIN_SET); #endif __HAL_SPI_DISABLE(hspi); return TPM_RC_FAILURE; } } /* Send remainder of payload */ status = HAL_SPI_TransmitReceive(hspi, (byte*)&txBuf[TPM_TIS_HEADER_SZ], &rxBuf[TPM_TIS_HEADER_SZ], xferSz - TPM_TIS_HEADER_SZ, STM32_CUBEMX_SPI_TIMEOUT); #else /* Send Entire Message - no wait states */ status = HAL_SPI_TransmitReceive(hspi, (byte*)txBuf, rxBuf, xferSz, STM32_CUBEMX_SPI_TIMEOUT); #endif /* WOLFTPM_CHECK_WAIT_STATE */ #ifndef USE_HW_SPI_CS HAL_GPIO_WritePin(GPIOA, GPIO_PIN_15, GPIO_PIN_SET); #endif __HAL_SPI_DISABLE(hspi); if (status == HAL_OK) ret = TPM_RC_SUCCESS; (void)ctx; return ret; } #endif /* WOLFTPM_I2C */ #endif #endif /* !(WOLFTPM_LINUX_DEV || WOLFTPM_SWTPM || WOLFTPM_WINAPI) */ #endif /* WOLFTPM_INCLUDE_IO_FILE */ /******************************************************************************/ /* --- END IO Callback Logic -- */ /******************************************************************************/