[Port4] : UrzÄ…dzenie kompozytowe USB Is Port User Connectable: yes Is Port Debug Capable: no Companion Port Number: 14 Companion Hub Symbolic Link Name: USB#ROOT_HUB30#4&65b2299&0&0#{f18a0e88-c30c-11d0-8815-00a0c906bed8} Protocols Supported: USB 1.1: yes USB 2.0: yes USB 3.0: no Device Power State: PowerDeviceD0 ---===>Device Information<===--- English product name: "RNDIS" ConnectionStatus: Current Config Value: 0x01 -> Device Bus Speed: Full (is not SuperSpeed or higher capable) Device Address: 0x13 Open Pipes: 3 ===>Device Descriptor<=== bLength: 0x12 bDescriptorType: 0x01 bcdUSB: 0x0201 bDeviceClass: 0xEF -> This is a Multi-interface Function Code Device bDeviceSubClass: 0x02 -> This is the Common Class Sub Class bDeviceProtocol: 0x01 -> This is the Interface Association Descriptor protocol bMaxPacketSize0: 0x40 = (64) Bytes idVendor: 0x0483 = STMicroelectronics idProduct: 0x5740 bcdDevice: 0x0200 iManufacturer: 0x01 English (United States) "STMicroelectronics" iProduct: 0x02 English (United States) "RNDIS" iSerialNumber: 0x03 English (United States) "205333705853" bNumConfigurations: 0x01 ---===>Open Pipes<===--- ===>Endpoint Descriptor<=== bLength: 0x07 bDescriptorType: 0x05 bEndpointAddress: 0x82 -> Direction: IN - EndpointID: 2 bmAttributes: 0x03 -> Interrupt Transfer Type wMaxPacketSize: 0x0010 = 0x10 bytes bInterval: 0x10 ===>Endpoint Descriptor<=== bLength: 0x07 bDescriptorType: 0x05 bEndpointAddress: 0x01 -> Direction: OUT - EndpointID: 1 bmAttributes: 0x02 -> Bulk Transfer Type wMaxPacketSize: 0x0040 = 0x40 bytes bInterval: 0x00 ===>Endpoint Descriptor<=== bLength: 0x07 bDescriptorType: 0x05 bEndpointAddress: 0x81 -> Direction: IN - EndpointID: 1 bmAttributes: 0x02 -> Bulk Transfer Type wMaxPacketSize: 0x0040 = 0x40 bytes bInterval: 0x00 ---===>Full Configuration Descriptor<===--- ===>Configuration Descriptor<=== bLength: 0x09 bDescriptorType: 0x02 wTotalLength: 0x004B -> Validated bNumInterfaces: 0x02 bConfigurationValue: 0x01 iConfiguration: 0x00 bmAttributes: 0xC0 -> Self Powered MaxPower: 0x32 = 100 mA ===>IAD Descriptor<=== bLength: 0x08 bDescriptorType: 0x0B bFirstInterface: 0x00 bInterfaceCount: 0x02 bFunctionClass: 0xE0 *!*CAUTION: This appears to be an invalid Interface Class bFunctionSubClass: 0x01 bFunctionProtocol: 0x03 iFunction: 0x00 ===>Interface Descriptor<=== bLength: 0x09 bDescriptorType: 0x04 bInterfaceNumber: 0x00 bAlternateSetting: 0x00 bNumEndpoints: 0x01 bInterfaceClass: 0x02 -> This is Communications (CDC Control) USB Device Interface Class bInterfaceSubClass: 0x02 bInterfaceProtocol: 0xFF iInterface: 0x00 -> This is a Communications (CDC Control) USB Device Interface Class ===>Descriptor Hex Dump<=== bLength: 0x05 bDescriptorType: 0x24 05 24 00 10 01 -> This is a Communications (CDC Control) USB Device Interface Class ===>Descriptor Hex Dump<=== bLength: 0x05 bDescriptorType: 0x24 05 24 01 00 01 -> This is a Communications (CDC Control) USB Device Interface Class ===>Descriptor Hex Dump<=== bLength: 0x04 bDescriptorType: 0x24 04 24 02 00 -> This is a Communications (CDC Control) USB Device Interface Class ===>Descriptor Hex Dump<=== bLength: 0x05 bDescriptorType: 0x24 05 24 06 00 01 ===>Endpoint Descriptor<=== bLength: 0x07 bDescriptorType: 0x05 bEndpointAddress: 0x82 -> Direction: IN - EndpointID: 2 bmAttributes: 0x03 -> Interrupt Transfer Type wMaxPacketSize: 0x0010 = 0x10 bytes bInterval: 0x10 ===>Interface Descriptor<=== bLength: 0x09 bDescriptorType: 0x04 bInterfaceNumber: 0x01 bAlternateSetting: 0x00 bNumEndpoints: 0x02 bInterfaceClass: 0x0A -> This is a CDC Data USB Device Interface Class bInterfaceSubClass: 0x00 bInterfaceProtocol: 0x00 iInterface: 0x00 ===>Endpoint Descriptor<=== bLength: 0x07 bDescriptorType: 0x05 bEndpointAddress: 0x01 -> Direction: OUT - EndpointID: 1 bmAttributes: 0x02 -> Bulk Transfer Type wMaxPacketSize: 0x0040 = 0x40 bytes bInterval: 0x00 ===>Endpoint Descriptor<=== bLength: 0x07 bDescriptorType: 0x05 bEndpointAddress: 0x81 -> Direction: IN - EndpointID: 1 bmAttributes: 0x02 -> Bulk Transfer Type wMaxPacketSize: 0x0040 = 0x40 bytes bInterval: 0x00 ===>BOS Descriptor<=== bLength: 0x05 bDescriptorType: 0x0F wTotalLength: 0x000C bNumDeviceCaps: 0x01 ===>USB 2.0 Extension Descriptor<=== bLength: 0x07 bDescriptorType: 0x10 bDevCapabilityType: 0x02 bmAttributes: 0x00000002 -> Supports Link Power Management protocol