[Port4] FailedEnumeration : Nieznane urządzenie USB (żądanie deskryptora urządzenia nie powiodło się) Is Port User Connectable: yes Is Port Debug Capable: no Companion Port Number: 14 Companion Hub Symbolic Link Name: USB#ROOT_HUB30#4&65b2299&0&0#{f18a0e88-c30c-11d0-8815-00a0c906bed8} Protocols Supported: USB 1.1: yes USB 2.0: yes USB 3.0: no ---===>Device Information<===--- ConnectionStatus: FailedEnumeration Current Config Value: 0x00 -> Device Bus Speed: Full (is not SuperSpeed or higher capable) Device Address: 0x00 Open Pipes: 0 *!*ERROR: No open pipes! ===>Device Descriptor<=== *!*ERROR: bLength of 0 incorrect, should be 18 bLength: 0x00 bDescriptorType: 0x00 bcdUSB: 0x0000 bDeviceClass: 0x00 *!*ERROR: Device enumeration failure