/** ****************************************************************************** * @file : usbd_cdc_if.c * @author : MCD Application Team * @version : V1.1.0 * @date : 19-March-2012 * @brief : ****************************************************************************** * COPYRIGHT(c) 2014 STMicroelectronics * * Redistribution and use in source and binary forms, with or without modification, * are permitted provided that the following conditions are met: * 1. Redistributions of source code must retain the above copyright notice, * this list of conditions and the following disclaimer. * 2. Redistributions in binary form must reproduce the above copyright notice, * this list of conditions and the following disclaimer in the documentation * and/or other materials provided with the distribution. * 3. Neither the name of STMicroelectronics nor the names of its contributors * may be used to endorse or promote products derived from this software * without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE * DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE * FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL * DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR * SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER * CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * ****************************************************************************** */ /* Includes ------------------------------------------------------------------*/ #include "usbd_cdc_if.h" #include "ecom_defs.h" /** @addtogroup STM32_USB_OTG_DEVICE_LIBRARY * @{ */ /** @defgroup USBD_CDC * @brief usbd core module * @{ */ /** @defgroup USBD_CDC_Private_TypesDefinitions * @{ */ /* USER CODE BEGIN 0 */ /* USER CODE END 0 */ /** * @} */ /** @defgroup USBD_CDC_Private_Defines * @{ */ /* USER CODE BEGIN 1 */ /* Define size for the receive and transmit buffer over CDC */ /* It's up to user to redefine and/or remove those define */ #define APP_RX_DATA_SIZE 512 #define APP_TX_DATA_SIZE 512 /* USER CODE END 1 */ /** * @} */ /** @defgroup USBD_CDC_Private_Macros * @{ */ /* USER CODE BEGIN 2 */ /* USER CODE END 2 */ /** * @} */ /** @defgroup USBD_CDC_Private_Variables * @{ */ /* USER CODE BEGIN 3 */ /* Create buffer for reception and transmission */ /* It's up to user to redefine and/or remove those define */ /* Received Data over USB are stored in this buffer */ uint8_t UserRxBufferFS[APP_RX_DATA_SIZE]; uint16_t head = 0; uint16_t tail = 0; uint8_t overrun_warn = 0; /* Send Data over USB CDC are stored in this buffer */ uint8_t UserTxBufferFS[APP_TX_DATA_SIZE]; /* USER CODE END 3 */ /* USB handler declaration */ /* Handle for USB Full Speed IP */ USBD_HandleTypeDef *hUsbDevice_0; extern USBD_HandleTypeDef hUsbDeviceFS; /** * @} */ /** @defgroup USBD_CDC_Private_FunctionPrototypes * @{ */ static int8_t CDC_Init_FS (void); static int8_t CDC_DeInit_FS (void); static int8_t CDC_Control_FS (uint8_t cmd, uint8_t* pbuf, uint16_t length); static int8_t CDC_Receive_FS (uint8_t* pbuf, uint32_t *Len); USBD_CDC_ItfTypeDef USBD_Interface_fops_FS = { CDC_Init_FS, CDC_DeInit_FS, CDC_Control_FS, CDC_Receive_FS }; /* Private functions ---------------------------------------------------------*/ /** * @brief CDC_Init_FS * Initializes the CDC media low layer over the FS USB IP * @param None * @retval Result of the opeartion: USBD_OK if all operations are OK else USBD_FAIL */ static int8_t CDC_Init_FS(void) { hUsbDevice_0 = &hUsbDeviceFS; /* USER CODE BEGIN 4 */ /* Set Application Buffers */ USBD_CDC_SetTxBuffer(hUsbDevice_0, UserTxBufferFS, 0); USBD_CDC_SetRxBuffer(hUsbDevice_0, UserRxBufferFS); return (USBD_OK); /* USER CODE END 4 */ } /** * @brief CDC_DeInit_FS * DeInitializes the CDC media low layer * @param None * @retval Result of the opeartion: USBD_OK if all operations are OK else USBD_FAIL */ static int8_t CDC_DeInit_FS(void) { /* USER CODE BEGIN 5 */ return (USBD_OK); /* USER CODE END 5 */ } /** * @brief CDC_Control_FS * Manage the CDC class requests * @param Cmd: Command code * @param Buf: Buffer containing command data (request parameters) * @param Len: Number of data to be sent (in bytes) * @retval Result of the opeartion: USBD_OK if all operations are OK else USBD_FAIL */ static int8_t CDC_Control_FS (uint8_t cmd, uint8_t* pbuf, uint16_t length) { /* USER CODE BEGIN 6 */ switch (cmd) { case CDC_SEND_ENCAPSULATED_COMMAND: break; case CDC_GET_ENCAPSULATED_RESPONSE: break; case CDC_SET_COMM_FEATURE: break; case CDC_GET_COMM_FEATURE: break; case CDC_CLEAR_COMM_FEATURE: break; /*******************************************************************************/ /* Line Coding Structure */ /*-----------------------------------------------------------------------------*/ /* Offset | Field | Size | Value | Description */ /* 0 | dwDTERate | 4 | Number |Data terminal rate, in bits per second*/ /* 4 | bCharFormat | 1 | Number | Stop bits */ /* 0 - 1 Stop bit */ /* 1 - 1.5 Stop bits */ /* 2 - 2 Stop bits */ /* 5 | bParityType | 1 | Number | Parity */ /* 0 - None */ /* 1 - Odd */ /* 2 - Even */ /* 3 - Mark */ /* 4 - Space */ /* 6 | bDataBits | 1 | Number Data bits (5, 6, 7, 8 or 16). */ /*******************************************************************************/ case CDC_SET_LINE_CODING: break; case CDC_GET_LINE_CODING: break; case CDC_SET_CONTROL_LINE_STATE: break; case CDC_SEND_BREAK: break; default: break; } return (USBD_OK); /* USER CODE END 6 */ } /** * @brief CDC_Receive_FS * Data received over USB OUT endpoint are sent over CDC interface * through this function. * * @note * This function will block any OUT packet reception on USB endpoint * untill exiting this function. If you exit this function before transfer * is complete on CDC interface (ie. using DMA controller) it will result * in receiving more data while previous ones are still not sent. * * @param Buf: Buffer of data to be received * @param Len: Number of data received (in bytes) * @retval Result of the opeartion: USBD_OK if all operations are OK else USBD_FAIL */ static int8_t CDC_Receive_FS (uint8_t* Buf, uint32_t *Len) { /* USER CODE BEGIN 7 */ /*if (overrun_warn && (head==tail)) return USBD_FAIL; memcpy(UserRxBufferFS+head, Buf, *Len); if (((tail-head)==8) || ((head-tail)==(sizeof(UserRxBufferFS)-8))) { overrun_warn = 1; } head += 8; if (head == sizeof(UserRxBufferFS)) head = 0;*/ LED_Toggle(LED_SERIAL_GREEN); return USBD_OK; /* USER CODE END 7 */ } /* Called by application */ uint8_t get_from_rx_buffer(uint8_t *buf, uint16_t max_len) { if ((tail==head) && !overrun_warn) return 0; //no new packets memcpy(buf, UserRxBufferFS+tail, max_len); tail += 8; overrun_warn = 0; if (tail == sizeof(UserRxBufferFS)) tail = 0; return max_len; //is it okay to return this?? } /** * @brief CDC_Transmit_FS * Data send over USB IN endpoint are sent over CDC interface * through this function. * @note * * * @param Buf: Buffer of data to be send * @param Len: Number of data to be send (in bytes) * @retval Result of the opeartion: USBD_OK if all operations are OK else USBD_FAIL or USBD_BUSY */ uint8_t CDC_Transmit_FS(uint8_t* Buf, uint16_t Len) { uint8_t result = USBD_OK; /* USER CODE BEGIN 8 */ USBD_CDC_SetTxBuffer(hUsbDevice_0, UserTxBufferFS, Len); result = USBD_CDC_TransmitPacket(hUsbDevice_0); /* USER CODE END 8 */ return result; } /** * @} */ /** * @} */ /** * @} */ /************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/