/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * *

© Copyright (c) 2019 STMicroelectronics. * All rights reserved.

* * This software component is licensed by ST under BSD 3-Clause license, * the "License"; You may not use this file except in compliance with the * License. You may obtain a copy of the License at: * opensource.org/licenses/BSD-3-Clause * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ #define FLASH_USER_START_ADDR 0x08007C00 /* Start @ of user Flash area - last page 1 kB */ #define FLASH_USER_END_ADDR 0x08007FFF /* End @ of user Flash area */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ ADC_HandleTypeDef hadc; DMA_HandleTypeDef hdma_adc; /* USER CODE BEGIN PV */ uint32_t Address = 0, PageError = 0; /*Variable used for Erase procedure*/ static FLASH_EraseInitTypeDef EraseInitStruct; uint16_t Level_mean; uint16_t Level[20]; __IO uint16_t Level_ADC, Level_valid=0,i=0; __IO uint16_t low_level=300;// __IO uint16_t high_level=3500;// /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_DMA_Init(void); static void MX_ADC_Init(void); static void MX_NVIC_Init(void); /* USER CODE BEGIN PFP */ void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin); //void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc); void HAL_SYSTICK_Callback(void); /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_DMA_Init(); MX_ADC_Init(); /* Initialize interrupts */ MX_NVIC_Init(); /* USER CODE BEGIN 2 */ HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK); HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000); HAL_GPIO_WritePin(RELAY_GPIO_Port, RELAY_Pin, GPIO_PIN_SET);//Close EZ while(HAL_ADCEx_Calibration_Start(&hadc) != HAL_OK); //HAL_ADC_Start(&hadc); //HAL_ADC_Start_IT(&hadc); HAL_ADC_Start_DMA(&hadc, &Level_ADC, 1); Address = FLASH_USER_START_ADDR; low_level=*(__IO uint16_t*)Address; Address = Address+4; high_level=*(__IO uint16_t*)Address; /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ while(Level_valid!=1); if (HAL_GPIO_ReadPin(MODE_GPIO_Port, MODE_Pin)==GPIO_PIN_SET) { if(Level_mean<= low_level) { HAL_GPIO_WritePin(RELAY_GPIO_Port, RELAY_Pin, GPIO_PIN_RESET);//Open EZ } else if(Level_mean> high_level) { HAL_GPIO_WritePin(RELAY_GPIO_Port, RELAY_Pin, GPIO_PIN_SET);//Close EZ } } else { HAL_GPIO_WritePin(RELAY_GPIO_Port, RELAY_Pin, GPIO_PIN_RESET);//Open EZ } } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Initializes the CPU, AHB and APB busses clocks */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB busses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV16; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK) { Error_Handler(); } } /** * @brief NVIC Configuration. * @retval None */ static void MX_NVIC_Init(void) { /* EXTI2_3_IRQn interrupt configuration */ HAL_NVIC_SetPriority(EXTI2_3_IRQn, 0, 0); HAL_NVIC_EnableIRQ(EXTI2_3_IRQn); } /** * @brief ADC Initialization Function * @param None * @retval None */ static void MX_ADC_Init(void) { /* USER CODE BEGIN ADC_Init 0 */ /* USER CODE END ADC_Init 0 */ ADC_ChannelConfTypeDef sConfig = {0}; /* USER CODE BEGIN ADC_Init 1 */ /* USER CODE END ADC_Init 1 */ /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion) */ hadc.Instance = ADC1; hadc.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4; hadc.Init.Resolution = ADC_RESOLUTION_12B; hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc.Init.ScanConvMode = ADC_SCAN_DIRECTION_FORWARD; hadc.Init.EOCSelection = ADC_EOC_SINGLE_CONV; hadc.Init.LowPowerAutoWait = DISABLE; hadc.Init.LowPowerAutoPowerOff = DISABLE; hadc.Init.ContinuousConvMode = ENABLE; hadc.Init.DiscontinuousConvMode = DISABLE; hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START; hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; hadc.Init.DMAContinuousRequests = ENABLE; hadc.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN; if (HAL_ADC_Init(&hadc) != HAL_OK) { Error_Handler(); } /** Configure for the selected ADC regular channel to be converted. */ sConfig.Channel = ADC_CHANNEL_9; sConfig.Rank = ADC_RANK_CHANNEL_NUMBER; sConfig.SamplingTime = ADC_SAMPLETIME_239CYCLES_5; if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN ADC_Init 2 */ /* USER CODE END ADC_Init 2 */ } /** * Enable DMA controller clock */ static void MX_DMA_Init(void) { /* DMA controller clock enable */ __HAL_RCC_DMA1_CLK_ENABLE(); /* DMA interrupt init */ /* DMA1_Channel1_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn); } /** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(RELAY_GPIO_Port, RELAY_Pin, GPIO_PIN_RESET); /*Configure GPIO pins : MODE_Pin HIGH_Pin LOW_Pin */ GPIO_InitStruct.Pin = MODE_Pin|HIGH_Pin|LOW_Pin; GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /*Configure GPIO pin : RELAY_Pin */ GPIO_InitStruct.Pin = RELAY_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(RELAY_GPIO_Port, &GPIO_InitStruct); /* EXTI interrupt init*/ HAL_NVIC_SetPriority(EXTI4_15_IRQn, 0, 0); HAL_NVIC_EnableIRQ(EXTI4_15_IRQn); } /* USER CODE BEGIN 4 */ void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) { if(HAL_GPIO_ReadPin(MODE_GPIO_Port, MODE_Pin)==GPIO_PIN_RESET) { if(GPIO_Pin == LOW_Pin) { //zapis do EEPROM niskiego poziomu zbiornika low_level=Level_ADC; //HAL_GPIO_TogglePin(LED_GPIO_Port, LED_Pin); HAL_FLASH_Unlock(); EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES; EraseInitStruct.PageAddress = FLASH_USER_START_ADDR; EraseInitStruct.NbPages = 1; HAL_FLASHEx_Erase(&EraseInitStruct, &PageError); /* Program the user Flash area word by word (area defined by FLASH_USER_START_ADDR and FLASH_USER_END_ADDR) ***********/ Address = FLASH_USER_START_ADDR; if(Address < FLASH_USER_END_ADDR) { HAL_FLASH_Program(FLASH_TYPEPROGRAM_HALFWORD, Address, low_level); HAL_FLASH_Program(FLASH_TYPEPROGRAM_HALFWORD, Address+4, high_level); } /* Lock the Flash to disable the flash control register access (recommended to protect the FLASH memory against possible unwanted operation) *********/ HAL_FLASH_Lock(); } if(GPIO_Pin == HIGH_Pin) { //zapis do EEPROM wysokiego stanu zbiornika high_level=Level_ADC; //HAL_GPIO_TogglePin(LED_GPIO_Port, LED_Pin); HAL_FLASH_Unlock(); EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES; EraseInitStruct.PageAddress = FLASH_USER_START_ADDR; EraseInitStruct.NbPages = 1; HAL_FLASHEx_Erase(&EraseInitStruct, &PageError); /* Program the user Flash area word by word (area defined by FLASH_USER_START_ADDR and FLASH_USER_END_ADDR) ***********/ Address = FLASH_USER_START_ADDR; if(Address < FLASH_USER_END_ADDR) { HAL_FLASH_Program(FLASH_TYPEPROGRAM_HALFWORD, Address, low_level); HAL_FLASH_Program(FLASH_TYPEPROGRAM_HALFWORD, Address+4, high_level); } /* Lock the Flash to disable the flash control register access (recommended to protect the FLASH memory against possible unwanted operation) *********/ HAL_FLASH_Lock(); } } } void HAL_SYSTICK_Callback(void) { Level[i]=Level_ADC; i++; if(i==20) { Level_valid=1; i=0; } if(Level_valid==1) { Level_mean=0; for(uint16_t j=0;j<20;j++) { Level_mean=Level_mean+Level[j]; } Level_mean=Level_mean/20; } } /*void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc) { if (__HAL_ADC_GET_FLAG(hadc, ADC_FLAG_EOC)) { Level_ADC = HAL_ADC_GetValue(hadc); } }*/ /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(char *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */ /************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/