Motor control via ADC NVIC STM32

Video created by HAMDI Mustapha on Dec 18, 2016

    Timer 2 used to time the ADC triggering and the interrupt requesting periodically. The end-of-conversion (eoc) signal from the ADC is connected to the Interrupt Component. Interrupts on the Cortex-M are controlled by the Nested Vectored Interrupt Controller (NVIC).The interrupt service routine will sample the ADC, process (or save) the data, and then return to the main thread. Motor control via ADC NVIC STM32
    IIA5 RT5 labs @INSAT