AnsweredAssumed Answered

Bad linker file with CubeMx

Question asked by Philippe on Jul 20, 2015
Latest reply on Feb 9, 2016 by STM32Cube-T
Hello,

i'm using a STM32F334C8 with STM32CubeMx and with Atollic True Studio or SW4STM32.
When i generate a project with STM32CubeMx (for TrueStudio or SW4STM32) the linker file is wrong. I get a 16ko size ram instead of 12ko. When i try to debug, an address error occurs. I have to manually modify the linker file (*.ld) and after everything is ok.
When i create a project with True Studio only, the linker file is ok.
This is very strange. Is it a bug or do i miss something ?

Thanks

Outcomes