AnsweredAssumed Answered

Where can I find "main.h"

Question asked by H.Rick on Jul 17, 2015
Latest reply on Jul 18, 2015 by H.Rick
Guys, where can I find "main.h"....? I use Keil MDK...

Thanks
I read from :
"Developing applications on STM32Cube with LwIP TCP/IP stack ", page 39


How do I choose between static or dynamic (DHCP)
IP address allocation?
When the macro #define USE_DHCP located in main.h is commented, a static IP address is assigned to the STM32 microcontroller (by default 192.168.0.10, this value can be modified from “main.h” file).
If the macro #define USE_DHCP is uncommented, the DHCP protocol is enabled, and the STM32 will act as a DHCP clien

Outcomes