AnsweredAssumed Answered

SPI Bus Fault due to xPortSysTickHandler FreeRTOS

Question asked by vrijelinck.ronny on Jul 10, 2015
When the xPortSysTickHandler is called at the moment the SPI HW block is executing a SPI communication the i get a Bus fault resulting in a Hardfault
Is this a known issue?
I can solve the issue by first executing the FreeRTOS command taskENTER_CRITICAL
but then the Systick is not running anymore, with the result that the Timeout functions in the stmf2xx_hal_spi are not working any more
Does any one know a solution for this issue?

Outcomes