AnsweredAssumed Answered

Is stm32cubemx v4.8 a beta?

Question asked by bonelli on Jul 1, 2015
Latest reply on Jul 17, 2015 by STM32Cube-T
Hello,


Since I had only bugs with previous versions, I have updated the cubeMX package. It produce the same bug in all following configurations :
- cubeMX + IAR
- cubeMX + SW4
- cubeMX as eclipse plugin + SW4


Create a new project, STM32F405 for instance, use ADC, click on "generate code" and try to compile.
1/- WHY does the *.ioc is copied in a subfolder ? Which one must be used later ?
2/- The adc.c/adc.h files are placed in the scr/inc folders (that's the only good news) BUT when compiling gcc reports "adc.h not found"


Other bug :
3/-"File/save project as" (or associated icons) sometime opens the "settings" window and sometime opens the "save as" windows (randomly).


Thank you

Outcomes