AnsweredAssumed Answered

STM32Cube_FW_F4 firmware library does not updated.

Question asked by just4you on Jun 25, 2015
Latest reply on Jun 26, 2015 by just4you
I use the STM32CubeMX 4.8 version and update the firmware package for Family STM32F4 1.6.0.
However, the source code of the library is 1.3.1.
I also use the STM32CubeF4 1.6.0 but it is the same version of STM32CubeMX 4.8.


The STM32F4 DSP and standard peripherals library is currently 1.5.1.
Why the difference is occured between the libraries?

Moreover, the STM32CubeF4 1.6.0 library has clock configuration bug.

I hope this problem would be solved as soon as possible.

Outcomes