AnsweredAssumed Answered

STM32CubeMX ethernet on stm32f107

Question asked by thomas.paul.001 on Jun 5, 2015
Latest reply on Jun 23, 2015 by Amel N
Hello,

I am trying to use STM32CubeMX to generate a simple Ethernet example for the Olimex STM32-P107 board. I'm using SWSTM32 and the problem appears to be in stm32f1xx_hal_eth.c line 215
while (((heth->Instance)->DMABMR & ETH_DMABMR_SR) != (uint32_t)RESET)
(heth->Instance)->DMABMR has a value of 0x20101
So I guess that lsb is 1 when it's looking for RESET which is 0.

Anyway, STM32CubeMX is a pretty cool tool. Hopefully, this will make sense to someone and we'll get it fixed quickly.

The project was generated with STM32CubeMX Version 4.8.0 and STM32CubeF1 Version 1.0.0

thanks,
Paul

Attachments

Outcomes